<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: eMMC support for iMX6 Linux BSP in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-support-for-iMX6-Linux-BSP/m-p/254373#M23995</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Honey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you are conused with eMMC and NAND. Usually, eMMC means NAND flash with controller including ECC and it is&amp;nbsp; connected thru SDHC. But NAND, usually it is refered as 'raw NAND', is pure NAND device which can be connected GPMI I/F of i.MX6. And our internal BCH block can be used for its operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;eMMC can be connected thru uSDHC I/F and it is supported by our BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Sep 2013 05:14:26 GMT</pubDate>
    <dc:creator>Paul_Kang</dc:creator>
    <dc:date>2013-09-24T05:14:26Z</dc:date>
    <item>
      <title>eMMC support for iMX6 Linux BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-support-for-iMX6-Linux-BSP/m-p/254371#M23993</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt; Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am a newbie in iMX platform.&lt;/P&gt;&lt;P&gt;I would like to know about the availability of eMMC NAND flash support in iMX6 BSP.&lt;/P&gt;&lt;P&gt;As per the i.MX_6Dual6Quad_Linux_Reference_Manual.pdf, the MMC Linux driver supports eMMC4.4 SDR and DDR modes.&lt;/P&gt;&lt;P&gt;Does it mean eMMC is supported in accessing NAND flash also?&lt;/P&gt;&lt;P&gt;As per Micron technical document e·MMC Linux Enablement, I understood that a platform specific host layer is needed&lt;/P&gt;&lt;P&gt;in the Linux kernel. Is this layer supported for iMX6 platform controllers in iMX6 BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Honey S&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Aug 2013 13:00:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-support-for-iMX6-Linux-BSP/m-p/254371#M23993</guid>
      <dc:creator>honeysukesan</dc:creator>
      <dc:date>2013-08-14T13:00:54Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC support for iMX6 Linux BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-support-for-iMX6-Linux-BSP/m-p/254372#M23994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone please put a reply to this post?&lt;/P&gt;&lt;P&gt;I am waiting for your reply. It's so urgent. please..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Honey S&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Aug 2013 06:02:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-support-for-iMX6-Linux-BSP/m-p/254372#M23994</guid>
      <dc:creator>honeysukesan</dc:creator>
      <dc:date>2013-08-16T06:02:28Z</dc:date>
    </item>
    <item>
      <title>Re: eMMC support for iMX6 Linux BSP</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/eMMC-support-for-iMX6-Linux-BSP/m-p/254373#M23995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Honey,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you are conused with eMMC and NAND. Usually, eMMC means NAND flash with controller including ECC and it is&amp;nbsp; connected thru SDHC. But NAND, usually it is refered as 'raw NAND', is pure NAND device which can be connected GPMI I/F of i.MX6. And our internal BCH block can be used for its operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;eMMC can be connected thru uSDHC I/F and it is supported by our BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Sep 2013 05:14:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/eMMC-support-for-iMX6-Linux-BSP/m-p/254373#M23995</guid>
      <dc:creator>Paul_Kang</dc:creator>
      <dc:date>2013-09-24T05:14:26Z</dc:date>
    </item>
  </channel>
</rss>