<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックIMX8MP Booting from ECSPI2 is inconsistent</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Booting-from-ECSPI2-is-inconsistent/m-p/2146662#M239850</link>
    <description>&lt;P&gt;Greetings,&amp;nbsp;&lt;BR /&gt;We have encountered an issue with attempting to boot from ECSPI2.&lt;BR /&gt;We changed the boot flags in the fuses to force boot from ECSPI2 (ECSPI2 is connected to a NOR Flash which is programmed with a valid boot image).&lt;/P&gt;&lt;P&gt;Booting is inconsistent, most of the times the booting will fail but occasionally it will succeeded.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To verify that this is an issue with the SOC, we switched to using the imx8mp-evb.&lt;/P&gt;&lt;P&gt;after performing the same fuse selection for the SOC on the evb we checked the spi transactions using an oscilloscope, which gave us the following findings:&lt;BR /&gt;1) The SCK dutycycle is 75% (where is should be 50% to my understanding)&amp;nbsp;&lt;BR /&gt;2) The SCK is 1.7v (where it should be 3.3v, should be identicle to MOSI which is 3.3v)&lt;/P&gt;&lt;P&gt;(These measurements are correct for the EVB and for our proprietary hardware)&lt;/P&gt;&lt;P&gt;I would greatly appreciate any help regarding this issue as it is a big issue for us!&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 05 Aug 2025 07:18:13 GMT</pubDate>
    <dc:creator>YorkerHazan</dc:creator>
    <dc:date>2025-08-05T07:18:13Z</dc:date>
    <item>
      <title>IMX8MP Booting from ECSPI2 is inconsistent</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Booting-from-ECSPI2-is-inconsistent/m-p/2146662#M239850</link>
      <description>&lt;P&gt;Greetings,&amp;nbsp;&lt;BR /&gt;We have encountered an issue with attempting to boot from ECSPI2.&lt;BR /&gt;We changed the boot flags in the fuses to force boot from ECSPI2 (ECSPI2 is connected to a NOR Flash which is programmed with a valid boot image).&lt;/P&gt;&lt;P&gt;Booting is inconsistent, most of the times the booting will fail but occasionally it will succeeded.&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To verify that this is an issue with the SOC, we switched to using the imx8mp-evb.&lt;/P&gt;&lt;P&gt;after performing the same fuse selection for the SOC on the evb we checked the spi transactions using an oscilloscope, which gave us the following findings:&lt;BR /&gt;1) The SCK dutycycle is 75% (where is should be 50% to my understanding)&amp;nbsp;&lt;BR /&gt;2) The SCK is 1.7v (where it should be 3.3v, should be identicle to MOSI which is 3.3v)&lt;/P&gt;&lt;P&gt;(These measurements are correct for the EVB and for our proprietary hardware)&lt;/P&gt;&lt;P&gt;I would greatly appreciate any help regarding this issue as it is a big issue for us!&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Aug 2025 07:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Booting-from-ECSPI2-is-inconsistent/m-p/2146662#M239850</guid>
      <dc:creator>YorkerHazan</dc:creator>
      <dc:date>2025-08-05T07:18:13Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MP Booting from ECSPI2 is inconsistent</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Booting-from-ECSPI2-is-inconsistent/m-p/2147228#M239874</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249033"&gt;@YorkerHazan&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Booting is inconsistent, most of the times the booting will fail but occasionally it will succeeded.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;gt;&amp;gt;&amp;gt;please check your hardware connection. It seems your HW connection error.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Wed, 06 Aug 2025 03:02:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MP-Booting-from-ECSPI2-is-inconsistent/m-p/2147228#M239874</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-08-06T03:02:54Z</dc:date>
    </item>
  </channel>
</rss>