<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8M Plus CPU current frequency dynamic running</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CPU-current-frequency-dynamic-running/m-p/2145767#M239801</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253341"&gt;@Maotom&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Scaling governors are used in the Linux kernel to set the CPU frequency. CPU frequencies can be scaled&lt;BR /&gt;automatically depending on the system load either in response to ACPI events or manually by userspace&lt;BR /&gt;programs. For more information about governors, read governors.txt from &lt;A href="http://www.kernel.org/doc/Documentation/" target="_blank"&gt;www.kernel.org/doc/Documentation/&lt;/A&gt;&lt;BR /&gt;cpu-freq/governors.txt.&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
    <pubDate>Mon, 04 Aug 2025 02:40:47 GMT</pubDate>
    <dc:creator>pengyong_zhang</dc:creator>
    <dc:date>2025-08-04T02:40:47Z</dc:date>
    <item>
      <title>i.MX8M Plus CPU current frequency dynamic running</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CPU-current-frequency-dynamic-running/m-p/2144816#M239757</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;The script can check i.MX8M plus current running frequency by "&amp;nbsp;sudo cat /sys/devices/system/cpu/cpu0/cpufreq/cpuinfo_cur_freq". There are 3 kinds available freqencey&amp;nbsp; 1200000, 160000&amp;nbsp; and 1800000 shown by command "cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_available_frequencies". After check current frequency second by second found the CPU frequency run between&amp;nbsp; 1600000 and 1800000&amp;nbsp;&lt;/P&gt;&lt;P&gt;2025-Aug-01_09:27:17 CPU 52000&lt;BR /&gt;1600000&lt;BR /&gt;2025-Aug-01_09:27:18 CPU 52000&lt;BR /&gt;1600000&lt;BR /&gt;2025-Aug-01_09:27:19 CPU 52000&lt;BR /&gt;1600000&lt;BR /&gt;2025-Aug-01_09:27:20 CPU 52000&lt;BR /&gt;1800000&lt;BR /&gt;2025-Aug-01_09:27:21 CPU 52000&lt;BR /&gt;1800000&lt;/P&gt;&lt;P&gt;What is the policy for CPU frequency dynamic running?&lt;/P&gt;&lt;P&gt;&lt;LI-PRODUCT title="i.MX8M" id="i.MX8M"&gt;&lt;/LI-PRODUCT&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Aug 2025 01:34:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CPU-current-frequency-dynamic-running/m-p/2144816#M239757</guid>
      <dc:creator>Maotom</dc:creator>
      <dc:date>2025-08-01T01:34:06Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Plus CPU current frequency dynamic running</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CPU-current-frequency-dynamic-running/m-p/2145767#M239801</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/253341"&gt;@Maotom&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Scaling governors are used in the Linux kernel to set the CPU frequency. CPU frequencies can be scaled&lt;BR /&gt;automatically depending on the system load either in response to ACPI events or manually by userspace&lt;BR /&gt;programs. For more information about governors, read governors.txt from &lt;A href="http://www.kernel.org/doc/Documentation/" target="_blank"&gt;www.kernel.org/doc/Documentation/&lt;/A&gt;&lt;BR /&gt;cpu-freq/governors.txt.&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Mon, 04 Aug 2025 02:40:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CPU-current-frequency-dynamic-running/m-p/2145767#M239801</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-08-04T02:40:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Plus CPU current frequency dynamic running</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CPU-current-frequency-dynamic-running/m-p/2149046#M239972</link>
      <description />
      <pubDate>Fri, 08 Aug 2025 08:42:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CPU-current-frequency-dynamic-running/m-p/2149046#M239972</guid>
      <dc:creator>Maotom</dc:creator>
      <dc:date>2025-08-08T08:42:36Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8M Plus CPU current frequency dynamic running</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CPU-current-frequency-dynamic-running/m-p/2149047#M239973</link>
      <description>Got it,Thanks</description>
      <pubDate>Fri, 08 Aug 2025 08:43:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8M-Plus-CPU-current-frequency-dynamic-running/m-p/2149047#M239973</guid>
      <dc:creator>Maotom</dc:creator>
      <dc:date>2025-08-08T08:43:28Z</dc:date>
    </item>
  </channel>
</rss>