<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: RT1176 issue from errata ERR011377</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-issue-from-errata-ERR011377/m-p/2145234#M239780</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The ERR011377 is more like FlexSPI: FlexSPI DLL lock status bit not accurate due to timing&lt;BR /&gt;issue and has nothing to do with your problem.&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;While the flash is being written or deleted, it must not be accessed in any other way. &lt;/SPAN&gt;&lt;SPAN class=""&gt;In particular, this means no code execution. &lt;/SPAN&gt;&lt;SPAN class=""&gt;Executing the FlexSPI code from the RAM is a good idea, but don't forget the constants from the '.rodata' section, which is also located in the flash. &lt;/SPAN&gt;&lt;SPAN class=""&gt;However, no other code may be executed, especially interrupts can cause problems. please check it:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-Debugging-custom-FlexSPI-Configuration-Block/td-p/1528009" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-Debugging-custom-FlexSPI-Configuration-Block/td-p/1528009&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 01 Aug 2025 14:27:13 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2025-08-01T14:27:13Z</dc:date>
    <item>
      <title>RT1176 issue from errata ERR011377</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-issue-from-errata-ERR011377/m-p/2145213#M239776</link>
      <description>&lt;P&gt;there is a problem with starting rt1176 with flash memory connected to flexSPI1.&amp;nbsp;At a memory speed of 60 MHz the device starts up, if higher then due to incorrect memory reading the device does not start up.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;-the question is how to make sure that this is because of the ERR011377 problem?&lt;/P&gt;&lt;P&gt;-is it possible to solve this problem if the main program code is on flash flexSPI1?&lt;/P&gt;&lt;P&gt;-were there any changes in the revisions of this MCU?&amp;nbsp;If yes, can I order several samples?&lt;/P&gt;</description>
      <pubDate>Fri, 01 Aug 2025 13:35:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-issue-from-errata-ERR011377/m-p/2145213#M239776</guid>
      <dc:creator>_And_</dc:creator>
      <dc:date>2025-08-01T13:35:28Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 issue from errata ERR011377</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-issue-from-errata-ERR011377/m-p/2145234#M239780</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;The ERR011377 is more like FlexSPI: FlexSPI DLL lock status bit not accurate due to timing&lt;BR /&gt;issue and has nothing to do with your problem.&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;While the flash is being written or deleted, it must not be accessed in any other way. &lt;/SPAN&gt;&lt;SPAN class=""&gt;In particular, this means no code execution. &lt;/SPAN&gt;&lt;SPAN class=""&gt;Executing the FlexSPI code from the RAM is a good idea, but don't forget the constants from the '.rodata' section, which is also located in the flash. &lt;/SPAN&gt;&lt;SPAN class=""&gt;However, no other code may be executed, especially interrupts can cause problems. please check it:&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-Debugging-custom-FlexSPI-Configuration-Block/td-p/1528009" target="_blank"&gt;https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1176-Debugging-custom-FlexSPI-Configuration-Block/td-p/1528009&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class=""&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 01 Aug 2025 14:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-issue-from-errata-ERR011377/m-p/2145234#M239780</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-08-01T14:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: RT1176 issue from errata ERR011377</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1176-issue-from-errata-ERR011377/m-p/2146110#M239819</link>
      <description>&lt;P&gt;I'm not sure we understand each other correctly. I now have the following configuration:&lt;BR /&gt;- Boot Mode 10 - internal boot&lt;BR /&gt;- Boot config - FlashSPI1 - Serial NOR (QSPI Flash)&lt;/P&gt;&lt;P&gt;the device does not work because the program does not start from flash memory when the memory speed is higher than 60 MHZ, the data starts to be read incorrectly (technically the data is read, but when reading at a higher speed there is a shift of 4-12 bits and the device does not work).&lt;/P&gt;&lt;P&gt;what are the possible reasons for the incorrect reading? And would like to receive confirmation or denial regarding the impact of ERR011377 in this situation&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 04 Aug 2025 09:55:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1176-issue-from-errata-ERR011377/m-p/2146110#M239819</guid>
      <dc:creator>_And_</dc:creator>
      <dc:date>2025-08-04T09:55:03Z</dc:date>
    </item>
  </channel>
</rss>