<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2143931#M239709</link>
    <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228214"&gt;@Ram2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well!&lt;/P&gt;
&lt;P&gt;According to your description, you have 2 requirements:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;SPAN&gt;SD-WLAN-UART-BT-IW611-LNX_6_12_20-IMX8-18.99.3.p25.10-18.99.3.p25.10-MM6X18537.p15-GPL&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN&gt;wpa_supplicant 2.12&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;There are 2 methods for you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;1. Using&amp;nbsp; LF6.6.3_1.0.0 bsp&amp;nbsp; for Yocto Project 4.3 (Nanbield)&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In the bsp, WiFi driver version is :&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;• BSP version: Linux 6.6.3-1.0.0&lt;BR /&gt;• Wi-Fi and Bluetooth/Bluetooth LE Firmware version: 18.99.2.p66.17&lt;BR /&gt;• Driver version: MM6X18437.p3-GPL&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;wpa_supplicant version should be v2.10&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;(1) Compile WiFi driver and wpa_supplicant 2.12 separately, and then replace the original ones in the image.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;(2) you can try to integrate them to the Yocto Version, no limitations.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;STRONG&gt;2. Using&amp;nbsp; LF6.12.20_2.0.0 bsp&amp;nbsp; for Yocto Project 5.2 (Walnascar)&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;The bsp version is the latest one, it has includes driver you want to use.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;SD-WLAN-UART-BT-IW611-LNX_6_12_20-IMX8-18.99.3.p25.10-18.99.3.p25.10-MM6X18537.p15-GPL&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But in the bsp, wpa_supplicant is v2.11,&amp;nbsp; you can try to replace it with v2.12 if you can get corresponding wpa_supplicant-2.12.bb&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;BR /&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;weidong&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Jul 2025 22:51:44 GMT</pubDate>
    <dc:creator>weidong_sun</dc:creator>
    <dc:date>2025-07-30T22:51:44Z</dc:date>
    <item>
      <title>Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2142537#M239655</link>
      <description>&lt;P&gt;Hi NXP Support Team,&lt;/P&gt;&lt;P&gt;As part of our ongoing BSP integration on the i.MX8QXP platform using the &lt;STRONG&gt;Yocto Nanbield&lt;/STRONG&gt; release, we are evaluating the below WLAN driver/firmware package and WPA supplicant version for compatibility:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;Driver-Firmware:&lt;/STRONG&gt; SD-WLAN-UART-BT-IW611-LNX_6_12_20-IMX8-18.99.3.p25.10-18.99.3.p25.10-MM6X18537.p15-GPL&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;&lt;STRONG&gt;WPA Supplicant Version:&lt;/STRONG&gt; wpa_supplicant_2.12&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;We would like your guidance on the following:&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;Are the above versions officially compatible with the &lt;STRONG&gt;Yocto Nanbield&lt;/STRONG&gt; release (and its respective kernel version)?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Are there any known limitations or regressions if we integrate this driver/firmware and wpa_supplicant_2.12 into Nanbield?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Are there any preferred or recommended versions of the WLAN driver/firmware and WPA supplicant specifically validated for Nanbield?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Please let us know if additional testing or patches are required when using these versions in the Nanbield environment.&lt;/P&gt;&lt;P&gt;Looking forward to your confirmation and guidance&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jul 2025 08:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2142537#M239655</guid>
      <dc:creator>Ram2</dc:creator>
      <dc:date>2025-07-29T08:49:36Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2142573#M239658</link>
      <description>&lt;P&gt;Which linux BSP version are you using? For the i.MX8QXP board you using the board you design yourself or the NXP board? Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jul 2025 09:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2142573#M239658</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-07-29T09:22:04Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2142580#M239659</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57740"&gt;@Rita_Wang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BSP Version : L6.6.3&amp;nbsp;&lt;BR /&gt;Yocto : Nanbield&lt;BR /&gt;iMX8QXP :&amp;nbsp; Is NXP but its custom board its a designed target&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jul 2025 09:25:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2142580#M239659</guid>
      <dc:creator>Ram2</dc:creator>
      <dc:date>2025-07-29T09:25:15Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2142593#M239660</link>
      <description>&lt;P&gt;I will help confirm it.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Jul 2025 09:38:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2142593#M239660</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-07-29T09:38:02Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2143366#M239690</link>
      <description>&lt;P&gt;I help creat case&amp;nbsp;&lt;SPAN&gt;00724744 to our Wifi team engineer, they will give you update there as soon as possible.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jul 2025 08:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2143366#M239690</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-07-30T08:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2143931#M239709</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228214"&gt;@Ram2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well!&lt;/P&gt;
&lt;P&gt;According to your description, you have 2 requirements:&lt;/P&gt;
&lt;UL&gt;
&lt;LI&gt;&lt;SPAN&gt;SD-WLAN-UART-BT-IW611-LNX_6_12_20-IMX8-18.99.3.p25.10-18.99.3.p25.10-MM6X18537.p15-GPL&lt;/SPAN&gt;&lt;/LI&gt;
&lt;LI&gt;&lt;SPAN&gt;wpa_supplicant 2.12&lt;/SPAN&gt;&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;There are 2 methods for you.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;1. Using&amp;nbsp; LF6.6.3_1.0.0 bsp&amp;nbsp; for Yocto Project 4.3 (Nanbield)&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In the bsp, WiFi driver version is :&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;• BSP version: Linux 6.6.3-1.0.0&lt;BR /&gt;• Wi-Fi and Bluetooth/Bluetooth LE Firmware version: 18.99.2.p66.17&lt;BR /&gt;• Driver version: MM6X18437.p3-GPL&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;wpa_supplicant version should be v2.10&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;(1) Compile WiFi driver and wpa_supplicant 2.12 separately, and then replace the original ones in the image.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;(2) you can try to integrate them to the Yocto Version, no limitations.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;STRONG&gt;2. Using&amp;nbsp; LF6.12.20_2.0.0 bsp&amp;nbsp; for Yocto Project 5.2 (Walnascar)&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;The bsp version is the latest one, it has includes driver you want to use.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;SD-WLAN-UART-BT-IW611-LNX_6_12_20-IMX8-18.99.3.p25.10-18.99.3.p25.10-MM6X18537.p15-GPL&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But in the bsp, wpa_supplicant is v2.11,&amp;nbsp; you can try to replace it with v2.12 if you can get corresponding wpa_supplicant-2.12.bb&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Thanks!&lt;BR /&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;weidong&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jul 2025 22:51:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2143931#M239709</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2025-07-30T22:51:44Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2147665#M239902</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26366"&gt;@weidong_sun&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;We have cloned&amp;nbsp;&lt;STRONG&gt;. Using&amp;nbsp; LF6.12.20_2.0.0 bsp&amp;nbsp; for Yocto Project 5.2 (Walnascar)&lt;/STRONG&gt;&lt;BR /&gt;But didnt find the rite path where exactly the nxp wifi recipe in latest one&lt;BR /&gt;&lt;BR /&gt;2. we have tried to implement bbappend as well on top of existing the 6.6.3 but still its picking older moal.ko and mlan.ko due to packages , since its getting updated with latest .ko&lt;BR /&gt;&lt;BR /&gt;Could you please provide integration yocto recipe steps for it or helpful inputs from your end so we can acheive to integrate it&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Aug 2025 13:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2147665#M239902</guid>
      <dc:creator>Ram2</dc:creator>
      <dc:date>2025-08-06T13:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2147931#M239918</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228214"&gt;@Ram2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;See the .bb file in yocoto source folder.&lt;/P&gt;
&lt;P&gt;# cd source&lt;/P&gt;
&lt;P&gt;./meta-freescale/recipes-kernel/kernel-modules/kernel-module-nxp-wlan_git.bb&lt;/P&gt;
&lt;P&gt;......&lt;/P&gt;
&lt;P&gt;SRCBRANCH = "lf-6.6.52_2.2.0"&lt;BR /&gt;MRVL_SRC ?= "git://github.com/nxp-imx/mwifiex.git;protocol=https"&lt;/P&gt;
&lt;P&gt;......&lt;/P&gt;
&lt;P&gt;The driver is patched based on the version for&amp;nbsp;lf-6.6.52_2.2.0. and then verified on L6.12.20 kernel.&lt;/P&gt;
&lt;P&gt;For your application,&amp;nbsp;LF6.12.20_2.0.0 bsp is no problem,&amp;nbsp; no need to focus on it, in the latest Linux bsp, always the latest Wi-Fi driver version is supported.&lt;/P&gt;
&lt;P&gt;As for wpa_supplicant-2.11 or wpa_supplicant-2.12, I think both are OK, but&amp;nbsp;wpa_supplicant-2.11 has been ready in default bsp, no need to change it to ver 2.12. Just my personal opinion for you.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;EM&gt;&lt;STRONG&gt;&amp;gt;&amp;gt;we have tried to implement bbappend as well on top of existing the 6.6.3 but still its picking older moal.ko and mlan.ko due to packages , since its getting updated with latest .ko&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;
&lt;P&gt;Actually you can also build the latest Wi-Fi driver independently, get 2 .ko files , then replace old 2 .ko files, the method is more flexible.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Aug 2025 01:35:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2147931#M239918</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2025-08-07T01:35:30Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2149490#M240005</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26366"&gt;@weidong_sun&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for reply&lt;BR /&gt;&lt;BR /&gt;Just wanted to inform that I have followed as you informed&lt;BR /&gt;Cloned separetely driver and generated driver .ko files and replaced in target&lt;BR /&gt;when I reboot I see kernel panic I m not sure why its is can you please help me with flow to proceed further&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wifi-crash-logs-1.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/351644iF9468C799C5C591D/image-size/large?v=v2&amp;amp;px=999" role="button" title="wifi-crash-logs-1.png" alt="wifi-crash-logs-1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wifi-crash-3.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/351646i8F6F7D6EA1035139/image-size/large?v=v2&amp;amp;px=999" role="button" title="wifi-crash-3.png" alt="wifi-crash-3.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="wifi-crash-2.png" style="width: 999px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/351645i326937DEE6DC01D0/image-size/large?v=v2&amp;amp;px=999" role="button" title="wifi-crash-2.png" alt="wifi-crash-2.png" /&gt;&lt;/span&gt;&lt;BR /&gt;Do you see any dependecny&lt;BR /&gt;1. My work around was just generatred .ko files first and instead of building in yocto&lt;BR /&gt;2. First I have done scp to target to replaced with latest .ko files&amp;nbsp;&lt;BR /&gt;i.e under&amp;nbsp;&lt;SPAN&gt;&lt;STRONG&gt;cp -rf moal.ko /usr/lib/modules/6.6.3-lts-next-gd4e47fe015ab/updates/&amp;nbsp;&lt;/STRONG&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &lt;STRONG&gt;cp -rf mlan.ko /usr/lib/modules/6.6.3-lts-next-gd4e47fe015ab/updates/&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp;&lt;BR /&gt;Please find the logs pasted&lt;BR /&gt;&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 09 Aug 2025 10:36:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2149490#M240005</guid>
      <dc:creator>Ram2</dc:creator>
      <dc:date>2025-08-09T10:36:31Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2149694#M240016</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228214"&gt;@Ram2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Follow the steps below to make a test, please!&lt;/P&gt;
&lt;P&gt;===========================&lt;/P&gt;
&lt;P&gt;1. Building default Yocto bsp to create images for you board.&lt;/P&gt;
&lt;P&gt;2.. Downloading images you built and starting your board.&lt;/P&gt;
&lt;P&gt;3.. Building the&amp;nbsp; wifi driver you want to use.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;-- Kernel directory should be like this:&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;tmp/work/imx8mm_ddr4_evk-poky-linux/linux-imx/6.6.52+git/build&lt;/P&gt;
&lt;P&gt;##export KERNELDIR= ....(absolute path)...&amp;nbsp; input it using your pat&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;--Setting cross compilation environment, should be like this:&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;# source&amp;nbsp;/opt/fsl-imx-wayland/6.6-nanbield/environment-setup-armv8a-poky-linux&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;[Note]&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;Toolchain should be the one you exported from yocto source&amp;nbsp; (populate_sdk), it menas you your image&amp;nbsp; and wifi driver must be built using the same cross compiler.&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;--Copying mlan.ko &amp;amp; moal.ko after building wifi driver to your board home directory.&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;&lt;STRONG&gt;--Copying &lt;FONT color="#FF0000"&gt;&lt;EM&gt;companion firmware&lt;/EM&gt;&lt;/FONT&gt; of the version of wifi driver to board (/lib/firmware/nxp)&lt;/STRONG&gt;&lt;/P&gt;
&lt;P&gt;4.. Loading Wi-Fi driver on your board.&lt;/P&gt;
&lt;P&gt;# cd ~/&lt;/P&gt;
&lt;P&gt;# insmod mlan.ko&lt;/P&gt;
&lt;P&gt;# insmod moal.ko mod_para=nxp/wifi_mod_para.conf&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#FF6600"&gt;&lt;U&gt;&lt;EM&gt;&lt;STRONG&gt;Don't use modprobe command, it will load default wifi driver in image, NOT yours.&lt;/STRONG&gt;&lt;/EM&gt;&lt;/U&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;===========================&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Try it, please!&lt;BR /&gt;Thanks!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 11 Aug 2025 04:13:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2149694#M240016</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2025-08-11T04:13:23Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2162043#M240461</link>
      <description>&lt;P&gt;Dear NXP Team,&lt;/P&gt;&lt;P&gt;As per your suggestion, we have been following the recommended steps to rebuild and load the NXP Wi-Fi driver mlan.ko, moal.ko against the Yocto BSP kernel. On our local builds the process works correctly — the .ko modules load without error when inserted using insmod.&lt;/P&gt;&lt;P&gt;However, when the same procedure is executed in our CI pipeline (different build host), we observe a mismatch in the kernel release string (uname -r) and the vermagic embedded in the .ko files.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Local build (working):&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;uname -r: &lt;STRONG&gt;kernel-module-mlan-6.6.3-lts-next-gd4e47fe015ab_git-r0_arm64.deb&lt;/STRONG&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;but your layer is producing:&lt;BR /&gt;vermagic (mlan/moal): &lt;STRONG&gt;kernel-module-mlan-6.6.3-lts-next-gd4e47fe015ab_git-r0_arm64.deb&lt;/STRONG&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Modules load correctly.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;CI build (failing):&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;uname -r: 6.6.3-lts-next-g88dffeae470f&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;vermagic (mlan/moal):&amp;nbsp;&lt;STRONG&gt;kernel-module-mlan-6.6.3-lts-next-g&amp;lt;hash&amp;gt;_1.0-r0_arm64.deb&lt;/STRONG&gt;&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;insmod fails with Unknown symbol errors.&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Root cause: the kernel in CI has CONFIG_LOCALVERSION_AUTO=y, which appends a git hash (-g88dffeae470f) to the release string, while our Wi-Fi driver is compiled expecting a fixed localversion.&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Because of this difference, the same Wi-Fi driver sources behave differently across local and CI builds.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Our questions:&lt;/STRONG&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;P&gt;What is the recommended way from NXP side to ensure a &lt;STRONG&gt;consistent kernel release string&lt;/STRONG&gt; between BSP kernel and external Wi-Fi modules (across different build environments)?&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Should we always fix CONFIG_LOCALVERSION and disable CONFIG_LOCALVERSION_AUTO?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Or is there an alternate NXP-recommended approach to build out-of-tree Wi-Fi modules in a reproducible way?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;The moal.ko driver also reports missing PM/QoS symbols when built against the CI kernel (e.g., cpu_latency_qos_add_request, device_wakeup_enable). Locally we enabled CONFIG_PM, CONFIG_PM_SLEEP, CONFIG_PM_RUNTIME, and CONFIG_PM_QOS, which resolves the issue. Could you please confirm if these kernel options are mandatory for moal?&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;We would like to stabilize this build process so the Wi-Fi driver works reliably across both local development and CI builds. Please guide us on the best practice to align kernel build config and Wi-Fi driver integration.&lt;BR /&gt;&lt;BR /&gt;Error we are facing like :&lt;BR /&gt;&lt;STRONG&gt;mlan: disagrees about version of symbol module_layout&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;moal: disagrees about version of symbol module_layout&lt;BR /&gt;&lt;BR /&gt;&lt;/STRONG&gt;Please help us to unblock asap&amp;nbsp;&lt;BR /&gt;Since it is a blocker&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 02 Sep 2025 09:40:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2162043#M240461</guid>
      <dc:creator>Ram2</dc:creator>
      <dc:date>2025-09-02T09:40:16Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2162465#M240487</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/26366"&gt;@weidong_sun&lt;/a&gt;&amp;nbsp;Could you help check again, for the update from customer, great thanks~~&lt;/P&gt;</description>
      <pubDate>Wed, 03 Sep 2025 02:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2162465#M240487</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-09-03T02:14:48Z</dc:date>
    </item>
    <item>
      <title>Re: Compatibility Check for IW611 WLAN Driver/Firmware and WPA Supplicant 2.12 with Yocto Nanbield</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2162517#M240489</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228214"&gt;@Ram2&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;This is a very common problem, and can usually be addressed as follows:&lt;BR /&gt;1. Disable CONFIG_LOCALVERSION_AUTO in CI&lt;BR /&gt;CONFIG_LOCALVERSION_AUTO=n&lt;BR /&gt;2. Set a fixed CONFIG_LOCALVERSION&lt;BR /&gt;CONFIG_LOCALVERSION="-gd4e47fe015ab_git-r0"&lt;BR /&gt;[Note]&lt;BR /&gt;This can be done by:&lt;BR /&gt;Editing defconfig or .config directly.&lt;BR /&gt;Or appending to your Yocto kernel recipe:&lt;BR /&gt;KERNEL_LOCALVERSION = "-gd4e47fe015ab_git-r0"&lt;BR /&gt;3. Using the same .config for kernel configuration (Local &amp;amp; CI)&lt;BR /&gt;OR&lt;BR /&gt;4. Copying your local_config (.config) to Yocto on the CI side, and in Yocto like this:&lt;/P&gt;
&lt;P&gt;SRC_URI += "file://local_config"&lt;BR /&gt;do_configure_prepend() {&lt;BR /&gt;cp ${WORKDIR}/local_config ${S}/.config&lt;/P&gt;
&lt;P&gt;OR&lt;BR /&gt;5. Using the same kernel source on both local and CI sides&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;We do not officially provide a standard method.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks!&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;weidong&lt;/P&gt;</description>
      <pubDate>Wed, 03 Sep 2025 03:20:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Compatibility-Check-for-IW611-WLAN-Driver-Firmware-and-WPA/m-p/2162517#M240489</guid>
      <dc:creator>weidong_sun</dc:creator>
      <dc:date>2025-09-03T03:20:38Z</dc:date>
    </item>
  </channel>
</rss>