<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem With Kernel Driver Compiled-In Data (mcx/gpu-viv) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Problem-With-Kernel-Driver-Compiled-In-Data-mcx-gpu-viv/m-p/2143651#M239704</link>
    <description>&lt;P&gt;This isn't so much a question as a hope for future Kernel upgrades.&amp;nbsp;&lt;BR /&gt;As a matter of policy, we don't like to have any identifying information written into the Kernel.&amp;nbsp;&lt;BR /&gt;There is a useful build&amp;nbsp;option KBUILD_BUILD_HOST, that can be applied to give a build host name of our choosing.&lt;BR /&gt;Scans through the binaries of our Kernel and module builds have shown that the mxc/gpu-viv portion of the source generates its own HOST variable instead of using the kernel option.&lt;BR /&gt;I know that the entire kernel source package is huge and that resources are minimal for things that are working/mature, however I was hoping that this "feature" could be perhaps modified in the Kbuild to use KBUILD_BUILD_HOST or simply removed.&lt;BR /&gt;For me it is extremely hard to really say what the value of the building host name has to the driver. Its only used here&amp;nbsp;mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_device.c .&lt;/P&gt;</description>
    <pubDate>Wed, 30 Jul 2025 15:16:57 GMT</pubDate>
    <dc:creator>A_Guyula</dc:creator>
    <dc:date>2025-07-30T15:16:57Z</dc:date>
    <item>
      <title>Problem With Kernel Driver Compiled-In Data (mcx/gpu-viv)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-With-Kernel-Driver-Compiled-In-Data-mcx-gpu-viv/m-p/2143651#M239704</link>
      <description>&lt;P&gt;This isn't so much a question as a hope for future Kernel upgrades.&amp;nbsp;&lt;BR /&gt;As a matter of policy, we don't like to have any identifying information written into the Kernel.&amp;nbsp;&lt;BR /&gt;There is a useful build&amp;nbsp;option KBUILD_BUILD_HOST, that can be applied to give a build host name of our choosing.&lt;BR /&gt;Scans through the binaries of our Kernel and module builds have shown that the mxc/gpu-viv portion of the source generates its own HOST variable instead of using the kernel option.&lt;BR /&gt;I know that the entire kernel source package is huge and that resources are minimal for things that are working/mature, however I was hoping that this "feature" could be perhaps modified in the Kbuild to use KBUILD_BUILD_HOST or simply removed.&lt;BR /&gt;For me it is extremely hard to really say what the value of the building host name has to the driver. Its only used here&amp;nbsp;mxc/gpu-viv/hal/os/linux/kernel/gc_hal_kernel_device.c .&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jul 2025 15:16:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-With-Kernel-Driver-Compiled-In-Data-mcx-gpu-viv/m-p/2143651#M239704</guid>
      <dc:creator>A_Guyula</dc:creator>
      <dc:date>2025-07-30T15:16:57Z</dc:date>
    </item>
    <item>
      <title>Re: Problem With Kernel Driver Compiled-In Data (mcx/gpu-viv)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Problem-With-Kernel-Driver-Compiled-In-Data-mcx-gpu-viv/m-p/2144713#M239754</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Thank you for your comments, will take it and share it with software team for evaluation.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Thu, 31 Jul 2025 19:03:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Problem-With-Kernel-Driver-Compiled-In-Data-mcx-gpu-viv/m-p/2144713#M239754</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-07-31T19:03:16Z</dc:date>
    </item>
  </channel>
</rss>