<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: ENGcm04758 ARM: Incorrect L2 cache eviction can occur when L2 is configured as an inner cache</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ENGcm04758-ARM-Incorrect-L2-cache-eviction-can-occur-when-L2-is/m-p/2143590#M239702</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes is the u-boot-2009.01 version&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Wed, 30 Jul 2025 13:49:50 GMT</pubDate>
    <dc:creator>Bio_TICFSL</dc:creator>
    <dc:date>2025-07-30T13:49:50Z</dc:date>
    <item>
      <title>ENGcm04758 ARM: Incorrect L2 cache eviction can occur when L2 is configured as an inner cache</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ENGcm04758-ARM-Incorrect-L2-cache-eviction-can-occur-when-L2-is/m-p/2143379#M239692</link>
      <description>&lt;P&gt;hi, I m trying to find the commit that does this::&lt;/P&gt;&lt;P&gt;&lt;EM&gt;&amp;nbsp;The software workaround is to disable write allocate in the Level 2 cache in the bootloader. So no&lt;/EM&gt;&lt;BR /&gt;&lt;EM&gt;condition is to trigger this issue. This workaround has performance penalty.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In the &lt;A href="https://github.com/nxp-imx/uboot-imx.git" target="_blank"&gt;https://github.com/nxp-imx/uboot-imx.git&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;thank you,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Mattias&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jul 2025 08:46:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ENGcm04758-ARM-Incorrect-L2-cache-eviction-can-occur-when-L2-is/m-p/2143379#M239692</guid>
      <dc:creator>MattiasBarthel1</dc:creator>
      <dc:date>2025-07-30T08:46:09Z</dc:date>
    </item>
    <item>
      <title>Re: ENGcm04758 ARM: Incorrect L2 cache eviction can occur when L2 is configured as an inner cache</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ENGcm04758-ARM-Incorrect-L2-cache-eviction-can-occur-when-L2-is/m-p/2143590#M239702</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes is the u-boot-2009.01 version&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jul 2025 13:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ENGcm04758-ARM-Incorrect-L2-cache-eviction-can-occur-when-L2-is/m-p/2143590#M239702</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-07-30T13:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: ENGcm04758 ARM: Incorrect L2 cache eviction can occur when L2 is configured as an inner cache</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ENGcm04758-ARM-Incorrect-L2-cache-eviction-can-occur-when-L2-is/m-p/2143644#M239703</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/34846"&gt;@Bio_TICFSL&lt;/a&gt;&amp;nbsp; thanks for your reply.&lt;BR /&gt;&lt;BR /&gt;Could you specify the exact commit from that tag, please?&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mattias&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jul 2025 15:04:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ENGcm04758-ARM-Incorrect-L2-cache-eviction-can-occur-when-L2-is/m-p/2143644#M239703</guid>
      <dc:creator>MattiasBarthel1</dc:creator>
      <dc:date>2025-07-30T15:04:47Z</dc:date>
    </item>
    <item>
      <title>Re: ENGcm04758 ARM: Incorrect L2 cache eviction can occur when L2 is configured as an inner cache</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ENGcm04758-ARM-Incorrect-L2-cache-eviction-can-occur-when-L2-is/m-p/2144481#M239742</link>
      <description>&lt;P&gt;I guess I have found it.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;commit 64fdf452a85718935d82416d141be144b262c542
Author: Stefano Babic &amp;lt;sbabic@denx.de&amp;gt;
Date: Wed Jan 20 18:19:32 2010 +0100

MX51: Add initial support for the Freescale MX51

The patch add initial support for the Freescale i.MX51 processor
(family arm cortex_a8).&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 31 Jul 2025 10:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ENGcm04758-ARM-Incorrect-L2-cache-eviction-can-occur-when-L2-is/m-p/2144481#M239742</guid>
      <dc:creator>MattiasBarthel1</dc:creator>
      <dc:date>2025-07-31T10:21:26Z</dc:date>
    </item>
  </channel>
</rss>