<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Secure Memory and Blob usage in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Memory-and-Blob-usage/m-p/2143373#M239691</link>
    <description>&lt;P&gt;Hey, is it possible to use the the secure memory and/or blobs from CAAM while not using the&amp;nbsp;i.MX BSP?&lt;/P&gt;&lt;PRE&gt;/dev/caam-keygen&lt;/PRE&gt;&lt;P&gt;cant get the driver for this.&lt;BR /&gt;Also using bitbake virtual/kernel -c menuconfig, there isnt an option to enable&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;CONFIG_CRYPTO_DEV_FSL_CAAM_SM=y&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 30 Jul 2025 08:44:24 GMT</pubDate>
    <dc:creator>Melonman1809</dc:creator>
    <dc:date>2025-07-30T08:44:24Z</dc:date>
    <item>
      <title>Secure Memory and Blob usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Memory-and-Blob-usage/m-p/2143373#M239691</link>
      <description>&lt;P&gt;Hey, is it possible to use the the secure memory and/or blobs from CAAM while not using the&amp;nbsp;i.MX BSP?&lt;/P&gt;&lt;PRE&gt;/dev/caam-keygen&lt;/PRE&gt;&lt;P&gt;cant get the driver for this.&lt;BR /&gt;Also using bitbake virtual/kernel -c menuconfig, there isnt an option to enable&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;CONFIG_CRYPTO_DEV_FSL_CAAM_SM=y&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 30 Jul 2025 08:44:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Memory-and-Blob-usage/m-p/2143373#M239691</guid>
      <dc:creator>Melonman1809</dc:creator>
      <dc:date>2025-07-30T08:44:24Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Memory and Blob usage</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Secure-Memory-and-Blob-usage/m-p/2146484#M239840</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;You can refer to the&amp;nbsp;&lt;A href="https://github.com/nxp-imx/keyctl_caam/tree/lf-6.12.20-2.0.0" target="_self"&gt;keyctl_caam&lt;/A&gt;&amp;nbsp;for driver. The Linux driver&amp;nbsp;&lt;A href="https://github.com/nxp-imx/linux-imx/tree/lf-6.12.y/drivers/crypto/caam" target="_self"&gt;linux-imx&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;and the Linux&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/supporting-information/LF6.12.20_2.0.0-Docs.zip" target="_self"&gt;User Guide&lt;/A&gt;&amp;nbsp;may help.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Tue, 05 Aug 2025 02:24:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Secure-Memory-and-Blob-usage/m-p/2146484#M239840</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-08-05T02:24:25Z</dc:date>
    </item>
  </channel>
</rss>