<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: tuning failed for SDR50 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/tuning-failed-for-SDR50/m-p/2141277#M239612</link>
    <description>&lt;P&gt;How about your usdhc2 hardware design? For the SD card design, for the IO power is 1.8V or 3.3V?&lt;/P&gt;</description>
    <pubDate>Mon, 28 Jul 2025 00:15:11 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2025-07-28T00:15:11Z</dc:date>
    <item>
      <title>tuning failed for SDR50</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/tuning-failed-for-SDR50/m-p/2135599#M239359</link>
      <description>&lt;P&gt;I am using an iMX8qxp on my custom board and I am experiencing tuning failed error when inserting a SDR50 SD card. This issue does not happen when I insert a SDR104 card.&lt;/P&gt;&lt;P&gt;Here is the device tree configuration&lt;/P&gt;&lt;LI-CODE lang="c"&gt;usdhc2: mmc@5b020000 {
		interrupts = &amp;lt;GIC_SPI 233 IRQ_TYPE_LEVEL_HIGH&amp;gt;;
		reg = &amp;lt;0x5b020000 0x10000&amp;gt;;
		clocks = &amp;lt;&amp;amp;sdhc1_lpcg 1&amp;gt;,
			 &amp;lt;&amp;amp;sdhc1_lpcg 0&amp;gt;,
			 &amp;lt;&amp;amp;sdhc1_lpcg 2&amp;gt;;
		clock-names = "ipg", "per", "ahb";
		assigned-clocks = &amp;lt;&amp;amp;clk IMX_SC_R_SDHC_1 IMX_SC_PM_CLK_PER&amp;gt;;
		assigned-clock-rates = &amp;lt;200000000&amp;gt;;
		power-domains = &amp;lt;&amp;amp;pd IMX_SC_R_SDHC_1&amp;gt;;
		fsl,tuning-start-tap = &amp;lt;20&amp;gt;;
		fsl,tuning-step= &amp;lt;2&amp;gt;;
		status = "disabled";
	};

&amp;amp;usdhc2 {
	assigned-clocks = &amp;lt;&amp;amp;clk IMX_SC_R_SDHC_1 IMX_SC_PM_CLK_PER&amp;gt;;
	assigned-clock-rates = &amp;lt;200000000&amp;gt;;
	pinctrl-names = "default", "state_100mhz", "state_200mhz";
	pinctrl-0 = &amp;lt;&amp;amp;pinctrl_usdhc2&amp;gt;, &amp;lt;&amp;amp;pinctrl_usdhc2_gpio&amp;gt;;
	pinctrl-1 = &amp;lt;&amp;amp;pinctrl_usdhc2_100mhz&amp;gt;, &amp;lt;&amp;amp;pinctrl_usdhc2_gpio&amp;gt;;
	pinctrl-2 = &amp;lt;&amp;amp;pinctrl_usdhc2_200mhz&amp;gt;, &amp;lt;&amp;amp;pinctrl_usdhc2_gpio&amp;gt;;
	bus-width = &amp;lt;4&amp;gt;;
	vmmc-supply = &amp;lt;&amp;amp;reg_usdhc2_vmmc&amp;gt;;
	cd-gpios = &amp;lt;&amp;amp;lsio_gpio4 22 GPIO_ACTIVE_LOW&amp;gt;;
	wp-gpios = &amp;lt;&amp;amp;lsio_gpio4 21 GPIO_ACTIVE_HIGH&amp;gt;;
	status = "okay";
};&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am wondering if trace length has something to do with this error. This is because previously I have tried on another board also using iMX8, but the SD card slot is nearer to the processor. In this case, I did not encounter any tuning failure for both SDR50 and SDR104&lt;/P&gt;&lt;P&gt;If trace length is the issue, what parameters I can tweak? Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jul 2025 08:10:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/tuning-failed-for-SDR50/m-p/2135599#M239359</guid>
      <dc:creator>litzchee</dc:creator>
      <dc:date>2025-07-17T08:10:25Z</dc:date>
    </item>
    <item>
      <title>Re: tuning failed for SDR50</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/tuning-failed-for-SDR50/m-p/2141277#M239612</link>
      <description>&lt;P&gt;How about your usdhc2 hardware design? For the SD card design, for the IO power is 1.8V or 3.3V?&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jul 2025 00:15:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/tuning-failed-for-SDR50/m-p/2141277#M239612</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-07-28T00:15:11Z</dc:date>
    </item>
  </channel>
</rss>