<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 About i.MX8M QSPI Function</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/About-i-MX8M-QSPI-Function/m-p/2137781#M239431</link>
    <description>&lt;P&gt;I have a question about the QSPI function of i.MX8M.&lt;BR /&gt;There are two QSPI, QSPI_A and QSPI_B.&lt;BR /&gt;The reference manual states the following, but is it possible to use them with devices other than serial flash devices (for example, SPI-connected SRAM)?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tank_0-1753142283470.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348651i4C32FC9969FF016B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tank_0-1753142283470.png" alt="tank_0-1753142283470.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Or is it only possible to use it with serial flash devices?&lt;/P&gt;</description>
    <pubDate>Tue, 22 Jul 2025 00:00:45 GMT</pubDate>
    <dc:creator>tan-k</dc:creator>
    <dc:date>2025-07-22T00:00:45Z</dc:date>
    <item>
      <title>About i.MX8M QSPI Function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-i-MX8M-QSPI-Function/m-p/2137781#M239431</link>
      <description>&lt;P&gt;I have a question about the QSPI function of i.MX8M.&lt;BR /&gt;There are two QSPI, QSPI_A and QSPI_B.&lt;BR /&gt;The reference manual states the following, but is it possible to use them with devices other than serial flash devices (for example, SPI-connected SRAM)?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="tank_0-1753142283470.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/348651i4C32FC9969FF016B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="tank_0-1753142283470.png" alt="tank_0-1753142283470.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Or is it only possible to use it with serial flash devices?&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jul 2025 00:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-i-MX8M-QSPI-Function/m-p/2137781#M239431</guid>
      <dc:creator>tan-k</dc:creator>
      <dc:date>2025-07-22T00:00:45Z</dc:date>
    </item>
    <item>
      <title>Re: About i.MX8M QSPI Function</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/About-i-MX8M-QSPI-Function/m-p/2138482#M239460</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes&amp;nbsp; is possible with QSPI_B, but configure your device tree.&lt;/P&gt;
&lt;P&gt;please check the chapter 10.2.3.4. There are the Memory Map of Flash A and B in the i.MX8M RM.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 22 Jul 2025 14:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/About-i-MX8M-QSPI-Function/m-p/2138482#M239460</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-07-22T14:24:03Z</dc:date>
    </item>
  </channel>
</rss>