<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: i.mx8M mini MIPI-CSI RGB565 raw data copy to RAM</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-mini-MIPI-CSI-RGB565-raw-data-copy-to-RAM/m-p/2134528#M239300</link>
    <description>&lt;P&gt;I suggest that you can consider imx8mp or imx8mm, if you don't need ISP, you can use iMX8MM, refer to the RM,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;13.5.1.2 Features&lt;BR /&gt;• MIPI D-PHY specification V1.2 (Board Approved)&lt;BR /&gt;• Compliant to MIPI CSI2 Specification V1.3 except for C-PHY feature (Board&lt;BR /&gt;Approved)&lt;BR /&gt;• Support primary and secondary Image format&lt;BR /&gt;• YUV420, YUV420 (Legacy), YUV420 (CSPS), YUV422 of 8-bits and 10-bits&lt;BR /&gt;• RGB565, RGB666, RGB888&lt;BR /&gt;• RAW6, RAW7, RAW8, RAW10, RAW12, RAW14&lt;BR /&gt;• All of User defined Byte-based Data packet&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 16 Jul 2025 02:00:45 GMT</pubDate>
    <dc:creator>joanxie</dc:creator>
    <dc:date>2025-07-16T02:00:45Z</dc:date>
    <item>
      <title>i.mx8M mini MIPI-CSI RGB565 raw data copy to RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-mini-MIPI-CSI-RGB565-raw-data-copy-to-RAM/m-p/2134478#M239295</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are looking for an MCU/MPU that supports RGB565 16-bit MIPI-CSI.&lt;/P&gt;&lt;P&gt;Our application will require the MIPI-CSI + DMA to store the RGB565 16-bit raw data to RAM and process the raw data through our software.&lt;/P&gt;&lt;P&gt;We need to bypass the HW ISP.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can i.mx8 mini or others support our requirement?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jul 2025 23:45:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-mini-MIPI-CSI-RGB565-raw-data-copy-to-RAM/m-p/2134478#M239295</guid>
      <dc:creator>kensu</dc:creator>
      <dc:date>2025-07-15T23:45:49Z</dc:date>
    </item>
    <item>
      <title>Re: i.mx8M mini MIPI-CSI RGB565 raw data copy to RAM</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-mini-MIPI-CSI-RGB565-raw-data-copy-to-RAM/m-p/2134528#M239300</link>
      <description>&lt;P&gt;I suggest that you can consider imx8mp or imx8mm, if you don't need ISP, you can use iMX8MM, refer to the RM,&amp;nbsp;&lt;/P&gt;
&lt;P&gt;13.5.1.2 Features&lt;BR /&gt;• MIPI D-PHY specification V1.2 (Board Approved)&lt;BR /&gt;• Compliant to MIPI CSI2 Specification V1.3 except for C-PHY feature (Board&lt;BR /&gt;Approved)&lt;BR /&gt;• Support primary and secondary Image format&lt;BR /&gt;• YUV420, YUV420 (Legacy), YUV420 (CSPS), YUV422 of 8-bits and 10-bits&lt;BR /&gt;• RGB565, RGB666, RGB888&lt;BR /&gt;• RAW6, RAW7, RAW8, RAW10, RAW12, RAW14&lt;BR /&gt;• All of User defined Byte-based Data packet&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 02:00:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-mx8M-mini-MIPI-CSI-RGB565-raw-data-copy-to-RAM/m-p/2134528#M239300</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-07-16T02:00:45Z</dc:date>
    </item>
  </channel>
</rss>