<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX95 decoder performance in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX95-decoder-performance/m-p/2133680#M239274</link>
    <description>&lt;P&gt;Hello. I have a question about the performance of the i.MX95 chip.&lt;/P&gt;&lt;P&gt;We are planning to decode and output more than 16 channels of 640×480 @ 30 fps, 600 kbps video on the i.MX95.&lt;BR /&gt;(1) Is this possible, and what is the maximum number of channels it supports?&lt;/P&gt;&lt;P&gt;When we used the i.MX8QuadMax, its VPU only supported up to eight simultaneous decoders.&lt;BR /&gt;(2) Does the i.MX95 also have a fixed number of hardware decoders like the QuadMax, or is its capacity determined dynamically by overall VPU performance?&lt;/P&gt;&lt;P&gt;Also, with the i.MX8QuadMax we could only use GStreamer (no native decoder API was provided).&lt;BR /&gt;(3) Does the i.MX95 offer a dedicated decoder API, or—like the QuadMax—must it be used solely through GStreamer?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
    <pubDate>Tue, 15 Jul 2025 02:54:35 GMT</pubDate>
    <dc:creator>kim-dong-hyun</dc:creator>
    <dc:date>2025-07-15T02:54:35Z</dc:date>
    <item>
      <title>i.MX95 decoder performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX95-decoder-performance/m-p/2133680#M239274</link>
      <description>&lt;P&gt;Hello. I have a question about the performance of the i.MX95 chip.&lt;/P&gt;&lt;P&gt;We are planning to decode and output more than 16 channels of 640×480 @ 30 fps, 600 kbps video on the i.MX95.&lt;BR /&gt;(1) Is this possible, and what is the maximum number of channels it supports?&lt;/P&gt;&lt;P&gt;When we used the i.MX8QuadMax, its VPU only supported up to eight simultaneous decoders.&lt;BR /&gt;(2) Does the i.MX95 also have a fixed number of hardware decoders like the QuadMax, or is its capacity determined dynamically by overall VPU performance?&lt;/P&gt;&lt;P&gt;Also, with the i.MX8QuadMax we could only use GStreamer (no native decoder API was provided).&lt;BR /&gt;(3) Does the i.MX95 offer a dedicated decoder API, or—like the QuadMax—must it be used solely through GStreamer?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jul 2025 02:54:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX95-decoder-performance/m-p/2133680#M239274</guid>
      <dc:creator>kim-dong-hyun</dc:creator>
      <dc:date>2025-07-15T02:54:35Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX95 decoder performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX95-decoder-performance/m-p/2135301#M239339</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;For video decoding, the h264 decoder support 4k60 max &lt;STRONG&gt;or&lt;/STRONG&gt; up to 32 streams.&lt;/P&gt;
&lt;P&gt;For&amp;nbsp;&lt;SPAN&gt;VPU&amp;nbsp;&amp;nbsp;simultaneous decoders number, it's decided by maximum DDR bandwith and&amp;nbsp;maximum resolution.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;No native decoder API was provided.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Zhiming_Liu_0-1752714703441.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/347928iAB9C31D2CBC5C4D9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Zhiming_Liu_0-1752714703441.png" alt="Zhiming_Liu_0-1752714703441.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;Zhiming&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jul 2025 01:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX95-decoder-performance/m-p/2135301#M239339</guid>
      <dc:creator>Zhiming_Liu</dc:creator>
      <dc:date>2025-07-17T01:12:06Z</dc:date>
    </item>
  </channel>
</rss>