<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2132266#M239195</link>
    <description>&lt;P&gt;I'm developing a project that requires independent use of ELE (EdgeLock Enclave) security features in M33 firmware. After SDK analysis, I found:&lt;/P&gt;&lt;P&gt;Missing Files:&lt;BR /&gt;drivers/fsl_s3mu.c/.h - S3MU driver implementation&lt;BR /&gt;drivers/fsl_ele_base_api.c - ELE base API&lt;BR /&gt;boards/evkmimx9352/driver_examples/s3mu/ - S3MU examples&lt;/P&gt;&lt;P&gt;Does i.MX93 architecture support direct M33-to-ELE communication via S3MU?&lt;BR /&gt;Are there alternative approaches or technical documentation available?&lt;/P&gt;</description>
    <pubDate>Fri, 11 Jul 2025 06:53:17 GMT</pubDate>
    <dc:creator>Dennis0513</dc:creator>
    <dc:date>2025-07-11T06:53:17Z</dc:date>
    <item>
      <title>i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2132266#M239195</link>
      <description>&lt;P&gt;I'm developing a project that requires independent use of ELE (EdgeLock Enclave) security features in M33 firmware. After SDK analysis, I found:&lt;/P&gt;&lt;P&gt;Missing Files:&lt;BR /&gt;drivers/fsl_s3mu.c/.h - S3MU driver implementation&lt;BR /&gt;drivers/fsl_ele_base_api.c - ELE base API&lt;BR /&gt;boards/evkmimx9352/driver_examples/s3mu/ - S3MU examples&lt;/P&gt;&lt;P&gt;Does i.MX93 architecture support direct M33-to-ELE communication via S3MU?&lt;BR /&gt;Are there alternative approaches or technical documentation available?&lt;/P&gt;</description>
      <pubDate>Fri, 11 Jul 2025 06:53:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2132266#M239195</guid>
      <dc:creator>Dennis0513</dc:creator>
      <dc:date>2025-07-11T06:53:17Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2134091#M239290</link>
      <description>&lt;P&gt;Hope the&amp;nbsp;&lt;A href="https://github.com/nxp-mcuxpresso/mcuxsdk-examples/blob/release/25.06.00/trustzone_examples/hello_world_s/readme.md" target="_self"&gt;the examples&lt;/A&gt;&amp;nbsp;help.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jul 2025 10:11:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2134091#M239290</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-07-15T10:11:46Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2134818#M239314</link>
      <description>This example appears to be explaining a use case for TrustZone, but I am more interested in developing on the M33 core of i.MX93. I would like to develop on this firmware and utilize the ELE related security features. Is this feasible?&lt;BR /&gt;&lt;BR /&gt;Thank you.</description>
      <pubDate>Wed, 16 Jul 2025 08:36:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2134818#M239314</guid>
      <dc:creator>Dennis0513</dc:creator>
      <dc:date>2025-07-16T08:36:29Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2134903#M239319</link>
      <description>&lt;P&gt;Send you system email with demo, please check there.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Wed, 16 Jul 2025 10:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2134903#M239319</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-07-16T10:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2135528#M239356</link>
      <description>Thank you for your reply.&lt;BR /&gt;I understand that the patch files you provided are primarily intended for the M7 core of the i.MX95, but my question is focused on SoCs with only the M33 core, such as the i.MX93.&lt;BR /&gt;Is it possible to develop my custom firmware on the M33 and invoke and utilize ELE-related security features on it?&lt;BR /&gt;Thank you!&lt;BR /&gt;</description>
      <pubDate>Thu, 17 Jul 2025 07:03:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2135528#M239356</guid>
      <dc:creator>Dennis0513</dc:creator>
      <dc:date>2025-07-17T07:03:11Z</dc:date>
    </item>
    <item>
      <title>回复： i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2135565#M239357</link>
      <description>&lt;P&gt;On an SoC like the i.MX93, which has only one Cortex-M33 core, does enabling the ELE functionality conflict with custom MCU firmware development? In other words, after enabling ELE, does it lock the M33, preventing the uploading of custom MCU firmware?&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jul 2025 07:35:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2135565#M239357</guid>
      <dc:creator>Dennis0513</dc:creator>
      <dc:date>2025-07-17T07:35:16Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 M33 Firmware ELE (EdgeLock Enclave) API Support - Missing S3MU Driver</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2135634#M239362</link>
      <description>&lt;P&gt;Replied back to you in system email.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jul 2025 08:58:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-M33-Firmware-ELE-EdgeLock-Enclave-API-Support-Missing/m-p/2135634#M239362</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-07-17T08:58:28Z</dc:date>
    </item>
  </channel>
</rss>