<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックUSB start failed in Uboot</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2131388#M239156</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have flashed the i.MX8M Mini board and interrupted the boot process to access the U-Boot prompt. However, when I run the &lt;STRONG&gt;usb start&lt;/STRONG&gt; command, I receive the following output&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;u-boot=&amp;gt; usb start&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;starting USB...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Bus usb@32e40000: Port not available.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Bus usb@32e50000: Port not available.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;It seems that the USB ports are not being detected or initialized correctly in U-Boot. I need to access USB functionality from U-Boot for further testing. Could you please guide me on how to debug or resolve this issue?&lt;/P&gt;&lt;P&gt;Looking forward to your suggestions.&lt;/P&gt;</description>
    <pubDate>Thu, 10 Jul 2025 05:15:15 GMT</pubDate>
    <dc:creator>rahul_raja</dc:creator>
    <dc:date>2025-07-10T05:15:15Z</dc:date>
    <item>
      <title>USB start failed in Uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2131388#M239156</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have flashed the i.MX8M Mini board and interrupted the boot process to access the U-Boot prompt. However, when I run the &lt;STRONG&gt;usb start&lt;/STRONG&gt; command, I receive the following output&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;u-boot=&amp;gt; usb start&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;starting USB...&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Bus usb@32e40000: Port not available.&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;Bus usb@32e50000: Port not available.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;It seems that the USB ports are not being detected or initialized correctly in U-Boot. I need to access USB functionality from U-Boot for further testing. Could you please guide me on how to debug or resolve this issue?&lt;/P&gt;&lt;P&gt;Looking forward to your suggestions.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Jul 2025 05:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2131388#M239156</guid>
      <dc:creator>rahul_raja</dc:creator>
      <dc:date>2025-07-10T05:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: USB start failed in Uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2133671#M239273</link>
      <description>&lt;P&gt;Which version BSP are you using? And which boot device you boot up from here, SD card or emmc?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jul 2025 02:49:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2133671#M239273</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-07-15T02:49:05Z</dc:date>
    </item>
    <item>
      <title>Re: USB start failed in Uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2133750#M239276</link>
      <description>&lt;P&gt;&lt;STRONG&gt;BSP Version:&lt;/STRONG&gt; Yocto Scarthgap (6.6.52)&lt;BR /&gt;&lt;STRONG&gt;Boot Device:&lt;/STRONG&gt; SD Card&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Additional Information:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have modified the U-Boot Device Tree Source (DTS) file by setting dr_mode = "host" for the usbotg2 node (usb@32e50000). Following this change, the USB controller at usb@32e50000 is now functional and successfully detecting connected USB devices.&lt;/P&gt;&lt;P&gt;However, the USB controller at usb@32e40000 (usbotg1) is still experiencing detection issues. The current configuration for usbotg1 has dr_mode = "otg".&lt;BR /&gt;&lt;BR /&gt;Looking forward to your suggestion&lt;/P&gt;</description>
      <pubDate>Tue, 15 Jul 2025 04:37:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2133750#M239276</guid>
      <dc:creator>rahul_raja</dc:creator>
      <dc:date>2025-07-15T04:37:04Z</dc:date>
    </item>
    <item>
      <title>Re: USB start failed in Uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2137143#M239411</link>
      <description>&lt;P&gt;How about your design, usb1 work as otg and usb2 work as host? Which usb interface are you using, type-C or micro usb?&lt;/P&gt;</description>
      <pubDate>Mon, 21 Jul 2025 07:46:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2137143#M239411</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-07-21T07:46:39Z</dc:date>
    </item>
    <item>
      <title>Re: USB start failed in Uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2137942#M239443</link>
      <description>Yes, our design configures USB1 to work as OTG and USB2 to function as host and also using micro usb</description>
      <pubDate>Tue, 22 Jul 2025 05:06:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2137942#M239443</guid>
      <dc:creator>rahul_raja</dc:creator>
      <dc:date>2025-07-22T05:06:39Z</dc:date>
    </item>
    <item>
      <title>Re: USB start failed in Uboot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2138832#M239482</link>
      <description>&lt;P&gt;You modify the usb2 setting may not affect the USB1 in generally, are you changing in the board dts file or chip dts file?&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jul 2025 02:21:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/USB-start-failed-in-Uboot/m-p/2138832#M239482</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-07-23T02:21:55Z</dc:date>
    </item>
  </channel>
</rss>