<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: i.MX8ULP USB connectivity issues</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-USB-connectivity-issues/m-p/2131198#M239145</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm attaching full schematic for USB part (Devboard-USB-PART)&lt;/P&gt;&lt;P&gt;SOM-USB-part is a screenshot from&amp;nbsp;MCIMX8ULP-EVK-SOM-a7.pdf , which is a part of&amp;nbsp;"&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8ULP-EVK-BB" target="_self"&gt;i.MX 8ULP EVK Base Board Design Files&lt;/A&gt;"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sergey&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jul 2025 22:22:45 GMT</pubDate>
    <dc:creator>texnikk</dc:creator>
    <dc:date>2025-07-09T22:22:45Z</dc:date>
    <item>
      <title>i.MX8ULP USB connectivity issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-USB-connectivity-issues/m-p/2131146#M239143</link>
      <description>&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;To evaluate i.MX8ULP processor for our products we're trying to build a custom devboard which is based on NXP-made SoM from&amp;nbsp;MCIMX8ULP-EVK-BB devkit.&amp;nbsp;&lt;BR /&gt;This board exposes USB0 from&amp;nbsp;MCIMX8ULP-EVK-SOM to a microUSB connector so that firmware can be uploaded using UUU utility in Serial Download mode.&lt;/P&gt;&lt;P&gt;Physical connectivity is quite simple (schematic screenshots attached)&lt;/P&gt;&lt;P&gt;But currently we're experiencing a USB connectivity issues with this board - in 90% of cases when we try to connect USB to host PC - the board is not detected. And even if it is detected - it starts to disappear and reappear. We've checked power and clocks - everything looks good, so we suspect some USB signal-related issue.&lt;/P&gt;&lt;P&gt;Is there any specific requirements for implementing USB2.0 connectivity with i.MX8ULP which must be obeyed for a stable and working USB (additionally to routing D+ and D- with 90 Ohm traces)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sergey&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 19:54:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-USB-connectivity-issues/m-p/2131146#M239143</guid>
      <dc:creator>texnikk</dc:creator>
      <dc:date>2025-07-09T19:54:48Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8ULP USB connectivity issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-USB-connectivity-issues/m-p/2131184#M239144</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Could you please share the connections in i.MX side?&lt;/P&gt;
&lt;P&gt;Did you perform a signal integrity simulation?&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 21:30:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-USB-connectivity-issues/m-p/2131184#M239144</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-07-09T21:30:53Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8ULP USB connectivity issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-USB-connectivity-issues/m-p/2131198#M239145</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm attaching full schematic for USB part (Devboard-USB-PART)&lt;/P&gt;&lt;P&gt;SOM-USB-part is a screenshot from&amp;nbsp;MCIMX8ULP-EVK-SOM-a7.pdf , which is a part of&amp;nbsp;"&lt;A href="https://www.nxp.com/webapp/Download?colCode=IMX8ULP-EVK-BB" target="_self"&gt;i.MX 8ULP EVK Base Board Design Files&lt;/A&gt;"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Sergey&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 22:22:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-USB-connectivity-issues/m-p/2131198#M239145</guid>
      <dc:creator>texnikk</dc:creator>
      <dc:date>2025-07-09T22:22:45Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX8ULP USB connectivity issues</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-USB-connectivity-issues/m-p/2131789#M239168</link>
      <description>&lt;DIV&gt;
&lt;DIV&gt;
&lt;DIV&gt;
&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Got it, thank you for the update.&lt;/P&gt;
&lt;P&gt;As I can see, you are using our SOM and connecting it to your custom base board with Micro USB.&lt;/P&gt;
&lt;P&gt;Please take a look in the next post, the i.MX8MM can be used as reference for i.MX8ULP.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-i-MX8MQ-USB2-0-Design-Without-USB-TYPE-C/ta-p/1129527" target="_blank"&gt;i.MX8MM &amp;amp; i.MX8MQ USB2.0 Design Without USB TYPE-C - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;
&lt;/DIV&gt;</description>
      <pubDate>Thu, 10 Jul 2025 15:02:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-USB-connectivity-issues/m-p/2131789#M239168</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-07-10T15:02:30Z</dc:date>
    </item>
  </channel>
</rss>