<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Fail to load m33.bin in u-boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Fail-to-load-m33-bin-in-u-boot/m-p/2130736#M239110</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195089"&gt;@WolsYang&lt;/a&gt;&amp;nbsp;, which imx93 linux BSP are you using? &lt;BR /&gt;&lt;BR /&gt;Do you not see any nodes inside this directory :-&lt;/P&gt;
&lt;PRE class="lia-code-sample  language-markup"&gt;&lt;CODE&gt;/sys/devices/platform&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;please paste the output of "ls /sys/devices/platform/"&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 09 Jul 2025 08:14:25 GMT</pubDate>
    <dc:creator>gaurav_sharma</dc:creator>
    <dc:date>2025-07-09T08:14:25Z</dc:date>
    <item>
      <title>Fail to load m33.bin in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fail-to-load-m33-bin-in-u-boot/m-p/2130697#M239106</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/228933"&gt;@gaurav_sharma&lt;/a&gt;&amp;nbsp;:&lt;/P&gt;&lt;P&gt;I try to do this example, but fail.&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Using-UART-as-wakeup-source-to-wake-Cortex-A55-from-Cortex-M33/ta-p/1806718" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Using-UART-as-wakeup-source-to-wake-Cortex-A55-from-Cortex-M33/ta-p/1806718&lt;/A&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;u-boot=&amp;gt; fatls mmc 0:1 /mcore-demos/
./
../
130428 imx93-11x11-evk_m33_TCM_low_power_wakeword.bin
19080 imx93-11x11-evk_m33_TCM_power_mode_switch.bin
47472 imx93-11x11-evk_m33_TCM_sai_low_power_audio.bin
18708 imx93-11x11-evk_m33_TCM_rpmsg_lite_pingpong_rtos_linux_remote.bin
17228 imx93-11x11-evk_m33_TCM_rpmsg_lite_str_echo_rtos.bin

5 file(s), 2 dir(s)

u-boot=&amp;gt; setenv fdtfile imx93-11x11-evk-rpmsg.dtb
u-boot=&amp;gt; setenv bootargs ${jh_clk} ${mcore_clk} console=${console} root=${mmcroot}
u-boot=&amp;gt; fatload mmc 0:1 0x80000000 /mcore-demos/imx93-11x11-evk_m33_TCM_power_mode_switch.bin
19080 bytes read in 19 ms (980.5 KiB/s)
u-boot=&amp;gt; cp.b 0x80000000 0x201e0000 19080



u-boot=&amp;gt; boot
Working FDT set to 83000000
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
libfdt fdt_path_offset() returned FDT_ERR_NOTFOUND
switch to partitions #0, OK
mmc0(part 0) is current device
Scanning mmc 0:1...
65298 bytes read in 3 ms (20.8 MiB/s)
MMC: no card present
Unable to open OP-TEE session (err=-5)
mm_communicate failed!
Error: Cannot initialize UEFI sub-system, r = 3
MMC: no card present
starting USB...
Bus usb@4c100000: SNK.Default on CC1
SNK.Default on CC1
SNK.Default on CC1
Port not available.
Bus usb@4c200000: tcpc_setup_ufp_mode: Polling ALERT register, TCPC_ALERT_CC_STATUS bit failed, ret = -62
Port not available.
USB is stopped. Please issue 'usb start' first.
Running BSP bootcmd ...
switch to partitions #0, OK
mmc0(part 0) is current device
Failed to load 'boot.scr'
34978304 bytes read in 133 ms (250.8 MiB/s)
Booting from mmc ...
65298 bytes read in 13 ms (4.8 MiB/s)
## Flattened Device Tree blob at 83000000
Booting using the fdt blob at 0x83000000
Working FDT set to 83000000
Using Device Tree in place at 0000000083000000, end 0000000083012f11
Working FDT set to 83000000
adv7535_mipi2hdmi hdmi@3d: Can't find cec device id=0x3c
fail to probe panel device hdmi@3d
fail to get display timings
probe video device failed, ret -19

Starting kernel ...&lt;/LI-CODE&gt;&lt;P&gt;But I can't start&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;echo start &amp;gt; /sys/devices/platform/imx93-cm33/remoteproc/remoteproc0/state
-sh: /sys/devices/platform/imx93-cm33/remoteproc/remoteproc0/state: No such file or directory

root@imx93-11x11-lpddr4x-evk:~# echo start &amp;gt; /sys/class/remoteproc/remoteproc0/state
-sh: echo: write error: No such file or directory
root@imx93-11x11-lpddr4x-evk:~# ls /sys/class/remoteproc/remoteproc0/state
/sys/class/remoteproc/remoteproc0/state&lt;/LI-CODE&gt;&lt;P&gt;But if I do in Linux it work&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93-11x11-lpddr4x-evk:~# echo /lib/firmware/imx93-11x11-evk_m33_TCM_power_mode_switch.elf &amp;gt; /sys/class/remoteproc/remoteproc0/firmware
root@imx93-11x11-lpddr4x-evk:~# echo start &amp;gt; /sys/class/remoteproc/remoteproc0/state
root@imx93-11x11-lpddr4x-evk:~#&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 07:23:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fail-to-load-m33-bin-in-u-boot/m-p/2130697#M239106</guid>
      <dc:creator>WolsYang</dc:creator>
      <dc:date>2025-07-09T07:23:24Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to load m33.bin in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fail-to-load-m33-bin-in-u-boot/m-p/2130736#M239110</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/195089"&gt;@WolsYang&lt;/a&gt;&amp;nbsp;, which imx93 linux BSP are you using? &lt;BR /&gt;&lt;BR /&gt;Do you not see any nodes inside this directory :-&lt;/P&gt;
&lt;PRE class="lia-code-sample  language-markup"&gt;&lt;CODE&gt;/sys/devices/platform&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;please paste the output of "ls /sys/devices/platform/"&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 08:14:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fail-to-load-m33-bin-in-u-boot/m-p/2130736#M239110</guid>
      <dc:creator>gaurav_sharma</dc:creator>
      <dc:date>2025-07-09T08:14:25Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to load m33.bin in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fail-to-load-m33-bin-in-u-boot/m-p/2130746#M239111</link>
      <description>&lt;P&gt;And if you want to boot cm33 binary at Uboot, you have to additionally do the following after copying the image to TCM[i.e the step in which you execute "cp.b"]: -&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P style="margin: 0in; font-family: Calibri; font-size: 11.0pt;" lang="en-US"&gt;&lt;FONT face="arial black,avant garde"&gt;bootaux 0x1ffe0000 0&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 08:20:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fail-to-load-m33-bin-in-u-boot/m-p/2130746#M239111</guid>
      <dc:creator>gaurav_sharma</dc:creator>
      <dc:date>2025-07-09T08:20:17Z</dc:date>
    </item>
    <item>
      <title>Re: Fail to load m33.bin in u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Fail-to-load-m33-bin-in-u-boot/m-p/2130826#M239120</link>
      <description>&lt;P&gt;I am working on 6.12&lt;/P&gt;&lt;P&gt;Boot m33 in u-boot by this cmd is work&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;bootaux 0x1ffe0000 0&lt;/LI-CODE&gt;&lt;P&gt;But boot in Linux is still fail(Well it should be, we didn't change any thing)&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;root@imx93-11x11-lpddr4x-evk:~# ls /sys/devices/platform
'Fixed MDIO bus.0'   firmware:optee   power          regulator-adc-vref    regulator-dvdd          regulator-usdhc3    remoteproc-cm33   serial8250      uevent
 acpi-einj           i2c-rpbus-1      psci           regulator-audio-pwr   regulator-hmisc-vddio   regulator-vdd-12v   rpmsg_audio       snd-soc-dummy   usbphynop1
 bt-sco-codec        imx93-lpm        psci-cpuidle   regulator-avdd        regulator-m2-pwr        regulator-vddo      rpmsg_micfil      soc@0           usbphynop2
 display-subsystem   pmu              reg-dummy      regulator-can2-stby   regulator-usdhc2        regulatory.0        secure-enclave    timer           usdhc3_pwrseq
root@imx93-11x11-lpddr4x-evk:~# cat /etc/os-release 
ID=fsl-imx-xwayland
NAME="NXP i.MX Release Distro"
VERSION="6.12-styhead (styhead)"
VERSION_ID=6.12-styhead
VERSION_CODENAME="styhead"
PRETTY_NAME="NXP i.MX Release Distro 6.12-styhead (styhead)"
CPE_NAME="cpe:/o:openembedded:fsl-imx-xwayland:6.12-styhead"
root@imx93-11x11-lpddr4x-evk:~# 
root@imx93-11x11-lpddr4x-evk:~# 
root@imx93-11x11-lpddr4x-evk:~# echo start &amp;gt; /sys/class/remoteproc/remoteproc0/state                                                                                                             
-sh: echo: write error: No such file or directory
root@imx93-11x11-lpddr4x-evk:~# ls /sys/class/remoteproc/remoteproc0/state 
/sys/class/remoteproc/remoteproc0/state
root@imx93-11x11-lpddr4x-evk:~# &lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Jul 2025 09:52:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Fail-to-load-m33-bin-in-u-boot/m-p/2130826#M239120</guid>
      <dc:creator>WolsYang</dc:creator>
      <dc:date>2025-07-09T09:52:13Z</dc:date>
    </item>
  </channel>
</rss>