<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Android 15: fastboot : Waiting for Any device.</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2129711#M239062</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Are you flashing a built image or did you download a prebuilt? Please try with a prebuilt one.&lt;/P&gt;
&lt;P&gt;When running the command without -D option, make sure that all the necessary files are under that directory. Finally, make sure to run the script with sudo.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;</description>
    <pubDate>Tue, 08 Jul 2025 03:11:19 GMT</pubDate>
    <dc:creator>JosephAtNXP</dc:creator>
    <dc:date>2025-07-08T03:11:19Z</dc:date>
    <item>
      <title>Android 15: fastboot : Waiting for Any device.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2125087#M238827</link>
      <description>&lt;P&gt;Hello.&lt;BR /&gt;I need help.&lt;BR /&gt;I have the Compulab board with the image on EMMC that doesn't provide ADB.&lt;BR /&gt;I tried to flash the new built image to SD card. This works well and now I can see&lt;BR /&gt;adb device with "adb devices" command.&lt;BR /&gt;But I want to flash the image to EMMC itself.&lt;BR /&gt;When I try do this with image booted from SD, I always have:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Axent_0-1751130759767.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/345159iCD1885735A7E3E87/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Axent_0-1751130759767.png" alt="Axent_0-1751130759767.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Axent_0-1751130759767.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Please, help. How can I reflash the EMMC?? Thanks.&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Sat, 28 Jun 2025 17:13:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2125087#M238827</guid>
      <dc:creator>Axent</dc:creator>
      <dc:date>2025-06-28T17:13:30Z</dc:date>
    </item>
    <item>
      <title>Re: Android 15: fastboot : Waiting for Any device.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2125859#M238856</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;You can use the uuu script for flashing eMMC.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;&amp;gt; uuu_imx_android_flash.sh for Linux OS
&amp;gt; uuu_imx_android_flash.bat for Windows OS&lt;/LI-CODE&gt;
&lt;P&gt;Refer to chapter &lt;A href="https://www.nxp.com/docs/en/quick-reference-guide/ANDROID_QUICK_START_GUIDE.pdf" target="_self"&gt;3.3 Flashing board images&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jun 2025 20:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2125859#M238856</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-06-30T20:31:29Z</dc:date>
    </item>
    <item>
      <title>Re: Android 15: fastboot : Waiting for Any device.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2126152#M238881</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;Thanks for reply.&lt;BR /&gt;But now I have another issue with EMMC.&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/Android-15-How-to-restore-EMMC/m-p/2125158#M238831" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/Android-15-How-to-restore-EMMC/m-p/2125158#M238831&lt;/A&gt;&lt;BR /&gt;I cannot reflash it through fastboot or uuu (accidentally wrong image downloaded, no uboot)&lt;BR /&gt;And now I am searching how to flash empty EMMC or some way to 'copy' booted image from SD card.&lt;BR /&gt;&lt;BR /&gt;Please, help. What should I do to flash bootloader at least to EMMC (or copy from SD).?&lt;BR /&gt;I don't have available detected USB device for UUU (EMMC doesn't have the valid bootloader), also fastboot is impossible.&lt;BR /&gt;I can just boot from SD card. But I'm really misunderstanding how to rebase my working bootloader from SD to EMMC.&lt;BR /&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jul 2025 06:47:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2126152#M238881</guid>
      <dc:creator>Axent</dc:creator>
      <dc:date>2025-07-01T06:47:50Z</dc:date>
    </item>
    <item>
      <title>Re: Android 15: fastboot : Waiting for Any device.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2126688#M238899</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/202119"&gt;@Axent&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;That's the function of UUU, it doesn't require U-boot to enter to fastboot. When the processor boots in serial download mode you can confirm it's UUU can burn eMMC/SD by running&lt;/P&gt;
&lt;P&gt;uuu -lsusb&lt;/P&gt;
&lt;P&gt;When you cannot access boot pins and the processor fails to fetch boot images, it should enter to serial download, please confirm with the past command.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jul 2025 23:53:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2126688#M238899</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-07-01T23:53:10Z</dc:date>
    </item>
    <item>
      <title>Re: Android 15: fastboot : Waiting for Any device.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2128099#M238966</link>
      <description>&lt;P&gt;Thanks Joseph.&lt;BR /&gt;This question is solved.&lt;BR /&gt;But I now have another issue.&lt;BR /&gt;If you can, I will be glad if you ll can help.&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/uuu-imx-android-flash-sh-doesn-t-work/m-p/2128098#M238965" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/uuu-imx-android-flash-sh-doesn-t-work/m-p/2128098#M238965&lt;/A&gt;&lt;BR /&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jul 2025 13:02:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2128099#M238966</guid>
      <dc:creator>Axent</dc:creator>
      <dc:date>2025-07-03T13:02:33Z</dc:date>
    </item>
    <item>
      <title>Re: Android 15: fastboot : Waiting for Any device.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2129711#M239062</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Are you flashing a built image or did you download a prebuilt? Please try with a prebuilt one.&lt;/P&gt;
&lt;P&gt;When running the command without -D option, make sure that all the necessary files are under that directory. Finally, make sure to run the script with sudo.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jul 2025 03:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Android-15-fastboot-Waiting-for-Any-device/m-p/2129711#M239062</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-07-08T03:11:19Z</dc:date>
    </item>
  </channel>
</rss>