<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: i.MX93 nxpele: Unknown command 'ele_message' in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-nxpele-Unknown-command-ele-message/m-p/2129202#M239037</link>
    <description>&lt;P&gt;I found the cause of the issue. The u-boot version provided with our karo evaluation board is not branched from the nxp u-boot repository. Therefore the ELE part nxp adds was not part of this repo, thus not part of the generated u-boot image.&lt;/P&gt;</description>
    <pubDate>Mon, 07 Jul 2025 09:25:04 GMT</pubDate>
    <dc:creator>HH_Mov</dc:creator>
    <dc:date>2025-07-07T09:25:04Z</dc:date>
    <item>
      <title>i.MX93 nxpele: Unknown command 'ele_message'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-nxpele-Unknown-command-ele-message/m-p/2126278#M238885</link>
      <description>&lt;P&gt;I am trying to fuse the SRKs of my i.MX93 evaluation module via the nxpele command line tool, based on &lt;A href="https://spsdk.readthedocs.io/en/stable/examples/ahab/imx93/imx93_signed_ahab_uboot.html" target="_blank"&gt;i.MX 93 signed and encrypted AHAB image — SPSDK documentation&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;The communication with the u-boot however does not seem to work for nxpele.&lt;BR /&gt;&lt;BR /&gt;As a reference, I call the "get-info" command, but I see the following on my cmd terminal:&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;FONT size="2"&gt;nxpele -p COM3 -f mimx9352 -v get-info&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;INFO:spsdk.ele.ele_comm:ELE communicator is using 131072 B size buffer at 83800000 address in mimx9352, Revision: latest target.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;INFO:spsdk.uboot.spsdk_uuu:setenv stdout serial,fastboot success=True response=&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;INFO:spsdk.uboot.spsdk_uuu:ele_message 0x83800000 0x20000 0604da17000000001800808300010000 success=False response=&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;SPSDKError: SPSDK: ELE Communication failed with UBoot: list index out of range&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;On the u-boot command prompt (via a serial connection to the board) it shows:&lt;/P&gt;&lt;P class="lia-indent-padding-left-30px"&gt;&lt;BR /&gt;&lt;FONT size="2"&gt;Unknown command 'ele_message' - try 'help'&lt;/FONT&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;I configured u-boot with CONFIG_AHAB_BOOT=y and&amp;nbsp;CONFIG_CONSOLE_MUX=y.&lt;BR /&gt;However it seems that the commands are not present.&lt;BR /&gt;&lt;BR /&gt;I am using a Yocto based image with u-boot based on the meta-imx and meta-karo-nxp layers.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;Am I missing a specific recipe/configuration flag/setting ?&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jul 2025 08:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-nxpele-Unknown-command-ele-message/m-p/2126278#M238885</guid>
      <dc:creator>HH_Mov</dc:creator>
      <dc:date>2025-07-01T08:56:22Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 nxpele: Unknown command 'ele_message'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-nxpele-Unknown-command-ele-message/m-p/2128546#M238985</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Which version of SPSDK package are you using and what's the BSP version(especially the ELE FW version)? Did you use i.MX93 A1 chip revision?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 04 Jul 2025 08:24:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-nxpele-Unknown-command-ele-message/m-p/2128546#M238985</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2025-07-04T08:24:39Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX93 nxpele: Unknown command 'ele_message'</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX93-nxpele-Unknown-command-ele-message/m-p/2129202#M239037</link>
      <description>&lt;P&gt;I found the cause of the issue. The u-boot version provided with our karo evaluation board is not branched from the nxp u-boot repository. Therefore the ELE part nxp adds was not part of this repo, thus not part of the generated u-boot image.&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jul 2025 09:25:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX93-nxpele-Unknown-command-ele-message/m-p/2129202#M239037</guid>
      <dc:creator>HH_Mov</dc:creator>
      <dc:date>2025-07-07T09:25:04Z</dc:date>
    </item>
  </channel>
</rss>