<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic i.MX 53 Linux OS Support in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-53-Linux-OS-Support/m-p/2128963#M239027</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm currently running &lt;STRONG&gt;WEC2013&lt;/STRONG&gt; on an &lt;STRONG&gt;i.MX53-based system&lt;/STRONG&gt;, but since WEC2013 is now obsolete, I'm planning to migrate to &lt;STRONG&gt;Linux&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;I understand that the officially supported Linux kernel version for i.MX53 is &lt;STRONG&gt;2.6.35&lt;/STRONG&gt;.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Are there newer Linux kernel versions (e.g., 3.x, 4.x, 5.x) that are known to work on i.MX53?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Would it be feasible to use a custom Yocto-based Linux distribution, for example using Yocto 4.0 (Kirkstone) or Yocto 5.0 (Scarthgap) for i.MX53?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I'm especially interested in knowing the current level of support in mainline kernels or through community-maintained BSPs, and any known limitations (e.g., graphics or multimedia features).&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
    <pubDate>Mon, 07 Jul 2025 04:01:57 GMT</pubDate>
    <dc:creator>pvshankar96</dc:creator>
    <dc:date>2025-07-07T04:01:57Z</dc:date>
    <item>
      <title>i.MX 53 Linux OS Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-53-Linux-OS-Support/m-p/2128963#M239027</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm currently running &lt;STRONG&gt;WEC2013&lt;/STRONG&gt; on an &lt;STRONG&gt;i.MX53-based system&lt;/STRONG&gt;, but since WEC2013 is now obsolete, I'm planning to migrate to &lt;STRONG&gt;Linux&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;I understand that the officially supported Linux kernel version for i.MX53 is &lt;STRONG&gt;2.6.35&lt;/STRONG&gt;.&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;P&gt;Are there newer Linux kernel versions (e.g., 3.x, 4.x, 5.x) that are known to work on i.MX53?&lt;/P&gt;&lt;/LI&gt;&lt;LI&gt;&lt;P&gt;Would it be feasible to use a custom Yocto-based Linux distribution, for example using Yocto 4.0 (Kirkstone) or Yocto 5.0 (Scarthgap) for i.MX53?&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I'm especially interested in knowing the current level of support in mainline kernels or through community-maintained BSPs, and any known limitations (e.g., graphics or multimedia features).&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jul 2025 04:01:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-53-Linux-OS-Support/m-p/2128963#M239027</guid>
      <dc:creator>pvshankar96</dc:creator>
      <dc:date>2025-07-07T04:01:57Z</dc:date>
    </item>
    <item>
      <title>Re: i.MX 53 Linux OS Support</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/i-MX-53-Linux-OS-Support/m-p/2129759#M239070</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/244189"&gt;@pvshankar96&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Sorry, we are not support imx5 after Linux kernel version 2.6.35. Also In Yocto 4.0, it mainly supports i.MX6 and above platforms, and no longer includes i.MX53.&lt;/P&gt;
&lt;P&gt;.B.R&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 08 Jul 2025 04:57:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/i-MX-53-Linux-OS-Support/m-p/2129759#M239070</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-07-08T04:57:06Z</dc:date>
    </item>
  </channel>
</rss>