<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 8MPLUSLPD4-PEVK in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2127114#M238909</link>
    <description>&lt;P&gt;I have sent a reply to myself so I will reply again.&lt;/P&gt;&lt;P&gt;I followed the instructions in this document but was unable to connect.&lt;/P&gt;&lt;P&gt;Below is the terminal output from muuxpresso.&lt;/P&gt;&lt;P&gt;Connecting to J-Link...&lt;BR /&gt;J-Link is connected.&lt;BR /&gt;Device "MIMX8ML8_M7" selected.&lt;BR /&gt;Firmware: J-Link V11 compiled Apr 1 2025 10:02:30&lt;BR /&gt;Hardware: V11.00&lt;BR /&gt;S/N: 51020038&lt;BR /&gt;Feature(s): GDB&lt;BR /&gt;Checking target voltage...&lt;BR /&gt;Target voltage: 1.71 V&lt;BR /&gt;Listening on TCP/IP port 2330&lt;BR /&gt;Connecting to target...&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;ConfigTargetSettings() end - Took 78us&lt;BR /&gt;InitTarget() start&lt;BR /&gt;InitTarget() end - Took 54.1ms&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;Failed to identify target. Resetting via Reset pin and trying again.&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;ConfigTargetSettings() end - Took 27us&lt;BR /&gt;InitTarget() start&lt;BR /&gt;InitTarget() end - Took 55.0ms&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;ERROR: Could not connect to target.&lt;BR /&gt;Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...&lt;BR /&gt;Shutting down...&lt;BR /&gt;Could not connect to target.&lt;BR /&gt;Please check power, connection and settings.[2025-07-02T07:22:26.760Z] SERVER CONSOLE DEBUG: GDB server connection closed.&lt;BR /&gt;GDB server connection closed. Terminal will be reused, waiting for next session to start...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 02 Jul 2025 09:32:00 GMT</pubDate>
    <dc:creator>takahashi1</dc:creator>
    <dc:date>2025-07-02T09:32:00Z</dc:date>
    <item>
      <title>8MPLUSLPD4-PEVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2126744#M238903</link>
      <description>&lt;P&gt;I am planning to develop RTOS-based firmware on the M7 with the i.MX8M plus.&lt;/P&gt;&lt;P&gt;I'll use A53 with Linux.&lt;/P&gt;&lt;P&gt;So I'm using the evaluation kit "8MPLUSLPD4-PEVK" that I have, building a sample project with MCUXpresso for VSCode, and trying to test debugging with Segger's j-Link.&lt;/P&gt;&lt;P&gt;I was able to generate the target elf and bin without any problems up until the build stage, but when I tried to debug, I couldn't connect to the target evaluation kit with j-Link.&lt;/P&gt;&lt;P&gt;The evaluation kit is SD booted, and u-boot is started with the debug UART, but Linux has not yet started.&lt;/P&gt;&lt;P&gt;Since I can't connect from VS Code in this state, I tried to connect with Segger's j-Link commander, but I couldn't connect.&lt;/P&gt;&lt;P&gt;I'd like to know if there are any settings required to debug the M7 via JTAG.&lt;/P&gt;&lt;P&gt;Below is the log from j-Link commander&lt;/P&gt;&lt;P&gt;SEGGER J-Link Commander V8.46 (Compiled Jun 26 2025 07:49:03)&lt;BR /&gt;DLL version V8.46, compiled Jun 26 2025 07:48:12&lt;/P&gt;&lt;P&gt;Connecting to J-Link via USB...O.K.&lt;BR /&gt;Firmware: J-Link V11 compiled Apr 1 2025 10:02:30&lt;BR /&gt;Hardware version: V11.00&lt;BR /&gt;J-Link uptime (since boot): 0d 00h 01m 58s&lt;BR /&gt;S/N: 51020038&lt;BR /&gt;License(s): GDB&lt;BR /&gt;USB speed mode: High speed (480 MBit/s)&lt;BR /&gt;VTref=1.704V&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Type "connect" to establish a target connection, '?' for help&lt;BR /&gt;J-Link&amp;gt;connect&lt;BR /&gt;Please specify device / core. &amp;lt;Default&amp;gt;: MIMX8ML8_M7&lt;BR /&gt;Type '?' for selection dialog&lt;BR /&gt;Device&amp;gt;&lt;BR /&gt;Please specify target interface:&lt;BR /&gt;J) JTAG (Default)&lt;BR /&gt;S) SWD&lt;BR /&gt;T) cJTAG&lt;BR /&gt;TIF&amp;gt;&lt;BR /&gt;Device position in JTAG chain (IRPre,DRPre) &amp;lt;Default&amp;gt;: -1,-1 =&amp;gt; Auto-detect&lt;BR /&gt;JTAGConf&amp;gt;&lt;BR /&gt;Specify target interface speed [kHz]. &amp;lt;Default&amp;gt;: 4000 kHz&lt;BR /&gt;Speed&amp;gt;&lt;BR /&gt;Device "MIMX8ML8_M7" selected.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Connecting to target via JTAG&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;ConfigTargetSettings() end - Took 1.91ms&lt;BR /&gt;InitTarget() start&lt;BR /&gt;InitTarget() end - Took 54.9ms&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;Failed to identify target. Resetting via Reset pin and trying again.&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;ConfigTargetSettings() end - Took 22us&lt;BR /&gt;InitTarget() start&lt;BR /&gt;InitTarget() end - Took 52.6ms&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;Error occurred: Could not connect to the target device.&lt;BR /&gt;For troubleshooting steps visit: &lt;A href="https://kb.segger.com/J-Link_Troubleshooting" target="_blank"&gt;https://kb.segger.com/J-Link_Troubleshooting&lt;/A&gt;&lt;BR /&gt;J-Link&amp;gt;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jul 2025 02:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2126744#M238903</guid>
      <dc:creator>takahashi1</dc:creator>
      <dc:date>2025-07-02T02:16:46Z</dc:date>
    </item>
    <item>
      <title>Re: 8MPLUSLPD4-PEVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2126867#M238905</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252221"&gt;@takahashi1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;please refer the attachment file.&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jul 2025 06:00:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2126867#M238905</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-07-02T06:00:02Z</dc:date>
    </item>
    <item>
      <title>Re: 8MPLUSLPD4-PEVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2126978#M238907</link>
      <description>&lt;P&gt;I followed the instructions in this document but was unable to connect.&lt;/P&gt;&lt;P&gt;Below is the terminal output from muuxpresso.&lt;/P&gt;&lt;P&gt;Connecting to J-Link...&lt;BR /&gt;J-Link is connected.&lt;BR /&gt;Device "MIMX8ML8_M7" selected.&lt;BR /&gt;Firmware: J-Link V11 compiled Apr 1 2025 10:02:30&lt;BR /&gt;Hardware: V11.00&lt;BR /&gt;S/N: 51020038&lt;BR /&gt;Feature(s): GDB&lt;BR /&gt;Checking target voltage...&lt;BR /&gt;Target voltage: 1.71 V&lt;BR /&gt;Listening on TCP/IP port 2330&lt;BR /&gt;Connecting to target...&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;ConfigTargetSettings() end - Took 78us&lt;BR /&gt;InitTarget() start&lt;BR /&gt;InitTarget() end - Took 54.1ms&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;Failed to identify target. Resetting via Reset pin and trying again.&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;ConfigTargetSettings() end - Took 27us&lt;BR /&gt;InitTarget() start&lt;BR /&gt;InitTarget() end - Took 55.0ms&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;ERROR: Could not connect to target.&lt;BR /&gt;Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...&lt;BR /&gt;Shutting down...&lt;BR /&gt;Could not connect to target.&lt;BR /&gt;Please check power, connection and settings.[2025-07-02T07:22:26.760Z] SERVER CONSOLE DEBUG: GDB server connection closed.&lt;BR /&gt;GDB server connection closed. Terminal will be reused, waiting for next session to start...&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jul 2025 07:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2126978#M238907</guid>
      <dc:creator>takahashi1</dc:creator>
      <dc:date>2025-07-02T07:37:15Z</dc:date>
    </item>
    <item>
      <title>Re: 8MPLUSLPD4-PEVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2127114#M238909</link>
      <description>&lt;P&gt;I have sent a reply to myself so I will reply again.&lt;/P&gt;&lt;P&gt;I followed the instructions in this document but was unable to connect.&lt;/P&gt;&lt;P&gt;Below is the terminal output from muuxpresso.&lt;/P&gt;&lt;P&gt;Connecting to J-Link...&lt;BR /&gt;J-Link is connected.&lt;BR /&gt;Device "MIMX8ML8_M7" selected.&lt;BR /&gt;Firmware: J-Link V11 compiled Apr 1 2025 10:02:30&lt;BR /&gt;Hardware: V11.00&lt;BR /&gt;S/N: 51020038&lt;BR /&gt;Feature(s): GDB&lt;BR /&gt;Checking target voltage...&lt;BR /&gt;Target voltage: 1.71 V&lt;BR /&gt;Listening on TCP/IP port 2330&lt;BR /&gt;Connecting to target...&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;ConfigTargetSettings() end - Took 78us&lt;BR /&gt;InitTarget() start&lt;BR /&gt;InitTarget() end - Took 54.1ms&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;Failed to identify target. Resetting via Reset pin and trying again.&lt;BR /&gt;ConfigTargetSettings() start&lt;BR /&gt;ConfigTargetSettings() end - Took 27us&lt;BR /&gt;InitTarget() start&lt;BR /&gt;InitTarget() end - Took 55.0ms&lt;BR /&gt;TotalIRLen = ?, IRPrint = 0x..000000000000000000000000&lt;BR /&gt;ERROR: Could not connect to target.&lt;BR /&gt;Target connection failed. GDBServer will be closed...Restoring target state and closing J-Link connection...&lt;BR /&gt;Shutting down...&lt;BR /&gt;Could not connect to target.&lt;BR /&gt;Please check power, connection and settings.[2025-07-02T07:22:26.760Z] SERVER CONSOLE DEBUG: GDB server connection closed.&lt;BR /&gt;GDB server connection closed. Terminal will be reused, waiting for next session to start...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jul 2025 09:32:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2127114#M238909</guid>
      <dc:creator>takahashi1</dc:creator>
      <dc:date>2025-07-02T09:32:00Z</dc:date>
    </item>
    <item>
      <title>Re: 8MPLUSLPD4-PEVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2127902#M238956</link>
      <description>&lt;P&gt;HI&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252221"&gt;@takahashi1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please share your this picture, check if your PC can find the J-Link device.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="pengyong_zhang_0-1751530168446.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/345946iCD3DEA808AF039E2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="pengyong_zhang_0-1751530168446.png" alt="pengyong_zhang_0-1751530168446.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;pengyong_zhang_0-1751530168446.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Jul 2025 08:10:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2127902#M238956</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-07-03T08:10:07Z</dc:date>
    </item>
    <item>
      <title>Re: 8MPLUSLPD4-PEVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2128906#M239021</link>
      <description>&lt;P&gt;The j-Link itself is connected.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="j-Link.png" style="width: 354px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/346193iD2F0D908B9932E33/image-size/large?v=v2&amp;amp;px=999" role="button" title="j-Link.png" alt="j-Link.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;j-Link.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jul 2025 02:01:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2128906#M239021</guid>
      <dc:creator>takahashi1</dc:creator>
      <dc:date>2025-07-07T02:01:48Z</dc:date>
    </item>
    <item>
      <title>Re: 8MPLUSLPD4-PEVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2129187#M239035</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252221"&gt;@takahashi1&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;i have tested the helloword demo on my i.mx 8MP EVK board, there is no error occured. Make sure your board is boot normal in uboot, and your J-link connect right. Did you try the helloword demo?&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;</description>
      <pubDate>Mon, 07 Jul 2025 09:13:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/8MPLUSLPD4-PEVK/m-p/2129187#M239035</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2025-07-07T09:13:12Z</dc:date>
    </item>
  </channel>
</rss>