<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: External Clock For i.MX 8M Plus</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/External-Clock-For-i-MX-8M-Plus/m-p/2125950#M238865</link>
    <description>&lt;P&gt;Already give reply to you in the case you created, please check it there.&lt;/P&gt;</description>
    <pubDate>Tue, 01 Jul 2025 02:16:14 GMT</pubDate>
    <dc:creator>Rita_Wang</dc:creator>
    <dc:date>2025-07-01T02:16:14Z</dc:date>
    <item>
      <title>External Clock For i.MX 8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-Clock-For-i-MX-8M-Plus/m-p/2124415#M238781</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;The i.MX 8M Plus processor has two external input system clocks: a low frequency (RTC_XTALI) and a high frequency (XTALI).&lt;/P&gt;&lt;P&gt;The i.MX 8M Plus datasheet, in Section 3.1.6 states:&lt;/P&gt;&lt;P&gt;Regarding the 32.768kHz external clock , the datasheet recommends: RTC_XTALO is connected to NVCC_SNVS_1P8 (1.8 V) through a 100 Kohm resistor. And the level range of the crystal's ViH is&amp;nbsp;0.7 x NVCC_SNVS_1P8 to&amp;nbsp;NVCC_SNVS_1P8 , the level range of the crystal's ViL is&amp;nbsp;0 to 0.3 x NVCC_SNVS_1P8.&lt;/P&gt;&lt;P&gt;Regarding the 24MHz external clock , the datasheet recommends: XTALO_24M is connected to VDD_24M_XTAL_1P8 through a 400 ohm resistor. And the level range of the crystal's ViH is0.7 x Vdd to Vdd + 0.3 , the level range of the crystal's ViL is -0.3 to 0.3 x Vdd.&lt;/P&gt;&lt;P&gt;However, in the schematic diagram of 8MPLUSLPD4-CPU Sheet 8 of 12, (Document No.: SCH-46368, PDF: SPF-46368), the above two resistors are not designed.&lt;/P&gt;&lt;P&gt;Questions:&lt;/P&gt;&lt;P&gt;1) Are these two resistors necessary for the development of the i.MX 8M Plus processor product (due to differences in datasheet and schematic)?&lt;/P&gt;&lt;P&gt;2) Must the ViH and ViL of the crystal oscillator strictly&amp;nbsp;adhere to the specified voltage ranges? If the high-level voltage does not meet the requirements, will the processor still function properly?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Canon Medical&lt;BR /&gt;Zhipeng Fan&lt;/P&gt;</description>
      <pubDate>Fri, 27 Jun 2025 04:47:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-Clock-For-i-MX-8M-Plus/m-p/2124415#M238781</guid>
      <dc:creator>Medical</dc:creator>
      <dc:date>2025-06-27T04:47:39Z</dc:date>
    </item>
    <item>
      <title>Re: External Clock For i.MX 8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-Clock-For-i-MX-8M-Plus/m-p/2125250#M238839</link>
      <description>&lt;P&gt;I will confirm it for you.&lt;/P&gt;</description>
      <pubDate>Mon, 30 Jun 2025 03:04:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-Clock-For-i-MX-8M-Plus/m-p/2125250#M238839</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-06-30T03:04:20Z</dc:date>
    </item>
    <item>
      <title>Re: External Clock For i.MX 8M Plus</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/External-Clock-For-i-MX-8M-Plus/m-p/2125950#M238865</link>
      <description>&lt;P&gt;Already give reply to you in the case you created, please check it there.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Jul 2025 02:16:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/External-Clock-For-i-MX-8M-Plus/m-p/2125950#M238865</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-07-01T02:16:14Z</dc:date>
    </item>
  </channel>
</rss>