<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 IMX6 booting enviroment issue</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-enviroment-issue/m-p/2120197#M238423</link>
    <description>&lt;P&gt;I am facing on boot environment ,&lt;BR /&gt;after successful flashing of imx-image-multimedia-imxsolosabresd.rootfs.wic file&amp;nbsp;&lt;BR /&gt;but the custom imx6s5d board is staying uboot not booting up&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 20 Jun 2025 11:39:42 GMT</pubDate>
    <dc:creator>vijay1251</dc:creator>
    <dc:date>2025-06-20T11:39:42Z</dc:date>
    <item>
      <title>IMX6 booting enviroment issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-enviroment-issue/m-p/2120197#M238423</link>
      <description>&lt;P&gt;I am facing on boot environment ,&lt;BR /&gt;after successful flashing of imx-image-multimedia-imxsolosabresd.rootfs.wic file&amp;nbsp;&lt;BR /&gt;but the custom imx6s5d board is staying uboot not booting up&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jun 2025 11:39:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-enviroment-issue/m-p/2120197#M238423</guid>
      <dc:creator>vijay1251</dc:creator>
      <dc:date>2025-06-20T11:39:42Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 booting enviroment issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-enviroment-issue/m-p/2120241#M238424</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Check the user guide document is probably that you have not enter with the desire boot in your SWs.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jun 2025 13:55:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-enviroment-issue/m-p/2120241#M238424</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-06-20T13:55:43Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 booting enviroment issue</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-enviroment-issue/m-p/2120410#M238444</link>
      <description>&lt;P&gt;The i.MX8M Nano (i.MX8MN) processor does not include a native CAN FD controller. This is why you won't find CAN FD documentation in the i.MX8MN Reference Manual.&lt;/P&gt;&lt;P&gt;However, you can still use CAN FD with the i.MX8MN by connecting an external CAN FD controller via SPI or PCIe, such as:&lt;/P&gt;&lt;P&gt;MCP2517FD (SPI-based CAN FD controller from Microchip)&lt;BR /&gt;TJA1044GT (CAN transceiver, used with external controllers)&lt;/P&gt;</description>
      <pubDate>Sat, 21 Jun 2025 01:49:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-enviroment-issue/m-p/2120410#M238444</guid>
      <dc:creator>lkuadhfe</dc:creator>
      <dc:date>2025-06-21T01:49:32Z</dc:date>
    </item>
  </channel>
</rss>