<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FRDM i.MX93 and NXP eIQ Model Zoo compatibility in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-i-MX93-and-NXP-eIQ-Model-Zoo-compatibility/m-p/2119304#M238389</link>
    <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;Is it possible in principle to evaluate NXP eIQ Model Zoo ResNet50 on an FRDM i.MX93 board?&lt;BR /&gt;I see that as per &lt;A href="https://github.com/NXP/eiq-model-zoo/tree/main/products" target="_blank" rel="noopener"&gt;NXP eIQ® Model Zoo supported platforms,&lt;/A&gt; i.MX93 in general is supported,&lt;BR /&gt;but is FRDM i.MX93 supported?&lt;/P&gt;&lt;P&gt;I try to evaluate NXP eIQ Model Zoo ResNet50 performance on an FRDM i.MX93.&lt;BR /&gt;I use the FRDM i.MX93 with its default settings: eMMC boot and followed&lt;BR /&gt;&lt;A href="https://github.com/NXP/eiq-model-zoo/blob/main/tasks/vision/classification/resnet/README.md" target="_blank" rel="noopener"&gt;NXP eIQ Model Zoo ResNet50 README&lt;/A&gt; which suggests to create TensorFlow Lite models&lt;BR /&gt;by running&amp;nbsp;bash recipe.sh.&lt;/P&gt;&lt;P&gt;To only create (not evaluate) models I needed to overcome the following hurdles:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;downgrade Python from 3.12 to 3.11 via pyenv: TensorFlow 2.12.0 demands 3.11,&lt;BR /&gt;the default image provides 3.12;&lt;/LI&gt;&lt;LI&gt;cross-compile git: pyenv needs it and the default Yocto-based image lacks it;&lt;/LI&gt;&lt;LI&gt;create an additional partition on the eMMC: model creation process easily overflows entire root partition with "No space left on device" (this implies boot from SD, gptfdisk compilation and MBR to GPT conversion);&lt;/LI&gt;&lt;LI&gt;move eiq-model-zoo repository to this additional partition, create tensorflow_datasets symlink in the home directory.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;And all this in vain as I still hit a wall with the kernel OOM Killer.&lt;BR /&gt;I can't even create&amp;nbsp;TensorFlow Lite models on the FRDM i.MX93, not to mention test its performance.&lt;/P&gt;&lt;P&gt;Any help on the matter will be appreciated.&lt;/P&gt;</description>
    <pubDate>Thu, 19 Jun 2025 09:56:14 GMT</pubDate>
    <dc:creator>goytin</dc:creator>
    <dc:date>2025-06-19T09:56:14Z</dc:date>
    <item>
      <title>FRDM i.MX93 and NXP eIQ Model Zoo compatibility</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-i-MX93-and-NXP-eIQ-Model-Zoo-compatibility/m-p/2119304#M238389</link>
      <description>&lt;P&gt;Hi.&lt;/P&gt;&lt;P&gt;Is it possible in principle to evaluate NXP eIQ Model Zoo ResNet50 on an FRDM i.MX93 board?&lt;BR /&gt;I see that as per &lt;A href="https://github.com/NXP/eiq-model-zoo/tree/main/products" target="_blank" rel="noopener"&gt;NXP eIQ® Model Zoo supported platforms,&lt;/A&gt; i.MX93 in general is supported,&lt;BR /&gt;but is FRDM i.MX93 supported?&lt;/P&gt;&lt;P&gt;I try to evaluate NXP eIQ Model Zoo ResNet50 performance on an FRDM i.MX93.&lt;BR /&gt;I use the FRDM i.MX93 with its default settings: eMMC boot and followed&lt;BR /&gt;&lt;A href="https://github.com/NXP/eiq-model-zoo/blob/main/tasks/vision/classification/resnet/README.md" target="_blank" rel="noopener"&gt;NXP eIQ Model Zoo ResNet50 README&lt;/A&gt; which suggests to create TensorFlow Lite models&lt;BR /&gt;by running&amp;nbsp;bash recipe.sh.&lt;/P&gt;&lt;P&gt;To only create (not evaluate) models I needed to overcome the following hurdles:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;downgrade Python from 3.12 to 3.11 via pyenv: TensorFlow 2.12.0 demands 3.11,&lt;BR /&gt;the default image provides 3.12;&lt;/LI&gt;&lt;LI&gt;cross-compile git: pyenv needs it and the default Yocto-based image lacks it;&lt;/LI&gt;&lt;LI&gt;create an additional partition on the eMMC: model creation process easily overflows entire root partition with "No space left on device" (this implies boot from SD, gptfdisk compilation and MBR to GPT conversion);&lt;/LI&gt;&lt;LI&gt;move eiq-model-zoo repository to this additional partition, create tensorflow_datasets symlink in the home directory.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;And all this in vain as I still hit a wall with the kernel OOM Killer.&lt;BR /&gt;I can't even create&amp;nbsp;TensorFlow Lite models on the FRDM i.MX93, not to mention test its performance.&lt;/P&gt;&lt;P&gt;Any help on the matter will be appreciated.&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jun 2025 09:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-i-MX93-and-NXP-eIQ-Model-Zoo-compatibility/m-p/2119304#M238389</guid>
      <dc:creator>goytin</dc:creator>
      <dc:date>2025-06-19T09:56:14Z</dc:date>
    </item>
  </channel>
</rss>