<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックMIMX9302CVVXDAB power consumption</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/MIMX9302CVVXDAB-power-consumption/m-p/2118607#M238334</link>
    <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am looking for better data on the powerconsumption of the rails for the&amp;nbsp;MIMX9302CVVXDAB&lt;/P&gt;&lt;P&gt;Since it is clocked down (900MHz) i expect the current to be lower. Not sure thou if i can apply lower voltage to the VDD SOC as well.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The DDR interface is also running at a lower speeed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So basically a full load measurement so that i can design a Power solution for it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;And no using the PMIC is not an option. I have a 3.3v rail and that will not change so the PMIC cannot be used.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anyone done these kind of measurements?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 18 Jun 2025 13:40:50 GMT</pubDate>
    <dc:creator>m_hjelm</dc:creator>
    <dc:date>2025-06-18T13:40:50Z</dc:date>
    <item>
      <title>MIMX9302CVVXDAB power consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX9302CVVXDAB-power-consumption/m-p/2118607#M238334</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am looking for better data on the powerconsumption of the rails for the&amp;nbsp;MIMX9302CVVXDAB&lt;/P&gt;&lt;P&gt;Since it is clocked down (900MHz) i expect the current to be lower. Not sure thou if i can apply lower voltage to the VDD SOC as well.&amp;nbsp;&lt;/P&gt;&lt;P&gt;The DDR interface is also running at a lower speeed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;So basically a full load measurement so that i can design a Power solution for it.&amp;nbsp;&lt;/P&gt;&lt;P&gt;And no using the PMIC is not an option. I have a 3.3v rail and that will not change so the PMIC cannot be used.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Has anyone done these kind of measurements?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 13:40:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX9302CVVXDAB-power-consumption/m-p/2118607#M238334</guid>
      <dc:creator>m_hjelm</dc:creator>
      <dc:date>2025-06-18T13:40:50Z</dc:date>
    </item>
    <item>
      <title>Re: MIMX9302CVVXDAB power consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX9302CVVXDAB-power-consumption/m-p/2118764#M238348</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251711"&gt;@m_hjelm&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for reaching out to NXP Support!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can refer to Application Note &lt;A href="https://www.nxp.com/docs/en/application-note/AN13917.pdf" target="_self"&gt;AN13917&lt;/A&gt;, where we present a variety of use cases along with their corresponding current consumption measurements.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jun 2025 18:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX9302CVVXDAB-power-consumption/m-p/2118764#M238348</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-06-18T18:05:40Z</dc:date>
    </item>
    <item>
      <title>Re: MIMX9302CVVXDAB power consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX9302CVVXDAB-power-consumption/m-p/2119153#M238378</link>
      <description>&lt;P&gt;Yes i have read the app note many times but i cannot find any power requirement when running the device on 900MHz, which is the only possibility of that device as well as reduced DDR speed, and full load. I do not think idle is the right test for designing the PoL of the system.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jun 2025 07:07:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX9302CVVXDAB-power-consumption/m-p/2119153#M238378</guid>
      <dc:creator>m_hjelm</dc:creator>
      <dc:date>2025-06-19T07:07:53Z</dc:date>
    </item>
    <item>
      <title>Re: MIMX9302CVVXDAB power consumption</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/MIMX9302CVVXDAB-power-consumption/m-p/2119419#M238394</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/251711"&gt;@m_hjelm&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We refer to Low Drive Mode when the processor operates at 900 MHz.&lt;/P&gt;
&lt;P&gt;All values labeled as "Low Drive Mode" in the application note correspond to the processor running at 900 MHz.&lt;/P&gt;
&lt;P&gt;Please refer to the following table for the naming conventions we use for each processor frequency.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Chavira_0-1750339445910.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/343783i998937D3DE738E94/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Chavira_0-1750339445910.png" alt="Chavira_0-1750339445910.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Chavira_0-1750339445910.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards!&lt;/P&gt;
&lt;P&gt;Chavira&lt;/P&gt;</description>
      <pubDate>Thu, 19 Jun 2025 13:53:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/MIMX9302CVVXDAB-power-consumption/m-p/2119419#M238394</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2025-06-19T13:53:35Z</dc:date>
    </item>
  </channel>
</rss>