<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic imx6ull optee peripheral access control UART or GPIO in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-optee-peripheral-access-control-UART-or-GPIO/m-p/2116964#M238258</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have optee-examples running on imx6ull board. also xtest pass all test.&lt;BR /&gt;&lt;BR /&gt;Now I want to implement access control for&amp;nbsp; UART or GPIO.&lt;/P&gt;&lt;P&gt;only TA can send/receive data over UART,&amp;nbsp;&lt;/P&gt;&lt;P&gt;or TA can toggle GPIO.&lt;/P&gt;&lt;P&gt;other then that it is not allowed to do so.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I searched online/NXP forum a lot about that, but could not get any help to get start.&lt;/P&gt;&lt;P&gt;Is there any reference or guide available?&lt;/P&gt;</description>
    <pubDate>Mon, 16 Jun 2025 13:08:47 GMT</pubDate>
    <dc:creator>Karun</dc:creator>
    <dc:date>2025-06-16T13:08:47Z</dc:date>
    <item>
      <title>imx6ull optee peripheral access control UART or GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-optee-peripheral-access-control-UART-or-GPIO/m-p/2116964#M238258</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have optee-examples running on imx6ull board. also xtest pass all test.&lt;BR /&gt;&lt;BR /&gt;Now I want to implement access control for&amp;nbsp; UART or GPIO.&lt;/P&gt;&lt;P&gt;only TA can send/receive data over UART,&amp;nbsp;&lt;/P&gt;&lt;P&gt;or TA can toggle GPIO.&lt;/P&gt;&lt;P&gt;other then that it is not allowed to do so.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I searched online/NXP forum a lot about that, but could not get any help to get start.&lt;/P&gt;&lt;P&gt;Is there any reference or guide available?&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jun 2025 13:08:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-optee-peripheral-access-control-UART-or-GPIO/m-p/2116964#M238258</guid>
      <dc:creator>Karun</dc:creator>
      <dc:date>2025-06-16T13:08:47Z</dc:date>
    </item>
    <item>
      <title>Re: imx6ull optee peripheral access control UART or GPIO</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx6ull-optee-peripheral-access-control-UART-or-GPIO/m-p/2117037#M238267</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;NXP don't have a reference for your design but you can check the current state of the system's GPIOs can be obtained in user-mode, as shown in the following example:&lt;/P&gt;
&lt;PRE&gt;cat /sys/kernel/debug/gpio&lt;/PRE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Check this note from our third party Variscite:&lt;/P&gt;
&lt;P&gt;&lt;A href="https://variwiki.com/index.php?title=MX8M_GPIO" target="_blank"&gt;https://variwiki.com/index.php?title=MX8M_GPIO&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jun 2025 14:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx6ull-optee-peripheral-access-control-UART-or-GPIO/m-p/2117037#M238267</guid>
      <dc:creator>Bio_TICFSL</dc:creator>
      <dc:date>2025-06-16T14:52:11Z</dc:date>
    </item>
  </channel>
</rss>