<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Imx6ull high speed adc in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Imx6ull-high-speed-adc/m-p/2116350#M238205</link>
    <description>&lt;P&gt;"What are the methods to implement timed periodic ADC sampling on an i.MX6ULL running Linux? I need to sample at 10 kHz to reconstruct a 1 kHz PWM wave and require low CPU usage."** **Key elements preserved in the translation:** 1. **Target Hardware:** "i.MX6ULL" (standard capitalization) 2. **OS:** "running Linux" 3. **Core Requirement:** "implement timed periodic ADC sampling" 4. **Sampling Rate:** "sample at 10 kHz" 5. **Purpose:** "to reconstruct a 1 kHz PWM wave" 6. **Constraint:** "require low CPU usage" This phrasing clearly states your technical requirements and constraints for an English-speaking audience. Good luck with your community post!&lt;/P&gt;</description>
    <pubDate>Fri, 13 Jun 2025 23:44:09 GMT</pubDate>
    <dc:creator>Yangan</dc:creator>
    <dc:date>2025-06-13T23:44:09Z</dc:date>
    <item>
      <title>Imx6ull high speed adc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6ull-high-speed-adc/m-p/2116350#M238205</link>
      <description>&lt;P&gt;"What are the methods to implement timed periodic ADC sampling on an i.MX6ULL running Linux? I need to sample at 10 kHz to reconstruct a 1 kHz PWM wave and require low CPU usage."** **Key elements preserved in the translation:** 1. **Target Hardware:** "i.MX6ULL" (standard capitalization) 2. **OS:** "running Linux" 3. **Core Requirement:** "implement timed periodic ADC sampling" 4. **Sampling Rate:** "sample at 10 kHz" 5. **Purpose:** "to reconstruct a 1 kHz PWM wave" 6. **Constraint:** "require low CPU usage" This phrasing clearly states your technical requirements and constraints for an English-speaking audience. Good luck with your community post!&lt;/P&gt;</description>
      <pubDate>Fri, 13 Jun 2025 23:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6ull-high-speed-adc/m-p/2116350#M238205</guid>
      <dc:creator>Yangan</dc:creator>
      <dc:date>2025-06-13T23:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: Imx6ull high speed adc</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Imx6ull-high-speed-adc/m-p/2117231#M238278</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Unfortunately, we do not have reference designs with external ADC IC integrated into the EVK.&lt;/P&gt;
&lt;P&gt;Usually, these implementations are done using SPI interface and our BSP has a driver to manage SPI communication devices so, I suggest you look for and IC to meet your requirements and check if driver is available to use it in your custom BSP or develop the driver.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 16 Jun 2025 21:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Imx6ull-high-speed-adc/m-p/2117231#M238278</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-06-16T21:10:51Z</dc:date>
    </item>
  </channel>
</rss>