<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックiMX8MP: P2P Failure with MiracleCast</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-P2P-Failure-with-MiracleCast/m-p/2116034#M238184</link>
    <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I’m unable to establish a P2P connection on the iMX8MP-EVK using MiracleCast (&lt;A href="https://github.com/albfan/miraclecast" target="_blank" rel="noopener noreferrer"&gt;https://github.com/albfan/miraclecast&lt;/A&gt;) for Miracast. The connection starts but fails with an “unknown” reason. Below are the details.&lt;/P&gt;&lt;H3&gt;&lt;FONT size="4"&gt;Hardware and Software Setup&lt;/FONT&gt;&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;Board&lt;/STRONG&gt;: iMX8MP-EVK (6GB)&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;Wi-Fi Module&lt;/STRONG&gt;: AW-CM276MA&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;OS&lt;/STRONG&gt;: Yocto-LF_v6.12.3-1.0.0_images_IMX8MPEVK&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;MiracleCast Version&lt;/STRONG&gt;: Latest from &lt;A href="https://github.com/albfan/miraclecast" target="_blank" rel="noopener noreferrer"&gt;https://github.com/albfan/miraclecast&lt;/A&gt;&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;Wi-Fi Interfaces&lt;/STRONG&gt;:&lt;/FONT&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;mlan0&lt;/SPAN&gt;: Station interface&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;uap0&lt;/SPAN&gt;: Access Point interface&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;wfd0&lt;SPAN&gt;: Wi-Fi Direct interface&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Steps&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;systemctl stop wpa_supplicant.service&lt;BR /&gt;sudo miracle-wifid &amp;amp;&lt;BR /&gt;sudo miracle-sinkctl&lt;BR /&gt;Select link (e.g., run 5), connection fails.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Logs&amp;nbsp;MiracleCast&lt;/STRONG&gt;&lt;BR /&gt;[ADD] Link: 5&lt;BR /&gt;[ADD] Link: 6&lt;BR /&gt;[ADD] Link: 7&lt;BR /&gt;run 5&lt;/P&gt;&lt;P&gt;[PROV] Peer: d2:39:fa:76:45:ad@5 Type: pbc&lt;BR /&gt;[GO NEG] Peer: d2:39:fa:76:45:ad@5 Type: pbc&lt;BR /&gt;[FAIL] Peer: d2:39:fa:76:45:ad@5 Reason: unknown&lt;BR /&gt;[REMOVE] Peer: d2:39:fa:76:45:ad@5&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*Attaching the Journal log&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ifconfig (mlan0 &amp;amp; wfd0)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;mlan0: flags=-28605&amp;lt;UP,BROADCAST,RUNNING,MULTICAST,DYNAMIC&amp;gt; mtu 1500&lt;BR /&gt;inet 192.168.1.106 netmask 255.255.255.0 broadcast 192.168.1.255&lt;BR /&gt;inet6 fe80::eafb:1cff:fee1:51d9 prefixlen 64 scopeid 0x20&amp;lt;link&amp;gt;&lt;BR /&gt;ether e8:fb:1c:e1:51:d9 txqueuelen 1000 (Ethernet)&lt;BR /&gt;RX packets 10 bytes 1426 (1.3 KiB)&lt;BR /&gt;RX errors 0 dropped 0 overruns 0 frame 0&lt;BR /&gt;TX packets 26 bytes 3175 (3.1 KiB)&lt;BR /&gt;TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;wfd0: flags=-28669&amp;lt;UP,BROADCAST,MULTICAST,DYNAMIC&amp;gt; mtu 1500&lt;BR /&gt;ether ea:fb:1c:e1:51:d9 txqueuelen 1000 (Ethernet)&lt;BR /&gt;RX packets 0 bytes 0 (0.0 B)&lt;BR /&gt;RX errors 0 dropped 0 overruns 0 frame 0&lt;BR /&gt;TX packets 0 bytes 0 (0.0 B)&lt;BR /&gt;TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0&lt;/P&gt;&lt;H3&gt;Observations&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;P2P negotiation starts, virtual interface (&lt;SPAN&gt;p2p-mlan0-0&lt;/SPAN&gt;) is created, and association occurs.&lt;/LI&gt;&lt;LI&gt;Connection fails with “unknown” reason; &lt;SPAN&gt;mlan0&lt;/SPAN&gt;&amp;nbsp;shows no activity.&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;rfkill: Cannot open RFKILL control device&lt;/SPAN&gt; error appears.&lt;BR /&gt;&lt;H3&gt;Questions&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;Has anyone used MiracleCast with iMX8MP-EVK ?&lt;/LI&gt;&lt;LI&gt;Are there driver/firmware updates for P2P ?&lt;/LI&gt;&lt;LI&gt;How to resolve the &lt;SPAN&gt;rfkill&lt;/SPAN&gt; error?&lt;BR /&gt;&lt;BR /&gt;&lt;P&gt;Thank you for any assistance!&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
    <pubDate>Fri, 13 Jun 2025 09:35:53 GMT</pubDate>
    <dc:creator>binil</dc:creator>
    <dc:date>2025-06-13T09:35:53Z</dc:date>
    <item>
      <title>iMX8MP: P2P Failure with MiracleCast</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-P2P-Failure-with-MiracleCast/m-p/2116034#M238184</link>
      <description>&lt;P&gt;Hello NXP Community,&lt;/P&gt;&lt;P&gt;I’m unable to establish a P2P connection on the iMX8MP-EVK using MiracleCast (&lt;A href="https://github.com/albfan/miraclecast" target="_blank" rel="noopener noreferrer"&gt;https://github.com/albfan/miraclecast&lt;/A&gt;) for Miracast. The connection starts but fails with an “unknown” reason. Below are the details.&lt;/P&gt;&lt;H3&gt;&lt;FONT size="4"&gt;Hardware and Software Setup&lt;/FONT&gt;&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;Board&lt;/STRONG&gt;: iMX8MP-EVK (6GB)&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;Wi-Fi Module&lt;/STRONG&gt;: AW-CM276MA&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;OS&lt;/STRONG&gt;: Yocto-LF_v6.12.3-1.0.0_images_IMX8MPEVK&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;MiracleCast Version&lt;/STRONG&gt;: Latest from &lt;A href="https://github.com/albfan/miraclecast" target="_blank" rel="noopener noreferrer"&gt;https://github.com/albfan/miraclecast&lt;/A&gt;&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;Wi-Fi Interfaces&lt;/STRONG&gt;:&lt;/FONT&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;mlan0&lt;/SPAN&gt;: Station interface&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;uap0&lt;/SPAN&gt;: Access Point interface&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="2"&gt;wfd0&lt;SPAN&gt;: Wi-Fi Direct interface&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Steps&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;systemctl stop wpa_supplicant.service&lt;BR /&gt;sudo miracle-wifid &amp;amp;&lt;BR /&gt;sudo miracle-sinkctl&lt;BR /&gt;Select link (e.g., run 5), connection fails.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Logs&amp;nbsp;MiracleCast&lt;/STRONG&gt;&lt;BR /&gt;[ADD] Link: 5&lt;BR /&gt;[ADD] Link: 6&lt;BR /&gt;[ADD] Link: 7&lt;BR /&gt;run 5&lt;/P&gt;&lt;P&gt;[PROV] Peer: d2:39:fa:76:45:ad@5 Type: pbc&lt;BR /&gt;[GO NEG] Peer: d2:39:fa:76:45:ad@5 Type: pbc&lt;BR /&gt;[FAIL] Peer: d2:39:fa:76:45:ad@5 Reason: unknown&lt;BR /&gt;[REMOVE] Peer: d2:39:fa:76:45:ad@5&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;*Attaching the Journal log&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ifconfig (mlan0 &amp;amp; wfd0)&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;mlan0: flags=-28605&amp;lt;UP,BROADCAST,RUNNING,MULTICAST,DYNAMIC&amp;gt; mtu 1500&lt;BR /&gt;inet 192.168.1.106 netmask 255.255.255.0 broadcast 192.168.1.255&lt;BR /&gt;inet6 fe80::eafb:1cff:fee1:51d9 prefixlen 64 scopeid 0x20&amp;lt;link&amp;gt;&lt;BR /&gt;ether e8:fb:1c:e1:51:d9 txqueuelen 1000 (Ethernet)&lt;BR /&gt;RX packets 10 bytes 1426 (1.3 KiB)&lt;BR /&gt;RX errors 0 dropped 0 overruns 0 frame 0&lt;BR /&gt;TX packets 26 bytes 3175 (3.1 KiB)&lt;BR /&gt;TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;wfd0: flags=-28669&amp;lt;UP,BROADCAST,MULTICAST,DYNAMIC&amp;gt; mtu 1500&lt;BR /&gt;ether ea:fb:1c:e1:51:d9 txqueuelen 1000 (Ethernet)&lt;BR /&gt;RX packets 0 bytes 0 (0.0 B)&lt;BR /&gt;RX errors 0 dropped 0 overruns 0 frame 0&lt;BR /&gt;TX packets 0 bytes 0 (0.0 B)&lt;BR /&gt;TX errors 0 dropped 0 overruns 0 carrier 0 collisions 0&lt;/P&gt;&lt;H3&gt;Observations&lt;/H3&gt;&lt;UL&gt;&lt;LI&gt;P2P negotiation starts, virtual interface (&lt;SPAN&gt;p2p-mlan0-0&lt;/SPAN&gt;) is created, and association occurs.&lt;/LI&gt;&lt;LI&gt;Connection fails with “unknown” reason; &lt;SPAN&gt;mlan0&lt;/SPAN&gt;&amp;nbsp;shows no activity.&lt;/LI&gt;&lt;LI&gt;&lt;SPAN&gt;rfkill: Cannot open RFKILL control device&lt;/SPAN&gt; error appears.&lt;BR /&gt;&lt;H3&gt;Questions&lt;/H3&gt;&lt;OL&gt;&lt;LI&gt;Has anyone used MiracleCast with iMX8MP-EVK ?&lt;/LI&gt;&lt;LI&gt;Are there driver/firmware updates for P2P ?&lt;/LI&gt;&lt;LI&gt;How to resolve the &lt;SPAN&gt;rfkill&lt;/SPAN&gt; error?&lt;BR /&gt;&lt;BR /&gt;&lt;P&gt;Thank you for any assistance!&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Fri, 13 Jun 2025 09:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-P2P-Failure-with-MiracleCast/m-p/2116034#M238184</guid>
      <dc:creator>binil</dc:creator>
      <dc:date>2025-06-13T09:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: iMX8MP: P2P Failure with MiracleCast</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-P2P-Failure-with-MiracleCast/m-p/2116332#M238204</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;And thank you for your detailed observation, from NXP side, we have not tested the repository attached, I can't tell if it works with Linux BSP but I can see that you will use P2P connection, from our side I can suggest that P2P needs to be enabled in driver config.&lt;/P&gt;
&lt;P&gt;Refer to&amp;nbsp;2.6 Configure and test Wi-Fi direct from&amp;nbsp;&lt;STRONG&gt;Feature Configuration Guide for NXP-based Wireless Modules on i.MX 8M Quad EVK&lt;/STRONG&gt;.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Fri, 13 Jun 2025 21:46:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/iMX8MP-P2P-Failure-with-MiracleCast/m-p/2116332#M238204</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-06-13T21:46:01Z</dc:date>
    </item>
  </channel>
</rss>