<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Monitoring M7 firmware run from u-boot in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Monitoring-M7-firmware-run-from-u-boot/m-p/2114781#M238107</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;this is because how the Cortex-M was lunched is different, in case for attached as shown in the remoteproc code:&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="com"&gt;If the remote processor has been started by an external&amp;nbsp;entity we have no idea of what image it is running. As such&amp;nbsp;simply display a generic string.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 11 Jun 2025 22:03:04 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2025-06-11T22:03:04Z</dc:date>
    <item>
      <title>Monitoring M7 firmware run from u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Monitoring-M7-firmware-run-from-u-boot/m-p/2113746#M238049</link>
      <description>&lt;P&gt;Hi, I run a M7 firmware from u-boot with the commands:&lt;/P&gt;&lt;P&gt;fatload mmc 1:1 0x48000000 rpmsg_lite_str_echo_rtos.bin;cp.b 0x48000000 0x7e0000 20000&lt;BR /&gt;bootaux 0x7e0000&lt;/P&gt;&lt;P&gt;and it works but when I check the status from /sys/class/remoteproc/remoteproc0/state I have "attached" but the M7 is running&lt;/P&gt;&lt;P&gt;Instead when I run M7 from linux the state is "running" as I expected&lt;/P&gt;&lt;P&gt;echo stop &amp;gt; /sys/class/remoteproc/remoteproc0/state&lt;BR /&gt;echo rpmsg_lite_str_echo_rtos_imxcm7.elf &amp;gt; /sys/class/remoteproc/remoteproc0/firmware&lt;BR /&gt;echo start &amp;gt; /sys/class/remoteproc/remoteproc0/state&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Why? I'm using yocto kirkstone with kernel 5.15.71, and I have an imx8mplus.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Jun 2025 16:24:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Monitoring-M7-firmware-run-from-u-boot/m-p/2113746#M238049</guid>
      <dc:creator>mirkoardinghi1</dc:creator>
      <dc:date>2025-06-10T16:24:59Z</dc:date>
    </item>
    <item>
      <title>Re: Monitoring M7 firmware run from u-boot</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Monitoring-M7-firmware-run-from-u-boot/m-p/2114781#M238107</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;this is because how the Cortex-M was lunched is different, in case for attached as shown in the remoteproc code:&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="com"&gt;If the remote processor has been started by an external&amp;nbsp;entity we have no idea of what image it is running. As such&amp;nbsp;simply display a generic string.&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jun 2025 22:03:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Monitoring-M7-firmware-run-from-u-boot/m-p/2114781#M238107</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-06-11T22:03:04Z</dc:date>
    </item>
  </channel>
</rss>