<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic The VSNVS voltage of the PF3000 remains at 1.159V even though VIN is set to 4.0V. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/The-VSNVS-voltage-of-the-PF3000-remains-at-1-159V-even-though/m-p/2112668#M238001</link>
    <description>&lt;P&gt;HI.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The VSNVS voltage of the PF3000 remains at 1.159V even though VIN is set to 4.0V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I thought that if I set VIN to 4.0V, it would unconditionally become 3.0V.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; Is there some setting?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Thank you.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 09 Jun 2025 08:00:35 GMT</pubDate>
    <dc:creator>tamotsu</dc:creator>
    <dc:date>2025-06-09T08:00:35Z</dc:date>
    <item>
      <title>The VSNVS voltage of the PF3000 remains at 1.159V even though VIN is set to 4.0V.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-VSNVS-voltage-of-the-PF3000-remains-at-1-159V-even-though/m-p/2112668#M238001</link>
      <description>&lt;P&gt;HI.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;The VSNVS voltage of the PF3000 remains at 1.159V even though VIN is set to 4.0V.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I thought that if I set VIN to 4.0V, it would unconditionally become 3.0V.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; Is there some setting?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Thank you.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jun 2025 08:00:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-VSNVS-voltage-of-the-PF3000-remains-at-1-159V-even-though/m-p/2112668#M238001</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-06-09T08:00:35Z</dc:date>
    </item>
    <item>
      <title>Re: The VSNVS voltage of the PF3000 remains at 1.159V even though VIN is set to 4.0V.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-VSNVS-voltage-of-the-PF3000-remains-at-1-159V-even-though/m-p/2112963#M238008</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;According to datasheet, when the coin cell is applied for the very first time, VSNVS outputs 1.0 V. Only when VIN is applied thereafter does VSNVS transition to its default value. Upon subsequent removal of VIN, with the coin cell attached, VSNVS changes configuration from an LDO to a switch, provided certain conditions are met as described in Table 67.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Mon, 09 Jun 2025 17:35:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-VSNVS-voltage-of-the-PF3000-remains-at-1-159V-even-though/m-p/2112963#M238008</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-06-09T17:35:11Z</dc:date>
    </item>
    <item>
      <title>Re: The VSNVS voltage of the PF3000 remains at 1.159V even though VIN is set to 4.0V.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/The-VSNVS-voltage-of-the-PF3000-remains-at-1-159V-even-though/m-p/2113095#M238012</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I understood it well.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt; Thanks to your help, &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I was able to solve the problem.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Jun 2025 00:51:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/The-VSNVS-voltage-of-the-PF3000-remains-at-1-159V-even-though/m-p/2113095#M238012</guid>
      <dc:creator>tamotsu</dc:creator>
      <dc:date>2025-06-10T00:51:53Z</dc:date>
    </item>
  </channel>
</rss>