<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックI.MX device-tree overlay implement</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-device-tree-overlay-implement/m-p/2110106#M237874</link>
    <description>&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; How to load dtbo (overlay file) in runtime.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; An example for imx8mp, In kernel 6.1.36 there have&amp;nbsp;imx8mp-evk-revb4.dtbo and it merge with others DTB file to generate a new one like :&lt;/P&gt;&lt;P&gt;imx8mp-evk-revb4-ov2775-dtbs = imx8mp-evk-ov2775.dtb imx8mp-evk-revb4.dtbo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;In this case can we use&amp;nbsp;imx8mp-evk-ov2775.dtb and runtime load&amp;nbsp;imx8mp-evk-revb4.dtbo ?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; If the answer is yes, how to do that ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;</description>
    <pubDate>Wed, 04 Jun 2025 06:36:54 GMT</pubDate>
    <dc:creator>charleshuang</dc:creator>
    <dc:date>2025-06-04T06:36:54Z</dc:date>
    <item>
      <title>I.MX device-tree overlay implement</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-device-tree-overlay-implement/m-p/2110106#M237874</link>
      <description>&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; How to load dtbo (overlay file) in runtime.&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; An example for imx8mp, In kernel 6.1.36 there have&amp;nbsp;imx8mp-evk-revb4.dtbo and it merge with others DTB file to generate a new one like :&lt;/P&gt;&lt;P&gt;imx8mp-evk-revb4-ov2775-dtbs = imx8mp-evk-ov2775.dtb imx8mp-evk-revb4.dtbo&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp;In this case can we use&amp;nbsp;imx8mp-evk-ov2775.dtb and runtime load&amp;nbsp;imx8mp-evk-revb4.dtbo ?&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; If the answer is yes, how to do that ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;Sean&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jun 2025 06:36:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX-device-tree-overlay-implement/m-p/2110106#M237874</guid>
      <dc:creator>charleshuang</dc:creator>
      <dc:date>2025-06-04T06:36:54Z</dc:date>
    </item>
    <item>
      <title>Re: I.MX device-tree overlay implement</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/I-MX-device-tree-overlay-implement/m-p/2111005#M237926</link>
      <description>&lt;P&gt;the purpose of your request is that you wan to add or remove dtbo file dynamically, right?&lt;/P&gt;
&lt;P&gt;you can refer to the document as below, which is verified on nxp bsp,&amp;nbsp;&lt;SPAN&gt;if/else test can meet your request or not&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-use-linux-device-tree-overlay-from-u-boot-and-apply-it/ta-p/1896858" target="_blank"&gt;How to use linux device tree overlay from u-boot and apply it automatically - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;you also can refer to&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://forums.raspberrypi.com/viewtopic.php?t=99401" target="_blank"&gt;Device tree overlay - dynamic load and unload - Raspberry Pi Forums&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://raspberrypi.stackexchange.com/questions/136839/using-the-dynamic-device-tree-to-add-overlays-at-run-time" target="_blank"&gt;pi 4 - Using the Dynamic Device Tree to add Overlays at Run Time - Raspberry Pi Stack Exchange&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jun 2025 06:44:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/I-MX-device-tree-overlay-implement/m-p/2111005#M237926</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-06-05T06:44:02Z</dc:date>
    </item>
  </channel>
</rss>