<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックSPDIFTxClk Register, TxClk_Source field. Valid options??</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/SPDIFTxClk-Register-TxClk-Source-field-Valid-options/m-p/2108796#M237825</link>
    <description>&lt;P&gt;I'm trying to write an SPDIF driver, and referencing this manual:&lt;/P&gt;&lt;P&gt;i.MX 8M Mini Applications Processor Reference Manual, Document Number: IMX8MMRM,&amp;nbsp;Rev. 3, 11/2020&lt;/P&gt;&lt;P&gt;On page 4211, the&amp;nbsp;SPDIFTxClk is described. bits 8-10 are the TxClk_Source field. However, I only see one option:&lt;/P&gt;&lt;P&gt;0000 - Clock selection from Audio Clock Mux (ACM).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1-What is the Audio Clock Mux??? There's no other references to the definition of that in this manual.&lt;/P&gt;&lt;P&gt;2-There is room for 8 options, yet only Option 0x0000 is given here. There must be more? The initialize function for the FSL library sets this field to 0x1 (!?)&lt;/P&gt;</description>
    <pubDate>Mon, 02 Jun 2025 17:15:29 GMT</pubDate>
    <dc:creator>sgordon777</dc:creator>
    <dc:date>2025-06-02T17:15:29Z</dc:date>
    <item>
      <title>SPDIFTxClk Register, TxClk_Source field. Valid options??</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/SPDIFTxClk-Register-TxClk-Source-field-Valid-options/m-p/2108796#M237825</link>
      <description>&lt;P&gt;I'm trying to write an SPDIF driver, and referencing this manual:&lt;/P&gt;&lt;P&gt;i.MX 8M Mini Applications Processor Reference Manual, Document Number: IMX8MMRM,&amp;nbsp;Rev. 3, 11/2020&lt;/P&gt;&lt;P&gt;On page 4211, the&amp;nbsp;SPDIFTxClk is described. bits 8-10 are the TxClk_Source field. However, I only see one option:&lt;/P&gt;&lt;P&gt;0000 - Clock selection from Audio Clock Mux (ACM).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;1-What is the Audio Clock Mux??? There's no other references to the definition of that in this manual.&lt;/P&gt;&lt;P&gt;2-There is room for 8 options, yet only Option 0x0000 is given here. There must be more? The initialize function for the FSL library sets this field to 0x1 (!?)&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 17:15:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/SPDIFTxClk-Register-TxClk-Source-field-Valid-options/m-p/2108796#M237825</guid>
      <dc:creator>sgordon777</dc:creator>
      <dc:date>2025-06-02T17:15:29Z</dc:date>
    </item>
  </channel>
</rss>