<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX8MQ MIPI DSI - Waveshare panel in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-MIPI-DSI-Waveshare-panel/m-p/2108563#M237812</link>
    <description>&lt;P&gt;Hi all,&lt;BR /&gt;&lt;BR /&gt;I'm trying to connect a waveshare panel via mipi dsi to my imx8mq board using a custom ffc. I used the lcdif controller of the imx, but it seems that I have clocks timing issues that I can't figure out.&lt;BR /&gt;&lt;BR /&gt;I'm using the &lt;A title="waveshare 10.1-DSI-TOUCH-A" href="https://www.waveshare.com/wiki/10.1-DSI-TOUCH-A" target="_self"&gt;waveshare 10.1-DSI-TOUCH-A&lt;/A&gt; and the drivers &lt;A title="panel waveshare dsi drivers" href="https://files.waveshare.com/wiki/common/Panel-waveshare-dsi2-driver.zip" target="_blank" rel="noopener"&gt;https://files.waveshare.com/wiki/common/Panel-waveshare-dsi2-driver.zip&lt;/A&gt;.&lt;BR /&gt;&lt;SPAN class=""&gt;Furthermore&lt;/SPAN&gt;, I'm working with linux kernel 5.15.71.&lt;BR /&gt;&lt;BR /&gt;I have currently no errors related to the drivers and the backlight works properly, but there are no pixels on screen. I checked by charging the HDMI overlay, which is working.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Based on my screen, I could verify and calculated the following:&lt;BR /&gt;- pixels_per_second: 1280 * 800 * 60 * 24 = 1_474_560_000 ~= 1,47Gpixels/sec&lt;BR /&gt;- pixelclock: (800 + 40 + 20 + 20) × (1280 + 20 + 4 + 20) × 60 = 69_907_200 ~= 70_000_000 = 70_000kHz&lt;BR /&gt;- bit_clk = pixelclock * bits_per_pixel / number_of_lanes = 70_000_000 * 24 / 2 = 840_000_000 = 840MHz&lt;BR /&gt;&lt;BR /&gt;I tried to apply them to my dsi overlay without success.&lt;BR /&gt;I linked the default values on which my overlay is based (cf files maaxboard.dts and imx8mq.dtsi named imx8mq.dts because of the forum restrictions), and the overlay I changed (named display-mipi.dts).&lt;BR /&gt;&lt;BR /&gt;Do you have any advice on how to configure clocks for lcdif controller (or even DCSS controller) ?&lt;BR /&gt;&lt;BR /&gt;Thanks for your time.&lt;/P&gt;</description>
    <pubDate>Mon, 02 Jun 2025 09:25:01 GMT</pubDate>
    <dc:creator>RomainLt</dc:creator>
    <dc:date>2025-06-02T09:25:01Z</dc:date>
    <item>
      <title>IMX8MQ MIPI DSI - Waveshare panel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-MIPI-DSI-Waveshare-panel/m-p/2108563#M237812</link>
      <description>&lt;P&gt;Hi all,&lt;BR /&gt;&lt;BR /&gt;I'm trying to connect a waveshare panel via mipi dsi to my imx8mq board using a custom ffc. I used the lcdif controller of the imx, but it seems that I have clocks timing issues that I can't figure out.&lt;BR /&gt;&lt;BR /&gt;I'm using the &lt;A title="waveshare 10.1-DSI-TOUCH-A" href="https://www.waveshare.com/wiki/10.1-DSI-TOUCH-A" target="_self"&gt;waveshare 10.1-DSI-TOUCH-A&lt;/A&gt; and the drivers &lt;A title="panel waveshare dsi drivers" href="https://files.waveshare.com/wiki/common/Panel-waveshare-dsi2-driver.zip" target="_blank" rel="noopener"&gt;https://files.waveshare.com/wiki/common/Panel-waveshare-dsi2-driver.zip&lt;/A&gt;.&lt;BR /&gt;&lt;SPAN class=""&gt;Furthermore&lt;/SPAN&gt;, I'm working with linux kernel 5.15.71.&lt;BR /&gt;&lt;BR /&gt;I have currently no errors related to the drivers and the backlight works properly, but there are no pixels on screen. I checked by charging the HDMI overlay, which is working.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Based on my screen, I could verify and calculated the following:&lt;BR /&gt;- pixels_per_second: 1280 * 800 * 60 * 24 = 1_474_560_000 ~= 1,47Gpixels/sec&lt;BR /&gt;- pixelclock: (800 + 40 + 20 + 20) × (1280 + 20 + 4 + 20) × 60 = 69_907_200 ~= 70_000_000 = 70_000kHz&lt;BR /&gt;- bit_clk = pixelclock * bits_per_pixel / number_of_lanes = 70_000_000 * 24 / 2 = 840_000_000 = 840MHz&lt;BR /&gt;&lt;BR /&gt;I tried to apply them to my dsi overlay without success.&lt;BR /&gt;I linked the default values on which my overlay is based (cf files maaxboard.dts and imx8mq.dtsi named imx8mq.dts because of the forum restrictions), and the overlay I changed (named display-mipi.dts).&lt;BR /&gt;&lt;BR /&gt;Do you have any advice on how to configure clocks for lcdif controller (or even DCSS controller) ?&lt;BR /&gt;&lt;BR /&gt;Thanks for your time.&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jun 2025 09:25:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-MIPI-DSI-Waveshare-panel/m-p/2108563#M237812</guid>
      <dc:creator>RomainLt</dc:creator>
      <dc:date>2025-06-02T09:25:01Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8MQ MIPI DSI - Waveshare panel</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-MIPI-DSI-Waveshare-panel/m-p/2112350#M237973</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Please have a look to the following community thread:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-config-MIPI-DSI-clock-and-data-rate-on-imx8mq/m-p/1041683" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/How-to-config-MIPI-DSI-clock-and-data-rate-on-imx8mq/m-p/1041683&lt;/A&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards/Saludos,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Sat, 07 Jun 2025 00:38:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX8MQ-MIPI-DSI-Waveshare-panel/m-p/2112350#M237973</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2025-06-07T00:38:38Z</dc:date>
    </item>
  </channel>
</rss>