<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ROM  boot from secondary container when secondary has higher SW version. in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/ROM-boot-from-secondary-container-when-secondary-has-higher-SW/m-p/2104813#M237645</link>
    <description>&lt;P&gt;&lt;A href="https://patches.linaro.org/project/u-boot/patch/1591698884-72174-3-git-send-email-ye.li@nxp.com/" target="_blank" rel="noopener"&gt;https://patches.linaro.org/project/u-boot/patch/1591698884-72174-3-git-send-email-ye.li@nxp.com/&lt;/A&gt;&lt;BR /&gt;On i.MX8QM B0 and i.MX8QXP C0, ROM supports to boot from secondary&lt;BR /&gt;container set when either booting from primary container set is failed&lt;BR /&gt;or secondary container set has higher SW version.&lt;BR /&gt;根据这个帖子的描述，rom 可以在secondary container 拥有更高版本号的时候主动选择secondary container。&lt;BR /&gt;我想知道都有哪些芯片支持这个特性，有没有官方文档，我们在调研新机种，需要知道哪些imx8 芯片支持这个特性&lt;/P&gt;</description>
    <pubDate>Tue, 27 May 2025 04:54:54 GMT</pubDate>
    <dc:creator>liuchao2665</dc:creator>
    <dc:date>2025-05-27T04:54:54Z</dc:date>
    <item>
      <title>ROM  boot from secondary container when secondary has higher SW version.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ROM-boot-from-secondary-container-when-secondary-has-higher-SW/m-p/2104813#M237645</link>
      <description>&lt;P&gt;&lt;A href="https://patches.linaro.org/project/u-boot/patch/1591698884-72174-3-git-send-email-ye.li@nxp.com/" target="_blank" rel="noopener"&gt;https://patches.linaro.org/project/u-boot/patch/1591698884-72174-3-git-send-email-ye.li@nxp.com/&lt;/A&gt;&lt;BR /&gt;On i.MX8QM B0 and i.MX8QXP C0, ROM supports to boot from secondary&lt;BR /&gt;container set when either booting from primary container set is failed&lt;BR /&gt;or secondary container set has higher SW version.&lt;BR /&gt;根据这个帖子的描述，rom 可以在secondary container 拥有更高版本号的时候主动选择secondary container。&lt;BR /&gt;我想知道都有哪些芯片支持这个特性，有没有官方文档，我们在调研新机种，需要知道哪些imx8 芯片支持这个特性&lt;/P&gt;</description>
      <pubDate>Tue, 27 May 2025 04:54:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ROM-boot-from-secondary-container-when-secondary-has-higher-SW/m-p/2104813#M237645</guid>
      <dc:creator>liuchao2665</dc:creator>
      <dc:date>2025-05-27T04:54:54Z</dc:date>
    </item>
    <item>
      <title>Re: ROM  boot from secondary container when secondary has higher SW version.</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/ROM-boot-from-secondary-container-when-secondary-has-higher-SW/m-p/2111011#M237927</link>
      <description>&lt;P&gt;it seems this is only for imx8qm/imx8qxp, for other processors, like imx8mp, you can refer to the RM&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="joanxie_0-1749106039792.png" style="width: 488px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/341534iABE1C17BEEA5EEFA/image-dimensions/488x89?v=v2" width="488" height="89" role="button" title="joanxie_0-1749106039792.png" alt="joanxie_0-1749106039792.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Jun 2025 06:47:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/ROM-boot-from-secondary-container-when-secondary-has-higher-SW/m-p/2111011#M237927</guid>
      <dc:creator>joanxie</dc:creator>
      <dc:date>2025-06-05T06:47:32Z</dc:date>
    </item>
  </channel>
</rss>