<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: IBIS Model Missing Differential Pair Description RT685</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-Missing-Differential-Pair-Description-RT685/m-p/2103768#M237550</link>
    <description>&lt;P&gt;Also looking to see if there is a possibility to run aggressor simulations on this USB pair with either a working IBIS model for this part or a similar part.&lt;/P&gt;</description>
    <pubDate>Fri, 23 May 2025 21:39:45 GMT</pubDate>
    <dc:creator>mkoven1226</dc:creator>
    <dc:date>2025-05-23T21:39:45Z</dc:date>
    <item>
      <title>IBIS Model Missing Differential Pair Description RT685</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-Missing-Differential-Pair-Description-RT685/m-p/2080160#M236291</link>
      <description>&lt;P&gt;I'm trying to run Hyperlynx simulations using the IBIS model provided by NXP for the RT685- FOWLP249 and there are no differential pairs defined in the files. Balls U2 and T1 should be USB0_DP and USB0_DM respectively, but these are defined as "NC" in the IBIS file, which causes the simulation to fail. Does anyone have experience with changing these to diff pairs? Here's a cut and paste from the IBIS file:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;U2 USB0_DP NC 0.49555 2.721e-09 6.162e-13&lt;/P&gt;&lt;P&gt;T1 USB0_DM NC 0.50751 2.703e-09 6.205e-13&lt;/P&gt;</description>
      <pubDate>Mon, 14 Apr 2025 17:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-Missing-Differential-Pair-Description-RT685/m-p/2080160#M236291</guid>
      <dc:creator>mkoven1226</dc:creator>
      <dc:date>2025-04-14T17:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: IBIS Model Missing Differential Pair Description RT685</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-Missing-Differential-Pair-Description-RT685/m-p/2103768#M237550</link>
      <description>&lt;P&gt;Also looking to see if there is a possibility to run aggressor simulations on this USB pair with either a working IBIS model for this part or a similar part.&lt;/P&gt;</description>
      <pubDate>Fri, 23 May 2025 21:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IBIS-Model-Missing-Differential-Pair-Description-RT685/m-p/2103768#M237550</guid>
      <dc:creator>mkoven1226</dc:creator>
      <dc:date>2025-05-23T21:39:45Z</dc:date>
    </item>
  </channel>
</rss>