<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Updating the M-Core image without the bootloader (iMX8ULP) in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Updating-the-M-Core-image-without-the-bootloader-iMX8ULP/m-p/2103074#M237513</link>
    <description>&lt;P&gt;As you can see the support from the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-M33-firmware-using-remoteproc-on-iMX8ULP/m-p/2044380/highlight/false#M234007" target="_self"&gt;update-the-M33-firmware-using-remoteproc-on-iMX8ULP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With checking internal team, so far, no definitive reply for our BSP.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Fri, 23 May 2025 02:41:24 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2025-05-23T02:41:24Z</dc:date>
    <item>
      <title>Updating the M-Core image without the bootloader (iMX8ULP)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Updating-the-M-Core-image-without-the-bootloader-iMX8ULP/m-p/2097259#M237205</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I want to update the M-core image without modifying the bootloader. Typically, the flash.bin file contains components such as the AHAB container, UPower firmware, U-Boot, and the M-core binary. However, I only want to update the M-core image, not the bootloader or other components.&lt;/P&gt;&lt;P&gt;Is it possible to do this?&lt;BR /&gt;&lt;BR /&gt;If yes how can I make that image and how can I flash it?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;RDS&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 May 2025 10:35:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Updating-the-M-Core-image-without-the-bootloader-iMX8ULP/m-p/2097259#M237205</guid>
      <dc:creator>dhruvinrajpura</dc:creator>
      <dc:date>2025-05-14T10:35:36Z</dc:date>
    </item>
    <item>
      <title>Re: Updating the M-Core image without the bootloader (iMX8ULP)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Updating-the-M-Core-image-without-the-bootloader-iMX8ULP/m-p/2097675#M237230</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please have a reference from the Chapter 4 of&amp;nbsp;&lt;A href="https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf" target="_self"&gt;This guide&lt;/A&gt;&amp;nbsp;there are guides related to M core images&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Thu, 15 May 2025 02:36:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Updating-the-M-Core-image-without-the-bootloader-iMX8ULP/m-p/2097675#M237230</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-05-15T02:36:40Z</dc:date>
    </item>
    <item>
      <title>Re: Updating the M-Core image without the bootloader (iMX8ULP)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Updating-the-M-Core-image-without-the-bootloader-iMX8ULP/m-p/2098010#M237249</link>
      <description>&lt;P&gt;Hi Harvey,&lt;BR /&gt;I have already gone through that reference manual, but unfortunately, it does not contain the section for i.MX8ULP (section 4.7.4).&lt;/P&gt;&lt;P&gt;I did find some community posts mentioning that on i.MX93, we can use remoteproc to update the M-core image from the A-core. I’m wondering if someone has already patched this functionality into the i.MX8ULP, and whether we can use it now?&lt;BR /&gt;&lt;BR /&gt;Here are links for those posts:&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-remoteproc-error-and-how-to-run-different-binaries-on/m-p/1852541" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/i-MX8ULP-remoteproc-error-and-how-to-run-different-binaries-on/m-p/1852541&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-M33-firmware-using-remoteproc-on-iMX8ULP/m-p/2044380/highlight/false#M234007" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-M33-firmware-using-remoteproc-on-iMX8ULP/m-p/2044380/highlight/false#M234007&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 15 May 2025 09:24:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Updating-the-M-Core-image-without-the-bootloader-iMX8ULP/m-p/2098010#M237249</guid>
      <dc:creator>dhruvinrajpura</dc:creator>
      <dc:date>2025-05-15T09:24:03Z</dc:date>
    </item>
    <item>
      <title>Re: Updating the M-Core image without the bootloader (iMX8ULP)</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Updating-the-M-Core-image-without-the-bootloader-iMX8ULP/m-p/2103074#M237513</link>
      <description>&lt;P&gt;As you can see the support from the&amp;nbsp;&lt;A href="https://community.nxp.com/t5/i-MX-Processors/How-to-update-the-M33-firmware-using-remoteproc-on-iMX8ULP/m-p/2044380/highlight/false#M234007" target="_self"&gt;update-the-M33-firmware-using-remoteproc-on-iMX8ULP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With checking internal team, so far, no definitive reply for our BSP.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 23 May 2025 02:41:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Updating-the-M-Core-image-without-the-bootloader-iMX8ULP/m-p/2103074#M237513</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-05-23T02:41:24Z</dc:date>
    </item>
  </channel>
</rss>