<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX28 gstreamer equalizer performance in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-gstreamer-equalizer-performance/m-p/253916#M23744</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am writing a app using gstreamer 0.10.35 on the IMX28 eval kit for audio playback only. The following command to play a .wav file works fine. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# gst-launch filesrc location=test.wav ! decodebin ! alsasink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I try adding the equalizer-10bands plugin into the pipeline then audio playback starts to stutter badly and CPU usage jumps to 100%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# gst-launch filesrc location=test.wav ! decodebin ! equalizer-10bands band0=1.0 ! alsasink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 3 band equalizer is usable but still uses up a lot of CPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is there something I can do to improve the performance? Or is the IMX28 just not capable of doing software equalization?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jan 2014 23:09:17 GMT</pubDate>
    <dc:creator>tomdeacon</dc:creator>
    <dc:date>2014-01-23T23:09:17Z</dc:date>
    <item>
      <title>IMX28 gstreamer equalizer performance</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX28-gstreamer-equalizer-performance/m-p/253916#M23744</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am writing a app using gstreamer 0.10.35 on the IMX28 eval kit for audio playback only. The following command to play a .wav file works fine. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# gst-launch filesrc location=test.wav ! decodebin ! alsasink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I try adding the equalizer-10bands plugin into the pipeline then audio playback starts to stutter badly and CPU usage jumps to 100%.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# gst-launch filesrc location=test.wav ! decodebin ! equalizer-10bands band0=1.0 ! alsasink&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The 3 band equalizer is usable but still uses up a lot of CPU.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is there something I can do to improve the performance? Or is the IMX28 just not capable of doing software equalization?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jan 2014 23:09:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX28-gstreamer-equalizer-performance/m-p/253916#M23744</guid>
      <dc:creator>tomdeacon</dc:creator>
      <dc:date>2014-01-23T23:09:17Z</dc:date>
    </item>
  </channel>
</rss>