<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックCan't Program Flash for i.MX RT1180 EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-Program-Flash-for-i-MX-RT1180-EVK/m-p/2097514#M237217</link>
    <description>&lt;P&gt;I can debug through LinkServer or JLink just fine but when I try to Program Flash it fails. I have attached the Console output for the LinkServer. I am trying to flash and boot from FlexSPI qspi. Any help on this would be great thanks.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 14 May 2025 20:07:25 GMT</pubDate>
    <dc:creator>jett</dc:creator>
    <dc:date>2025-05-14T20:07:25Z</dc:date>
    <item>
      <title>Can't Program Flash for i.MX RT1180 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-Program-Flash-for-i-MX-RT1180-EVK/m-p/2097514#M237217</link>
      <description>&lt;P&gt;I can debug through LinkServer or JLink just fine but when I try to Program Flash it fails. I have attached the Console output for the LinkServer. I am trying to flash and boot from FlexSPI qspi. Any help on this would be great thanks.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 May 2025 20:07:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-Program-Flash-for-i-MX-RT1180-EVK/m-p/2097514#M237217</guid>
      <dc:creator>jett</dc:creator>
      <dc:date>2025-05-14T20:07:25Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Program Flash for i.MX RT1180 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-Program-Flash-for-i-MX-RT1180-EVK/m-p/2097648#M237227</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242681"&gt;@jett&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The project you want to program into the flash is a RAM target indeed, as it is for M7 which is not the default boot core of RT1180.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_0-1747273395216.png" style="width: 602px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/337842i257AEF3E6702A629/image-dimensions/602x194?v=v2" width="602" height="194" role="button" title="Kan_Li_0-1747273395216.png" alt="Kan_Li_0-1747273395216.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Kan_Li_0-1747273395216.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please use the project for M33 instead.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Kan_Li_1-1747273496211.png" style="width: 600px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/337843iAAB9F9B267182036/image-dimensions/600x270?v=v2" width="600" height="270" role="button" title="Kan_Li_1-1747273496211.png" alt="Kan_Li_1-1747273496211.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Kan_Li_1-1747273496211.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;Kan&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;BR /&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 May 2025 01:45:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-Program-Flash-for-i-MX-RT1180-EVK/m-p/2097648#M237227</guid>
      <dc:creator>Kan_Li</dc:creator>
      <dc:date>2025-05-15T01:45:46Z</dc:date>
    </item>
    <item>
      <title>Re: Can't Program Flash for i.MX RT1180 EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Can-t-Program-Flash-for-i-MX-RT1180-EVK/m-p/2098144#M237255</link>
      <description>Thank you and I also didn't see AN14589 cleared up my remaining boot questions</description>
      <pubDate>Thu, 15 May 2025 12:11:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Can-t-Program-Flash-for-i-MX-RT1180-EVK/m-p/2098144#M237255</guid>
      <dc:creator>jett</dc:creator>
      <dc:date>2025-05-15T12:11:56Z</dc:date>
    </item>
  </channel>
</rss>