<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックPreforming Basic Image Programming onto an IMX93EVK</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Preforming-Basic-Image-Programming-onto-an-IMX93EVK/m-p/2095886#M237141</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Using the prebuilt images from NXP, available here: &lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt; I have attempted to program my IMX93EVK with these images including both the 6.12 kernel builds and the 6.6.52 for the IMX93EVK.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;All of my attempts, when it seems uuu can recognize the board, have ended with the following message:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;"'C:\Users\kleavell\Downloads\uuu(1).exe' .\uuu.auto uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.182-0-gda3cd53 Success 0 Failure 1 1:91-2F0B37F 1/ 1 [HID(W): LIBUSB_ERROR_PIPE (-9) ] SDPS: boot -f imx-boot-imx93-1 PS C:\Users\kleavell\Desktop\reference\LF_v6.12.3-1.0.0_images_IMX93EVK&amp;gt;" &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I have done some poking around and it seems that uuu.exe recognizes the board as a IMX93 as it shows up when I issue a `uuu.exe -lsusb`. Any ideas on what could be going wrong?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I have configured the board boot like so:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;dip switch 1301 has the pins at the following state when it seems like my board is recognized by uuu: 1234 respectively are 1100 based on the silk screen next to the switch.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kleavell_1-1747101876623.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/337314i5FC61F23AAD184A2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kleavell_1-1747101876623.jpeg" alt="kleavell_1-1747101876623.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;kleavell_1-1747101876623.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any thoughts are appreciated!&lt;/P&gt;</description>
    <pubDate>Tue, 13 May 2025 02:07:39 GMT</pubDate>
    <dc:creator>kleavell</dc:creator>
    <dc:date>2025-05-13T02:07:39Z</dc:date>
    <item>
      <title>Preforming Basic Image Programming onto an IMX93EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Preforming-Basic-Image-Programming-onto-an-IMX93EVK/m-p/2095886#M237141</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;Using the prebuilt images from NXP, available here: &lt;A href="https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX" target="_blank" rel="noopener"&gt;https://www.nxp.com/design/design-center/software/embedded-software/i-mx-software/embedded-linux-for-i-mx-applications-processors:IMXLINUX&lt;/A&gt; I have attempted to program my IMX93EVK with these images including both the 6.12 kernel builds and the 6.6.52 for the IMX93EVK.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;All of my attempts, when it seems uuu can recognize the board, have ended with the following message:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;"'C:\Users\kleavell\Downloads\uuu(1).exe' .\uuu.auto uuu (Universal Update Utility) for nxp imx chips -- libuuu_1.5.182-0-gda3cd53 Success 0 Failure 1 1:91-2F0B37F 1/ 1 [HID(W): LIBUSB_ERROR_PIPE (-9) ] SDPS: boot -f imx-boot-imx93-1 PS C:\Users\kleavell\Desktop\reference\LF_v6.12.3-1.0.0_images_IMX93EVK&amp;gt;" &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I have done some poking around and it seems that uuu.exe recognizes the board as a IMX93 as it shows up when I issue a `uuu.exe -lsusb`. Any ideas on what could be going wrong?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;I have configured the board boot like so:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;dip switch 1301 has the pins at the following state when it seems like my board is recognized by uuu: 1234 respectively are 1100 based on the silk screen next to the switch.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="kleavell_1-1747101876623.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/337314i5FC61F23AAD184A2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="kleavell_1-1747101876623.jpeg" alt="kleavell_1-1747101876623.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;kleavell_1-1747101876623.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Any thoughts are appreciated!&lt;/P&gt;</description>
      <pubDate>Tue, 13 May 2025 02:07:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Preforming-Basic-Image-Programming-onto-an-IMX93EVK/m-p/2095886#M237141</guid>
      <dc:creator>kleavell</dc:creator>
      <dc:date>2025-05-13T02:07:39Z</dc:date>
    </item>
    <item>
      <title>Re: Preforming Basic Image Programming onto an IMX93EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Preforming-Basic-Image-Programming-onto-an-IMX93EVK/m-p/2096224#M237153</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/196183"&gt;@kleavell&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I have tested on my board it work well.&lt;/P&gt;
&lt;P&gt;LF_v6.12.3-1.0.0_images_IMX93EVK&amp;gt; .\uuu.exe .\uuu.auto&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Using this command.&lt;/P&gt;
&lt;P&gt;Your "&lt;SPAN&gt;[HID(W): LIBUSB_ERROR_PIPE (-9) ] SDPS: boot -f imx-boot-imx93-1 PS&lt;/SPAN&gt;" error caused by the usb connection, I think you can try to change another usb type-c line to try, and make sure boot mode pins: SW1301 &lt;STRONG&gt;1100&lt;/STRONG&gt; (from 1-4, low to high).&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Rita_Wang_0-1747121195352.jpeg" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/337480i96362D0BAF0E2155/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Rita_Wang_0-1747121195352.jpeg" alt="Rita_Wang_0-1747121195352.jpeg" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Rita_Wang_0-1747121195352.jpeg&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;You can try it, if still not work tell me freely&lt;/P&gt;
&lt;P&gt;Wish you have a nice day&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Rita&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 13 May 2025 07:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Preforming-Basic-Image-Programming-onto-an-IMX93EVK/m-p/2096224#M237153</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-05-13T07:26:44Z</dc:date>
    </item>
    <item>
      <title>Re: Preforming Basic Image Programming onto an IMX93EVK</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Preforming-Basic-Image-Programming-onto-an-IMX93EVK/m-p/2097437#M237210</link>
      <description>&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/57740"&gt;@Rita_Wang&lt;/a&gt;Thank you for taking the time to test and respond, your feedback helped me!&lt;/P&gt;&lt;P&gt;Turns out that I ended up with an older revision dye. In the forums they call it the A0. But it is etched into my IC as: &lt;SPAN&gt;PIMX9352CVUXMAA&lt;/SPAN&gt;. Chatted with a colleague of mine and he had no issues loading up the newest IMX-Linux release from NXP 6.12.3 using the A1 revision of the dye with the exact same process.&lt;/P&gt;&lt;P&gt;His EVK has an IC that reads &lt;SPAN&gt;PIMX9352CVVXMAB&lt;/SPAN&gt; which I assume is the A1.&lt;/P&gt;&lt;P&gt;Additional Clues that this may be the case: The EVK won't boot from the SD card either if you load it with a newer kernel version than 6.1&lt;/P&gt;&lt;P&gt;Which is actually what led me to this post: &lt;A href="https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1779127" target="_blank"&gt;https://community.nxp.com/t5/i-MX-Processors/imx93evk-cannot-boot-from-sd-card/m-p/1779127&lt;/A&gt; in-which the solution was found!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 14 May 2025 15:49:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Preforming-Basic-Image-Programming-onto-an-IMX93EVK/m-p/2097437#M237210</guid>
      <dc:creator>kleavell</dc:creator>
      <dc:date>2025-05-14T15:49:27Z</dc:date>
    </item>
  </channel>
</rss>