<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: why is touchscreen calibration taking forever?</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/why-is-touchscreen-calibration-taking-forever/m-p/156480#M2371</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eduardo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is an old thread, I have solved the problem minuets after I posted it here though, It was a hardware problem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 03 Sep 2011 15:11:35 GMT</pubDate>
    <dc:creator>danix</dc:creator>
    <dc:date>2011-09-03T15:11:35Z</dc:date>
    <item>
      <title>why is touchscreen calibration taking forever?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/why-is-touchscreen-calibration-taking-forever/m-p/156478#M2369</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my custom board I have a four wire resistive TS connected to the imx LRADC as in the EVK...&lt;/P&gt;&lt;P&gt;when I ran ts_calibrate it takes like 15 minuites to change the test points&lt;/P&gt;&lt;P&gt;does the ts caliberation has something to do with the panel selected, b/c it's fast when I'm using the default panel driver (LMS430),...all the problem show up after I edited the driver to my specific panel (320x240 3.5"....&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2011 17:28:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/why-is-touchscreen-calibration-taking-forever/m-p/156478#M2369</guid>
      <dc:creator>danix</dc:creator>
      <dc:date>2011-06-01T17:28:42Z</dc:date>
    </item>
    <item>
      <title>Re: why is touchscreen calibration taking forever?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/why-is-touchscreen-calibration-taking-forever/m-p/156479#M2370</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I'm using imx53 and i had had the same problem. It was fixed with an update manufactory drive.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Sep 2011 23:00:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/why-is-touchscreen-calibration-taking-forever/m-p/156479#M2370</guid>
      <dc:creator>G_rio</dc:creator>
      <dc:date>2011-09-02T23:00:54Z</dc:date>
    </item>
    <item>
      <title>Re: why is touchscreen calibration taking forever?</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/why-is-touchscreen-calibration-taking-forever/m-p/156480#M2371</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eduardo,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This is an old thread, I have solved the problem minuets after I posted it here though, It was a hardware problem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 03 Sep 2011 15:11:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/why-is-touchscreen-calibration-taking-forever/m-p/156480#M2371</guid>
      <dc:creator>danix</dc:creator>
      <dc:date>2011-09-03T15:11:35Z</dc:date>
    </item>
  </channel>
</rss>