<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Debugging M7-Core on i.MX95 using SEGGER J-Link in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-M7-Core-on-i-MX95-using-SEGGER-J-Link/m-p/2094593#M237086</link>
    <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am currently working on the i.MX95 EVK and exploring the appropriate platform and SDK to begin development—specifically targeting the M7 core. As per NXP’s recommendation, I am using the MCUXpresso SDK along with Visual Studio Code and the MCUXpresso extension for development.&lt;/P&gt;&lt;P&gt;According to the application note "Debugging Cortex-M with VS Code (AN14120)", the SEGGER J-Link is required for debugging. However, the application note provides the patch and example setup only for the i.MX8 series and i.MX93. While I understand that the debugging procedure for the i.MX95 is similar to that of the i.MX93, I am unable to find the specific SEGGER J-Link patch for the i.MX95 in the documentation or on NXP's official website.&lt;/P&gt;&lt;P&gt;Could you please help me with the appropriate steps, tools, or patch required to enable development and debugging on the M7 core of the i.MX95?&lt;/P&gt;&lt;P&gt;Your prompt response would be greatly appreciated and will be helpful in proceeding with development smoothly.&lt;/P&gt;</description>
    <pubDate>Fri, 09 May 2025 11:18:01 GMT</pubDate>
    <dc:creator>Abinandhan</dc:creator>
    <dc:date>2025-05-09T11:18:01Z</dc:date>
    <item>
      <title>Debugging M7-Core on i.MX95 using SEGGER J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-M7-Core-on-i-MX95-using-SEGGER-J-Link/m-p/2094593#M237086</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am currently working on the i.MX95 EVK and exploring the appropriate platform and SDK to begin development—specifically targeting the M7 core. As per NXP’s recommendation, I am using the MCUXpresso SDK along with Visual Studio Code and the MCUXpresso extension for development.&lt;/P&gt;&lt;P&gt;According to the application note "Debugging Cortex-M with VS Code (AN14120)", the SEGGER J-Link is required for debugging. However, the application note provides the patch and example setup only for the i.MX8 series and i.MX93. While I understand that the debugging procedure for the i.MX95 is similar to that of the i.MX93, I am unable to find the specific SEGGER J-Link patch for the i.MX95 in the documentation or on NXP's official website.&lt;/P&gt;&lt;P&gt;Could you please help me with the appropriate steps, tools, or patch required to enable development and debugging on the M7 core of the i.MX95?&lt;/P&gt;&lt;P&gt;Your prompt response would be greatly appreciated and will be helpful in proceeding with development smoothly.&lt;/P&gt;</description>
      <pubDate>Fri, 09 May 2025 11:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-M7-Core-on-i-MX95-using-SEGGER-J-Link/m-p/2094593#M237086</guid>
      <dc:creator>Abinandhan</dc:creator>
      <dc:date>2025-05-09T11:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging M7-Core on i.MX95 using SEGGER J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-M7-Core-on-i-MX95-using-SEGGER-J-Link/m-p/2094698#M237099</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/249590"&gt;@Abinandhan&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Unfortunately, as the i.MX95 is still in Pre-Production, we have not much information about it.&lt;/P&gt;
&lt;P&gt;There is not an Application note or patch prepared fo the i.MX95, so, we need to wait the release to get more information, steps to debug and patches.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Fri, 09 May 2025 14:42:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-M7-Core-on-i-MX95-using-SEGGER-J-Link/m-p/2094698#M237099</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-05-09T14:42:44Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging M7-Core on i.MX95 using SEGGER J-Link</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Debugging-M7-Core-on-i-MX95-using-SEGGER-J-Link/m-p/2367764#M245282</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/203368"&gt;@Manuel_Salas&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am planning to buy FRDM i.MX95, can i ask that does this board support JTAG, and if yes, does the software fully support yet ?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 19 May 2026 15:44:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Debugging-M7-Core-on-i-MX95-using-SEGGER-J-Link/m-p/2367764#M245282</guid>
      <dc:creator>Zk47T</dc:creator>
      <dc:date>2026-05-19T15:44:53Z</dc:date>
    </item>
  </channel>
</rss>