<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: FRDM-MX91 CPU lifecycle OEM_OPEN</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2094493#M237083</link>
    <description>&lt;P&gt;Authentication is not required, but release RDC is required, as only ele has permission at the beginning.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regarding blank EVK, I've checked with the internal team that only OEM OPEN LC chips are provided.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
    <pubDate>Fri, 09 May 2025 09:10:04 GMT</pubDate>
    <dc:creator>Harvey021</dc:creator>
    <dc:date>2025-05-09T09:10:04Z</dc:date>
    <item>
      <title>FRDM-MX91 CPU lifecycle OEM_OPEN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2091196#M236917</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I recently got a FRDM-MX91 board to do some bare-metal experiment with the A55, just to discover that the CPU lifecycle is OEM_OPEN ("OO" in USB descriptor string), thus preventing unauthenticated debugging. This means, for example, that TRDC registers cannot be accessed and debugging hangs quite often.&lt;/P&gt;&lt;P&gt;Is there any specific reason why the CPU lifecycle on this development board (and I suppose also on FRDM-MX93) is not TEST/DEVELOPMENT (i.e., "BA" in USB descriptor string)?&lt;/P&gt;&lt;P&gt;To my knowledge, the only solution to this issue is to replace the CPU with a brand new one - or do I have other options?&lt;/P&gt;&lt;P&gt;Thank you in advance and best regards,&lt;BR /&gt;Stefano&lt;/P&gt;</description>
      <pubDate>Sun, 04 May 2025 23:28:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2091196#M236917</guid>
      <dc:creator>TheUncle</dc:creator>
      <dc:date>2025-05-04T23:28:12Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MX91 CPU lifecycle OEM_OPEN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2091332#M236929</link>
      <description>&lt;P&gt;Just wondering if on the standard EVKs the chips are shipped as blank.&lt;/P&gt;&lt;P&gt;Thanks,&lt;BR /&gt;Stefano&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 09:44:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2091332#M236929</guid>
      <dc:creator>TheUncle</dc:creator>
      <dc:date>2025-05-05T09:44:09Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MX91 CPU lifecycle OEM_OPEN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2092015#M236961</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Before the LC for chip move forward to OEM_CLOSE from OEM_OPEN, it can be considered as&amp;nbsp;&lt;SPAN&gt;TEST/DEVELOPMENT.&amp;nbsp;If I don't misunderstand.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regards&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Harvey&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 06 May 2025 08:34:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2092015#M236961</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-05-06T08:34:41Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MX91 CPU lifecycle OEM_OPEN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2092102#M236965</link>
      <description>&lt;P&gt;Seems not. In TEST/DEVELOPMENT debugging does not require authentication and all registers should be accessible (including TRDC), while in OEM_OPEN they are locked.&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Stefano&lt;/P&gt;</description>
      <pubDate>Tue, 06 May 2025 10:21:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2092102#M236965</guid>
      <dc:creator>TheUncle</dc:creator>
      <dc:date>2025-05-06T10:21:29Z</dc:date>
    </item>
    <item>
      <title>Re: FRDM-MX91 CPU lifecycle OEM_OPEN</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2094493#M237083</link>
      <description>&lt;P&gt;Authentication is not required, but release RDC is required, as only ele has permission at the beginning.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Regarding blank EVK, I've checked with the internal team that only OEM OPEN LC chips are provided.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Harvey&lt;/P&gt;</description>
      <pubDate>Fri, 09 May 2025 09:10:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/FRDM-MX91-CPU-lifecycle-OEM-OPEN/m-p/2094493#M237083</guid>
      <dc:creator>Harvey021</dc:creator>
      <dc:date>2025-05-09T09:10:04Z</dc:date>
    </item>
  </channel>
</rss>