<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: RT1024 WATCHDOG TIMER 1 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/RT1024-WATCHDOG-TIMER-1/m-p/2092043#M236962</link>
    <description>&lt;P&gt;Unfortunately, our project is too advanced for us to afford to change IDEs or SDKs.&lt;BR /&gt;We use the MCU-LINK debugger.&lt;BR /&gt;We only observe the problem with the watchdog active and only with watchdogs 1 and 2.&lt;BR /&gt;We don't have the problem if we use the RT watchdog (watchdog 3).&lt;/P&gt;</description>
    <pubDate>Tue, 06 May 2025 09:12:14 GMT</pubDate>
    <dc:creator>Gaetan</dc:creator>
    <dc:date>2025-05-06T09:12:14Z</dc:date>
    <item>
      <title>RT1024 WATCHDOG TIMER 1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1024-WATCHDOG-TIMER-1/m-p/2088548#M236771</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We have installed watchdog timer 1 in our application.&lt;BR /&gt;It works correctly, but debugging has some issues.&lt;BR /&gt;The breakpoints work fine, but the single-step mode is giving an error.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Gaetan_0-1745855857233.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335289i501C9A3A33019159/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Gaetan_0-1745855857233.png" alt="Gaetan_0-1745855857233.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;our watchdog configuration :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Gaetan_1-1745855894280.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/335290iA68F9F93DA9DCCC9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Gaetan_1-1745855894280.png" alt="Gaetan_1-1745855894280.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;SDK 2.15&lt;BR /&gt;MCUXpresso 11.9.1&lt;/P&gt;</description>
      <pubDate>Mon, 28 Apr 2025 15:58:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1024-WATCHDOG-TIMER-1/m-p/2088548#M236771</guid>
      <dc:creator>Gaetan</dc:creator>
      <dc:date>2025-04-28T15:58:40Z</dc:date>
    </item>
    <item>
      <title>Re: RT1024 WATCHDOG TIMER 1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1024-WATCHDOG-TIMER-1/m-p/2089598#M236828</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/246648"&gt;@Gaetan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Do you see issues with single step only when watchdog is enabled? Or also when it is disabled? What debugger are you using (MCU-Link, J-Link, etc.)? Are you certain this debugger is updated to the latest firmware version? Please try updating your debugger to the latest version.&lt;/P&gt;
&lt;P&gt;BTW, speaking of latest firmware versions, note that SDK 2.15 is over a year old now and might have bugs or issues. I highly recommend you update to the latest SDK version (25.03.00). In order to use this SDK, you will also require the latest IDE version (v&lt;SPAN&gt;24.12.148&lt;/SPAN&gt;).&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 18:23:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1024-WATCHDOG-TIMER-1/m-p/2089598#M236828</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-04-29T18:23:50Z</dc:date>
    </item>
    <item>
      <title>Re: RT1024 WATCHDOG TIMER 1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1024-WATCHDOG-TIMER-1/m-p/2092043#M236962</link>
      <description>&lt;P&gt;Unfortunately, our project is too advanced for us to afford to change IDEs or SDKs.&lt;BR /&gt;We use the MCU-LINK debugger.&lt;BR /&gt;We only observe the problem with the watchdog active and only with watchdogs 1 and 2.&lt;BR /&gt;We don't have the problem if we use the RT watchdog (watchdog 3).&lt;/P&gt;</description>
      <pubDate>Tue, 06 May 2025 09:12:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1024-WATCHDOG-TIMER-1/m-p/2092043#M236962</guid>
      <dc:creator>Gaetan</dc:creator>
      <dc:date>2025-05-06T09:12:14Z</dc:date>
    </item>
    <item>
      <title>Re: RT1024 WATCHDOG TIMER 1</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/RT1024-WATCHDOG-TIMER-1/m-p/2095745#M237138</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/246648"&gt;@Gaetan&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I understand that you are not able to upgrade SDK on this specific project. In this case, I would recommend you stick to the WDT that does not show this error (WDT3 in this case).&lt;/P&gt;
&lt;P&gt;BR,&lt;BR /&gt;Edwin.&lt;/P&gt;</description>
      <pubDate>Mon, 12 May 2025 20:58:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/RT1024-WATCHDOG-TIMER-1/m-p/2095745#M237138</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-05-12T20:58:36Z</dc:date>
    </item>
  </channel>
</rss>