<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX ProcessorsのトピックRe: Launch bare metal sample</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Launch-bare-metal-sample/m-p/2091648#M236945</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;You could use the time command for measuring the time executing the command of loading and running the demo, you will use this command:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;# Use the command from 3.3.2.3.1.2 RTEDGEUG
setenv load_baremetal "ext4load mmc 1:2 0xC0000000 /examples/heterogeneous-multicore/hello-world-ca/ddr_release/hello_world_ca53_RTOS0_RAM_CONSOLE-0xc0fff000.bin; dcache flush; icache flush; cpu 2 release 0xC0000000"
# Measure the time that takes to run the script
time run load_baremetal&lt;/LI-CODE&gt;
&lt;P&gt;Then, you can add the script to &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Custom-Scripts-in-U-Boot/ta-p/1792382" target="_self"&gt;bootscript&lt;/A&gt; for its automatic execution upon boot.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
    <pubDate>Mon, 05 May 2025 18:30:50 GMT</pubDate>
    <dc:creator>JosephAtNXP</dc:creator>
    <dc:date>2025-05-05T18:30:50Z</dc:date>
    <item>
      <title>Launch bare metal sample</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Launch-bare-metal-sample/m-p/2091324#M236927</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I use a Imx 93 evk board&lt;BR /&gt;I am tring to measure the launch time of a bare metal yocto application&lt;/P&gt;&lt;P&gt;i launch&lt;BR /&gt;MACHINE=imx91-11x11-lpddr4-evk DISTRO=nxp-real-time-edge source ./real-time-edge-setup-env.sh -b build&lt;BR /&gt;bitbake nxp-image-real-time-edge&lt;/P&gt;&lt;P&gt;in the image there are samples&lt;BR /&gt;/root/examples/heterogeneous-multicore/&lt;/P&gt;&lt;P&gt;i would like to launch a sample which emit an Ethernet trame like : hello-world-ca&lt;BR /&gt;/root/examples/heterogeneous-multicore/hello-world-ca/ddr_release&lt;/P&gt;&lt;P&gt;I would like to launch wireshark on the host PC and measure approximatively the time beetween the power on and the first trame on wireshark&lt;/P&gt;&lt;P&gt;Is there a way to flash an SD card with this example so that it boots immediately ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Greeting&amp;nbsp;&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 09:28:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Launch-bare-metal-sample/m-p/2091324#M236927</guid>
      <dc:creator>OlivierG</dc:creator>
      <dc:date>2025-05-05T09:28:39Z</dc:date>
    </item>
    <item>
      <title>Re: Launch bare metal sample</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Launch-bare-metal-sample/m-p/2091648#M236945</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;You could use the time command for measuring the time executing the command of loading and running the demo, you will use this command:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;# Use the command from 3.3.2.3.1.2 RTEDGEUG
setenv load_baremetal "ext4load mmc 1:2 0xC0000000 /examples/heterogeneous-multicore/hello-world-ca/ddr_release/hello_world_ca53_RTOS0_RAM_CONSOLE-0xc0fff000.bin; dcache flush; icache flush; cpu 2 release 0xC0000000"
# Measure the time that takes to run the script
time run load_baremetal&lt;/LI-CODE&gt;
&lt;P&gt;Then, you can add the script to &lt;A href="https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Custom-Scripts-in-U-Boot/ta-p/1792382" target="_self"&gt;bootscript&lt;/A&gt; for its automatic execution upon boot.&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Mon, 05 May 2025 18:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Launch-bare-metal-sample/m-p/2091648#M236945</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-05-05T18:30:50Z</dc:date>
    </item>
  </channel>
</rss>