<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Harpoon without Linux in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Harpoon-without-Linux/m-p/2091135#M236916</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When I look at the pictures about Harpoon it seems that Both Linux and other RTOS modules are running on top of Jailhouse Hypervisor. It also says:&lt;/P&gt;&lt;P&gt;"Enables a choice of RTOS’s to run within Jailhouse hypervisor environment on the Arm® Cortex®-A cores of NXP MPU’s."&lt;/P&gt;&lt;P&gt;So this implies Harpoon can be used without Linux. Is that correct?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Sat, 03 May 2025 23:42:22 GMT</pubDate>
    <dc:creator>simmania</dc:creator>
    <dc:date>2025-05-03T23:42:22Z</dc:date>
    <item>
      <title>Harpoon without Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Harpoon-without-Linux/m-p/2091135#M236916</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;When I look at the pictures about Harpoon it seems that Both Linux and other RTOS modules are running on top of Jailhouse Hypervisor. It also says:&lt;/P&gt;&lt;P&gt;"Enables a choice of RTOS’s to run within Jailhouse hypervisor environment on the Arm® Cortex®-A cores of NXP MPU’s."&lt;/P&gt;&lt;P&gt;So this implies Harpoon can be used without Linux. Is that correct?&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Sat, 03 May 2025 23:42:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Harpoon-without-Linux/m-p/2091135#M236916</guid>
      <dc:creator>simmania</dc:creator>
      <dc:date>2025-05-03T23:42:22Z</dc:date>
    </item>
    <item>
      <title>Re: Harpoon without Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Harpoon-without-Linux/m-p/2092510#M236986</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Simmania:&lt;/P&gt;
&lt;P&gt;From the Harpoon User's Guide: Linux is needed&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielchen_0-1746582449571.png" style="width: 754px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/336438iCCD29E4F8989147F/image-dimensions/754x66?v=v2" width="754" height="66" role="button" title="danielchen_0-1746582449571.png" alt="danielchen_0-1746582449571.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;
&lt;P&gt;Daniel&lt;/P&gt;</description>
      <pubDate>Wed, 07 May 2025 01:48:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Harpoon-without-Linux/m-p/2092510#M236986</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2025-05-07T01:48:00Z</dc:date>
    </item>
    <item>
      <title>Re: Harpoon without Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Harpoon-without-Linux/m-p/2092714#M236994</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN class=""&gt;This text does not say that Linux is required.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;It says that both Linux and an RTOS can run in parallel on the Harpoon environment.&lt;/SPAN&gt;&lt;/SPAN&gt; &lt;SPAN class=""&gt;&lt;SPAN class=""&gt;That does not mean that Linux is mandatory.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 May 2025 07:20:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Harpoon-without-Linux/m-p/2092714#M236994</guid>
      <dc:creator>simmania</dc:creator>
      <dc:date>2025-05-07T07:20:45Z</dc:date>
    </item>
    <item>
      <title>Re: Harpoon without Linux</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Harpoon-without-Linux/m-p/2100174#M237361</link>
      <description>&lt;P&gt;Thanks, but the doc says the system starts on Linux and the Jailhouse hypervisor partitions the hardware to run both Linux and the guest RTOS in parallel.&lt;/P&gt;
&lt;DIV id="tinyMceEditordanielchen_0" class="mceNonEditable lia-copypaste-placeholder"&gt;&amp;nbsp;&lt;/DIV&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="danielchen_1-1747703720860.png" style="width: 679px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/338572i589B806AE4DA9E1D/image-dimensions/679x258?v=v2" width="679" height="258" role="button" title="danielchen_1-1747703720860.png" alt="danielchen_1-1747703720860.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 May 2025 01:17:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Harpoon-without-Linux/m-p/2100174#M237361</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2025-05-20T01:17:20Z</dc:date>
    </item>
  </channel>
</rss>