<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GPIO config register in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-config-register/m-p/2090997#M236906</link>
    <description>&lt;P&gt;I am using the iMX8 Quad Max, and I have seen examples of gpio settings where those bits are not used, but the bits they alledgedly control are modified. The information supplied is not a solution, the documentation does not appear to say if/when it needs to be used.&lt;/P&gt;&lt;P&gt;Could someone please explain if/when the update_mux_mode and udate_pad_ctrl need to be used?&lt;/P&gt;</description>
    <pubDate>Fri, 02 May 2025 16:09:03 GMT</pubDate>
    <dc:creator>flobro</dc:creator>
    <dc:date>2025-05-02T16:09:03Z</dc:date>
    <item>
      <title>GPIO config register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-config-register/m-p/913819#M137591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello，&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could u help detail explain about GPIO config below：&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;update_mux_mode&lt;BR /&gt;update lock for mux control&lt;BR /&gt;write 1 to allow programming to mux control [29:19]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;update_pad_ctl&lt;BR /&gt;update lock for pad control&lt;BR /&gt;write 1 to allow programming to pad control [14-1:0]&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Just for little words I can not understand it more,when set the register 1 and when set 0?&lt;/P&gt;&lt;P&gt;pls help it&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2019 03:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIO-config-register/m-p/913819#M137591</guid>
      <dc:creator>xu_ji1</dc:creator>
      <dc:date>2019-05-29T03:01:40Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO config register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-config-register/m-p/913820#M137592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Xu&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can check sect.2.1.5.6 IOMUX Control Through GPIO Module attached Linux Manual and&lt;/P&gt;&lt;P&gt;sect.Chapter 8 Configuring IOMUX Porting Guide from nxp software documentation link below&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW"&gt;https://www.nxp.com/support/developer-resources/run-time-software/i.mx-developer-resources/i.mx-6series-i.mx-7series-software-and-development-tool-resources:IMX_SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;For i.MX8 series use SCFW documentation in &lt;A class="" href="https://www.nxp.com/webapp/sps/download/license.jsp?colCode=L4.14.98_2.0.0_SCFWKIT-1.2" target="_blank"&gt;SCFW Porting Kit&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2019 05:04:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIO-config-register/m-p/913820#M137592</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-05-29T05:04:24Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO config register</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/GPIO-config-register/m-p/2090997#M236906</link>
      <description>&lt;P&gt;I am using the iMX8 Quad Max, and I have seen examples of gpio settings where those bits are not used, but the bits they alledgedly control are modified. The information supplied is not a solution, the documentation does not appear to say if/when it needs to be used.&lt;/P&gt;&lt;P&gt;Could someone please explain if/when the update_mux_mode and udate_pad_ctrl need to be used?&lt;/P&gt;</description>
      <pubDate>Fri, 02 May 2025 16:09:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/GPIO-config-register/m-p/2090997#M236906</guid>
      <dc:creator>flobro</dc:creator>
      <dc:date>2025-05-02T16:09:03Z</dc:date>
    </item>
  </channel>
</rss>