<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Exception with uuu in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Exception-with-uuu/m-p/2089891#M236837</link>
    <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;The result is&lt;/P&gt;&lt;P&gt;c.zst&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;Error: can't find ext name in path: &amp;gt;imx-boot-imx93evk-sd.bin-flash_singleboot&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;the closest file is : u-boot-spl.bin-sd-2024.04-r0&lt;/P&gt;&lt;P&gt;when i prompt&lt;BR /&gt;sudo uuu -b emmc_all u-boot-spl.bin-sd-2024.04-r0 core-image-minimal-imx93-11x11-lpddr4x-evk.rootfs-20250425121719.wic.zst&lt;/P&gt;&lt;P&gt;The result is&lt;/P&gt;&lt;P&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;BR /&gt;Success 0 Failure 1&lt;BR /&gt;1:2 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -scanterm -f u-boot-spl.bin-sd-2024.04-r0 -scanlimited 0x800000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does a device need to be present in /dev ?&lt;/P&gt;&lt;P&gt;Greeting&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;</description>
    <pubDate>Wed, 30 Apr 2025 06:35:18 GMT</pubDate>
    <dc:creator>OlivierG</dc:creator>
    <dc:date>2025-04-30T06:35:18Z</dc:date>
    <item>
      <title>Exception with uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Exception-with-uuu/m-p/2089301#M236818</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I'm using a imx93 evk board&lt;BR /&gt;i'm tring to flash an image to the emmc memory&lt;/P&gt;&lt;P&gt;i set the switch SW1301 to the right positions : Serial downloader (USB)&lt;/P&gt;&lt;P&gt;i rely the card USB C DRP2 (J401) the the Ubuntu PC&lt;/P&gt;&lt;P&gt;i built an image using&lt;BR /&gt;MACHINE=imx93-11x11-lpddr4x-evk&lt;BR /&gt;DISTRO=fsl-imx-xwayland&lt;BR /&gt;bitbake core-image-minimal&lt;/P&gt;&lt;P&gt;i got "uuu" using :&lt;BR /&gt;sudo apt install uuu&lt;/P&gt;&lt;P&gt;When i run&lt;/P&gt;&lt;P&gt;uuu core-image-minimal-imx93-11x11-lpddr4x-evk.rootfs-20250425121719.wic.zst&lt;/P&gt;&lt;P&gt;i got an exception :&lt;/P&gt;&lt;P&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;/P&gt;&lt;P&gt;Success 0 Failure 0 Wait for Known USB Device Appear...&lt;BR /&gt;&lt;BR /&gt;Prep 1/ 0 [387M ] Http Download\Uncompress&lt;BR /&gt;terminate called after throwing an instance of 'std::invalid_argument'&lt;BR /&gt;what(): stoll&lt;BR /&gt;Aborted (core dumped)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Where am i wrong ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Greetings&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 10:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Exception-with-uuu/m-p/2089301#M236818</guid>
      <dc:creator>OlivierG</dc:creator>
      <dc:date>2025-04-29T10:58:52Z</dc:date>
    </item>
    <item>
      <title>Re: Exception with uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Exception-with-uuu/m-p/2089579#M236827</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/245939"&gt;@OlivierG&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope you are doing very well.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please try with:&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;$ sudo uuu -b emmc_all imx-boot-imx93evk-sd.bin-flash_singleboot core-image-minimal-imx93-11x11-lpddr4x-evk.rootfs-20250425121719.wic.zst&lt;/LI-CODE&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 17:57:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Exception-with-uuu/m-p/2089579#M236827</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-04-29T17:57:23Z</dc:date>
    </item>
    <item>
      <title>Re: Exception with uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Exception-with-uuu/m-p/2089891#M236837</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;The result is&lt;/P&gt;&lt;P&gt;c.zst&lt;BR /&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;BR /&gt;Wait for Known USB Device Appear...&lt;BR /&gt;Error: can't find ext name in path: &amp;gt;imx-boot-imx93evk-sd.bin-flash_singleboot&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;the closest file is : u-boot-spl.bin-sd-2024.04-r0&lt;/P&gt;&lt;P&gt;when i prompt&lt;BR /&gt;sudo uuu -b emmc_all u-boot-spl.bin-sd-2024.04-r0 core-image-minimal-imx93-11x11-lpddr4x-evk.rootfs-20250425121719.wic.zst&lt;/P&gt;&lt;P&gt;The result is&lt;/P&gt;&lt;P&gt;uuu (Universal Update Utility) for nxp imx chips -- lib1.5.141&lt;BR /&gt;Success 0 Failure 1&lt;BR /&gt;1:2 1/ 1 [HID(W):LIBUSB_ERROR_NO_DEVICE ] SDPS: boot -scanterm -f u-boot-spl.bin-sd-2024.04-r0 -scanlimited 0x800000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does a device need to be present in /dev ?&lt;/P&gt;&lt;P&gt;Greeting&lt;/P&gt;&lt;P&gt;Olivier&lt;/P&gt;</description>
      <pubDate>Wed, 30 Apr 2025 06:35:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Exception-with-uuu/m-p/2089891#M236837</guid>
      <dc:creator>OlivierG</dc:creator>
      <dc:date>2025-04-30T06:35:18Z</dc:date>
    </item>
    <item>
      <title>Re: Exception with uuu</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Exception-with-uuu/m-p/2090326#M236848</link>
      <description>&lt;P&gt;Please share the file names under your tmp/deploy/images/&amp;lt;your_board&amp;gt;/.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Also, what Chip revision in EVK are you using?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Salas.&lt;/P&gt;</description>
      <pubDate>Wed, 30 Apr 2025 15:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Exception-with-uuu/m-p/2090326#M236848</guid>
      <dc:creator>Manuel_Salas</dc:creator>
      <dc:date>2025-04-30T15:55:40Z</dc:date>
    </item>
  </channel>
</rss>