<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: HSM Code Signing Tool for Debian 12 in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/HSM-Code-Signing-Tool-for-Debian-12/m-p/2089398#M236821</link>
    <description>&lt;P&gt;Now there are several backends in one binary.&lt;BR /&gt;For the HSM backend we have to call cst&amp;nbsp;-b pkcs11 ...&lt;/P&gt;&lt;P&gt;linux64/bin/cst works well with Debian 12 if we do a&lt;BR /&gt;export PKCS11_MODULE_PATH=/usr/lib/x86_64-linux-gnu/p11-kit-proxy.so&lt;BR /&gt;before.&lt;/P&gt;&lt;P&gt;Kind regards&lt;BR /&gt;Frank&lt;/P&gt;</description>
    <pubDate>Tue, 29 Apr 2025 13:29:45 GMT</pubDate>
    <dc:creator>fsylla</dc:creator>
    <dc:date>2025-04-29T13:29:45Z</dc:date>
    <item>
      <title>HSM Code Signing Tool for Debian 12</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HSM-Code-Signing-Tool-for-Debian-12/m-p/2089072#M236796</link>
      <description>&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;we are currently using the HSM code signing tool built from&amp;nbsp;code/back_end-hsm in the cst-3.3.1 source tree on a Debian 11 host.&lt;BR /&gt;We need to update to Debian 12 but the cst version 3.3.1 doesn't work any longer due to compatibility issues with&amp;nbsp;OpenSSL 3.0.15.&lt;BR /&gt;Is it possible to get a more recent version of&amp;nbsp;back_end-hsm that works with Debian 12?&lt;/P&gt;&lt;P&gt;I downloaded&amp;nbsp;IMX_CST_TOOL_NEW.tgz that seems to be version 4.0.0 but it doesn't contain the back_end_hsm folder any longer.&lt;/P&gt;&lt;P&gt;Kind regards&lt;BR /&gt;Frank Sylla&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 07:33:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HSM-Code-Signing-Tool-for-Debian-12/m-p/2089072#M236796</guid>
      <dc:creator>fsylla</dc:creator>
      <dc:date>2025-04-29T07:33:21Z</dc:date>
    </item>
    <item>
      <title>Re: HSM Code Signing Tool for Debian 12</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/HSM-Code-Signing-Tool-for-Debian-12/m-p/2089398#M236821</link>
      <description>&lt;P&gt;Now there are several backends in one binary.&lt;BR /&gt;For the HSM backend we have to call cst&amp;nbsp;-b pkcs11 ...&lt;/P&gt;&lt;P&gt;linux64/bin/cst works well with Debian 12 if we do a&lt;BR /&gt;export PKCS11_MODULE_PATH=/usr/lib/x86_64-linux-gnu/p11-kit-proxy.so&lt;BR /&gt;before.&lt;/P&gt;&lt;P&gt;Kind regards&lt;BR /&gt;Frank&lt;/P&gt;</description>
      <pubDate>Tue, 29 Apr 2025 13:29:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/HSM-Code-Signing-Tool-for-Debian-12/m-p/2089398#M236821</guid>
      <dc:creator>fsylla</dc:creator>
      <dc:date>2025-04-29T13:29:45Z</dc:date>
    </item>
  </channel>
</rss>