<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx config tool ddr tool in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/imx-config-tool-ddr-tool/m-p/2085625#M236626</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;If you are using a custom configuration, please check the next:&lt;/P&gt;
&lt;P&gt;- If you use a different debug UART port as NXP EVK does, you must configure debug UART IOMUX and debug port in the beginning of the DDR script according to your schematics.&lt;/P&gt;
&lt;P&gt;- If you are not using a PMIC in your design, you need to skip the PMIC initialization, but you need to verify that the board is following the power up sequence of i.MX95.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Wed, 23 Apr 2025 17:07:38 GMT</pubDate>
    <dc:creator>JorgeCas</dc:creator>
    <dc:date>2025-04-23T17:07:38Z</dc:date>
    <item>
      <title>imx config tool ddr tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-config-tool-ddr-tool/m-p/2084747#M236577</link>
      <description>&lt;DIV class=""&gt;&lt;P&gt;Hello, I get stuck at reset target. I’m not using PMIC, is this issue due to PMIC? I selected inside config tool DDR config → Board Configuration → PMIC initialization disabled&lt;/P&gt;&lt;P&gt;#################### Result for: phy_init ###### Run 1 ############################################&lt;SPAN class=""&gt;#Microsoft&lt;/SPAN&gt; Windows [Version 10.0.22631.5189]&lt;BR /&gt;(c) Microsoft Corporation. All rights reserved.&lt;/P&gt;&lt;P&gt;C:\nxp\i.MX_CFG_25.03\bin&amp;gt;prompt test-prefix :&lt;/P&gt;&lt;P&gt;test-prefix : “C:/nxp/i.MX_CFG_25.03/bin/python3/python” “C:/nxp/i.MX_CFG_25.03/bin/python3/memtool/memtool_entry.py” -t “runtest” -d “C:/ProgramData/NXP/mcu_data_25.03/processors/MIMX9596xxxxQ/ksdk2_0/mem_validation/ddrc” -p “C:/Users//AppData/Local/Temp/mem_validation/phy_training_phy_test_0_0_.log” -l INFO “C:/Users//AppData/Local/Temp/mem_validation/connect.json” “C:/Users//AppData/Local/Temp/mem_validation/test.json” “C:/Users//AppData/Local/Temp/mem_validation/phy.json” “C:/Users//AppData/Local/Temp/mem_validation/ddrc_registers.json” “C:/Users//AppData/Local/Temp/mem_validation/ddrc_config.json” “C:/Users/163055~1/AppData/Local/Temp/mem_validation/ddrc_config_in.json”&lt;BR /&gt;INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/connect.json&lt;BR /&gt;INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/test.json&lt;BR /&gt;INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/phy.json&lt;BR /&gt;INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/ddrc_registers.json&lt;BR /&gt;INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/ddrc_config.json&lt;BR /&gt;INFO memtool.utils.helper *****C:/Users//AppData/Local/Temp/mem_validation/ddrc_config_in.json&lt;BR /&gt;INFO memtool.processor.imx9.imx9_processor Xls mapping load time 0.052813&lt;BR /&gt;INFO memtool.processor.imx9.imx9_processor Config time 0.000317&lt;BR /&gt;INFO memtool.processor.imx9.imx9_processor DS file time 0.359792&lt;BR /&gt;INFO memtool.phyinit.phy_init Run phyinit for 2024.09\lpddr5&lt;BR /&gt;INFO memtool.comm.serial_channel Using serial: COM3&lt;BR /&gt;INFO memtool.comm.serial_channel Send reset to target&lt;/P&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 22 Apr 2025 14:39:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-config-tool-ddr-tool/m-p/2084747#M236577</guid>
      <dc:creator>stoemarc</dc:creator>
      <dc:date>2025-04-22T14:39:22Z</dc:date>
    </item>
    <item>
      <title>Re: imx config tool ddr tool</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/imx-config-tool-ddr-tool/m-p/2085625#M236626</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;If you are using a custom configuration, please check the next:&lt;/P&gt;
&lt;P&gt;- If you use a different debug UART port as NXP EVK does, you must configure debug UART IOMUX and debug port in the beginning of the DDR script according to your schematics.&lt;/P&gt;
&lt;P&gt;- If you are not using a PMIC in your design, you need to skip the PMIC initialization, but you need to verify that the board is following the power up sequence of i.MX95.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Wed, 23 Apr 2025 17:07:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/imx-config-tool-ddr-tool/m-p/2085625#M236626</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2025-04-23T17:07:38Z</dc:date>
    </item>
  </channel>
</rss>