<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>i.MX Processors中的主题 Re: Changing kernel start address</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/Changing-kernel-start-address/m-p/2081992#M236412</link>
    <description>&lt;P&gt;If the modifications detailed in the application note are not implemented the kernel boots and functions normally.&lt;/P&gt;</description>
    <pubDate>Wed, 16 Apr 2025 21:11:01 GMT</pubDate>
    <dc:creator>dogisfat</dc:creator>
    <dc:date>2025-04-16T21:11:01Z</dc:date>
    <item>
      <title>Changing kernel start address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Changing-kernel-start-address/m-p/2081083#M236353</link>
      <description>&lt;P&gt;I have implemented the change detailed in Application note AN5127 (&lt;A href="https://www.nxp.com/docs/en/application-note/AN5127.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN5127.pdf&lt;/A&gt;) successfully for a i.MX7D platform with kernel 4.9. I am trying to update to a Yocto Kirkstone based BSP with kernel 5.10 and am failing to successfully boot when making the same modifications. The system gets stuck after printing "Staring Kernel ..."&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;What changes should I be aware of that will require additional changes to the kernel to get the modifications working for Kernel 5.10?&lt;/P&gt;</description>
      <pubDate>Tue, 15 Apr 2025 19:58:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Changing-kernel-start-address/m-p/2081083#M236353</guid>
      <dc:creator>dogisfat</dc:creator>
      <dc:date>2025-04-15T19:58:08Z</dc:date>
    </item>
    <item>
      <title>Re: Changing kernel start address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Changing-kernel-start-address/m-p/2081981#M236411</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you for your interest in NXP Semiconductor products,&lt;/P&gt;
&lt;P&gt;If it fails when specifying the kernel address, what happen if you don't and flash a fresh build?&lt;/P&gt;
&lt;P&gt;Regards&lt;/P&gt;</description>
      <pubDate>Wed, 16 Apr 2025 20:40:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Changing-kernel-start-address/m-p/2081981#M236411</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2025-04-16T20:40:22Z</dc:date>
    </item>
    <item>
      <title>Re: Changing kernel start address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Changing-kernel-start-address/m-p/2081992#M236412</link>
      <description>&lt;P&gt;If the modifications detailed in the application note are not implemented the kernel boots and functions normally.&lt;/P&gt;</description>
      <pubDate>Wed, 16 Apr 2025 21:11:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Changing-kernel-start-address/m-p/2081992#M236412</guid>
      <dc:creator>dogisfat</dc:creator>
      <dc:date>2025-04-16T21:11:01Z</dc:date>
    </item>
    <item>
      <title>Re: Changing kernel start address</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/Changing-kernel-start-address/m-p/2086908#M236693</link>
      <description>&lt;P&gt;I have narrowed the failure to boot to be in the __turn_mmu_on function in arch/arm/kernel/head.S. Unfortunately the comment for __turn_mmu_on specifies that you cannot trace through this function which I assume applies to jtag debuggers. I also have been unable to print to the UART though it (unsurprisingly).&lt;BR /&gt;&lt;BR /&gt;What do I need to verify prior to that call to ensure the platform is correctly set up?&lt;/P&gt;</description>
      <pubDate>Thu, 24 Apr 2025 21:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/Changing-kernel-start-address/m-p/2086908#M236693</guid>
      <dc:creator>dogisfat</dc:creator>
      <dc:date>2025-04-24T21:51:32Z</dc:date>
    </item>
  </channel>
</rss>