<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IMX6 booting Random failure in i.MX Processors</title>
    <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-Random-failure/m-p/2081497#M236378</link>
    <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have a custom board based on iMX6 quad core processor. It is designed to boot from eMMC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Processor:&amp;nbsp;&lt;/SPAN&gt; IMX6 Quad， MCIMX6Q6AVT10AD&lt;/P&gt;&lt;P&gt;eMMC ：&lt;SPAN&gt; IS21ES08G-JCLI&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PMIC：MMPF0100F0AEP（Unconnected button battery）&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN&gt;Problem :&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We see majority of boards boots as designed.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;But there are random failures on one or two boards per hundred( 1 to 2% only).&lt;/SPAN&gt;When the startup fails, both SD3_CMD and SD3_CK remain high without any communication waveform.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Power supply design reference SCH-27516, VDDHIGH_IN is provided through PMIC GEN5, and VDD_SNVS_IN is provided through PMIC VSNVS.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EELiu_2-1744788913840.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333402iB69E11833E0F07C5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EELiu_2-1744788913840.png" alt="EELiu_2-1744788913840.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The following figure shows the power on timing sequence of the power supply&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EELiu_0-1744787394194.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333394i008888C6C7F85C5D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EELiu_0-1744787394194.png" alt="EELiu_0-1744787394194.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When we modified the design and changed VDDHIGH_IN from PMIC GEN5 to PMIC SW2, the issue of startup failure was resolved.&lt;/P&gt;&lt;P&gt;The following figure shows the modified power on sequence of the power supply&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EELiu_1-1744787751294.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333397i681E5F7FF050C77A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EELiu_1-1744787751294.png" alt="EELiu_1-1744787751294.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It can be observed that the time difference between VDDHIGH_IN and POR_B has increased from 2.8ms to 16ms.&lt;/P&gt;&lt;P&gt;Our question is:&lt;/P&gt;&lt;P&gt;1. Does VDDHIGH_IN have to be connected to VDD_SNVSIN without using button batteries&lt;/P&gt;&lt;P&gt;2. Does VDHIGH_IN have any power on sequence requirements relative to other power rails such as VDDARM_IN and VDDSOC_IN&lt;/P&gt;&lt;P&gt;3.Is there a time requirement for POR_B signal relative to VDDHIGH_IN, such as setting POR_B high after VDDHIGH_IN is ready for more than 5ms.&lt;/P&gt;&lt;P&gt;Looking forward to receiving a response to our questions, thank you!&lt;/P&gt;</description>
    <pubDate>Wed, 16 Apr 2025 07:39:25 GMT</pubDate>
    <dc:creator>EE-Liu</dc:creator>
    <dc:date>2025-04-16T07:39:25Z</dc:date>
    <item>
      <title>IMX6 booting Random failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-Random-failure/m-p/2081497#M236378</link>
      <description>&lt;P&gt;Hello All,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We have a custom board based on iMX6 quad core processor. It is designed to boot from eMMC.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Processor:&amp;nbsp;&lt;/SPAN&gt; IMX6 Quad， MCIMX6Q6AVT10AD&lt;/P&gt;&lt;P&gt;eMMC ：&lt;SPAN&gt; IS21ES08G-JCLI&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;PMIC：MMPF0100F0AEP（Unconnected button battery）&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;&lt;SPAN&gt;Problem :&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;We see majority of boards boots as designed.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;But there are random failures on one or two boards per hundred( 1 to 2% only).&lt;/SPAN&gt;When the startup fails, both SD3_CMD and SD3_CK remain high without any communication waveform.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Power supply design reference SCH-27516, VDDHIGH_IN is provided through PMIC GEN5, and VDD_SNVS_IN is provided through PMIC VSNVS.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EELiu_2-1744788913840.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333402iB69E11833E0F07C5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EELiu_2-1744788913840.png" alt="EELiu_2-1744788913840.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The following figure shows the power on timing sequence of the power supply&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EELiu_0-1744787394194.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333394i008888C6C7F85C5D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EELiu_0-1744787394194.png" alt="EELiu_0-1744787394194.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;When we modified the design and changed VDDHIGH_IN from PMIC GEN5 to PMIC SW2, the issue of startup failure was resolved.&lt;/P&gt;&lt;P&gt;The following figure shows the modified power on sequence of the power supply&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="EELiu_1-1744787751294.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/333397i681E5F7FF050C77A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="EELiu_1-1744787751294.png" alt="EELiu_1-1744787751294.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It can be observed that the time difference between VDDHIGH_IN and POR_B has increased from 2.8ms to 16ms.&lt;/P&gt;&lt;P&gt;Our question is:&lt;/P&gt;&lt;P&gt;1. Does VDDHIGH_IN have to be connected to VDD_SNVSIN without using button batteries&lt;/P&gt;&lt;P&gt;2. Does VDHIGH_IN have any power on sequence requirements relative to other power rails such as VDDARM_IN and VDDSOC_IN&lt;/P&gt;&lt;P&gt;3.Is there a time requirement for POR_B signal relative to VDDHIGH_IN, such as setting POR_B high after VDDHIGH_IN is ready for more than 5ms.&lt;/P&gt;&lt;P&gt;Looking forward to receiving a response to our questions, thank you!&lt;/P&gt;</description>
      <pubDate>Wed, 16 Apr 2025 07:39:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-Random-failure/m-p/2081497#M236378</guid>
      <dc:creator>EE-Liu</dc:creator>
      <dc:date>2025-04-16T07:39:25Z</dc:date>
    </item>
    <item>
      <title>Re: IMX6 booting Random failure</title>
      <link>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-Random-failure/m-p/2083692#M236508</link>
      <description>&lt;P&gt;I alreday give you update in the case you create, so close it here.&lt;/P&gt;</description>
      <pubDate>Mon, 21 Apr 2025 07:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/i-MX-Processors/IMX6-booting-Random-failure/m-p/2083692#M236508</guid>
      <dc:creator>Rita_Wang</dc:creator>
      <dc:date>2025-04-21T07:12:45Z</dc:date>
    </item>
  </channel>
</rss>